Blog Cheap portable LCD for Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fustini
  • Date Created: 4 Jul 2012 6:36 AM Date Created
  • Views 4487 views
  • Likes 2 likes
  • Comments 25 comments
Related
Recommended
  • raspberry_pi

Cheap portable LCD for Raspberry Pi

fustini
fustini
4 Jul 2012

I've been wanting a small portable display for the Pi.  Unfortunately, portable HDMI displays are quite expensive, and the DSI connector is not an option currently as far as I know.  Then I realized that there a large number of small composite LCDs available which are intended for use in vehicles for backup rearview cameras.  I bought this inexpensive LCD on Amazon, the 3.5 Inch TFT LCD Monitor for Car / Automobile by kingsmart for $21.48 (my order was sold by ePathDirect and fulfilled by Amazon):

imageimage

It arrived today, and I put the photos I took in a Picasa gallery.  I hooked it up to my bench power supply and simply connected it's yellow connector to the composite output on the Pi.  The monitor displayed the Pi's ouptut ok right at power on, through the boot process and beyond.  As I expected, the resolution is poor, especially for small text, given it is standard definition and connected with composite.  However, I'm intending to use this monitor to display tweets, so I can increase the font size as tweets are only 140 characters.  I think this monitor will also be handy for basic troubleshooting when ssh or serial won't suffice, and I don't want to bother with a regular sized monitor.

 

Anyone have any other ideas for inexpensive displays?

 

Cheers,

Drew

  • Sign in to reply

Top Comments

  • sknipas
    sknipas over 13 years ago +1
    I have a 9 inch monitor from an old mini laptop. I also bought a lvds controler from e-bay and I am planning to use this monitor and the r-pi as a car pc. Screen resolution goes up to 1024x600.
  • Former Member
    Former Member over 13 years ago in reply to fustini +1
    It works quite well... But there are some minor disadvantages... 1. you have to concentrate your eyes to have the two displays properly over each other so you have a single image 2. the border region is…
  • jeffbiss
    jeffbiss over 12 years ago in reply to fustini +1
    Now that you mention it, I did the same thing and plumb forgot about it because the screen came with no information! The LCD uses about 5 VDC and has a regulator internally that reduces the car's 12 VDC…
Parents
  • Former Member
    Former Member over 13 years ago

    Not quite inexpenisve (54.99$ +34.25$ shipping) but maybe interesting anyway... I used the myvu solo plus ev video-glasses... quite funny and still working on finding a good resulution setting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fustini
    fustini over 13 years ago in reply to Former Member

    groovy, I would interested to hear more about it works out for you.  google glass has got me interested in wearable displays.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to fustini

    It works quite well... But there are some minor disadvantages...

    1. you have to concentrate your eyes to have the two displays properly over each other so you have a single image

    2. the border region is a little bit fuzzy.

    3. you must adjust the resolution to see the text in the shell.

    Overall it is not the perfect solution but looks very cool image and you can make adjustments on your pi without using a normal screen and an extra power supply for the screen.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Former Member
    Former Member over 13 years ago in reply to fustini

    It works quite well... But there are some minor disadvantages...

    1. you have to concentrate your eyes to have the two displays properly over each other so you have a single image

    2. the border region is a little bit fuzzy.

    3. you must adjust the resolution to see the text in the shell.

    Overall it is not the perfect solution but looks very cool image and you can make adjustments on your pi without using a normal screen and an extra power supply for the screen.
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.