Blog chipKIT™︎ Pi – the Technicals
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: VictoriaJones
  • Date Created: 16 Sep 2013 12:28 PM Date Created
  • Views 1697 views
  • Likes 2 likes
  • Comments 8 comments
Related
Recommended
  • microchip
  • mpide
  • raspi_accessories
  • raspberry_pi
  • chipkit_pi
  • raspeberry_pi_accessories
  • pic32_mcu
  • pic32
  • arduino
  • chipkit™

chipKIT™︎ Pi – the Technicals

VictoriaJones
VictoriaJones
16 Sep 2013

chipKITimage Pi from Microchip and element14

 

As Raspberry Piimage sales continued to rocket we started to try and define what an add-on board might look like (with most of these discussions taking place in the Premier Farnell canteen over numerous cups of coffee or by squeezing in time-zone friendly conference calls with the US team). We all knew that we wanted something using a similar form factor to the Arduinoimage / chipKITimage but we also wanted it to mate with the Raspberry Pi’s I/O connector.

 

We also wanted to differentiate ourselves from mainstream Arduino boards so we chose to use a 28-pin dip PIC32 MCU. Using a DIP MCU kept the product well within the hobbyist domain (how many folk can solder fine pitch parts on their kitchen table?!). Price, needless to say, was also an issue so to keep the board as low cost as we could; we used as many Microchip components as possible.

 

Downloading the completed sketch code onto the chipKIT Pi was always going to be done via the UART on the Raspberry Pi – this would keep the Pi USB ports free for other things. This meant we could conveniently sit the chipKIT Pi over the Raspberry Pi, as long as we positioned the I/O socket on the chipKIT Pi correctly.

 

The PICimage MCU would feature a boot loader and would be placed in boot loader mode by pressing certain buttons on the chipKIT Pi.  The idea was that this would create a nice neat solution that would also be reasonably rugged – but of course we had to consider exactly how this was done without compromising on the boards compatibility with chipKIT / Arduino shields. To help this, various voltage regulators were added to the board, pretty much replicating the circuit on the chipKIT UNO. Other changes included looking at status LEDs as well as providing access to the other Raspberry Pi I/O. Just as on other chipKITs, we provided ICSP (In Circuit Serial Programming) pins to allow the MCU to be reflashed onboard. The other major change made was in adding a USB connector with the eventual aim of allowing the board to work within MPIDE on a Windows platform.

 

With the ideas flowing and momentum pushing forward, the design brief was fired over to Embest for board design and the manufacture kick off.

 

 

Mike McGlade – Senior Regional Channel Manager

  • Sign in to reply
Parents
  • Former Member
    Former Member over 11 years ago

    Hi.

     

    I'm Jean-Yves, my native langage is french so can you be tolerant if i am not very clear!

     

    Many questions on that Chipkit Pi board :

     

    1) can it work alone : i mean without raspberry Pi with MPIDE program?

    2) It is made to program arduino chips? That's it?

    if so what kind of chips? where could i see supported references?

    3) If so can it program also Baseline, Midrange, and advanced Microchip chips?

    4) In not : why? Is it so different?

    5) In the same idea what permits ICSP connector and what are the strange seeked golden pads wholes relative to ICSP on the board?

    6) ICSP : Is it for output to external boards or input from external boards.

     

    Or may i am completly out of subject but i really don't understant what this miracle board could do.

    Really Sorry!

     

    I builded a programmer/tester by  and for my own and have a Chipkit PI at home since 2 month but do not know yet if it will be usable for my needs.

     

    Any help would be appreciable

     

    Thank you very much in advance.

     

    jeanyves.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Former Member
    Former Member over 11 years ago

    Hi.

     

    I'm Jean-Yves, my native langage is french so can you be tolerant if i am not very clear!

     

    Many questions on that Chipkit Pi board :

     

    1) can it work alone : i mean without raspberry Pi with MPIDE program?

    2) It is made to program arduino chips? That's it?

    if so what kind of chips? where could i see supported references?

    3) If so can it program also Baseline, Midrange, and advanced Microchip chips?

    4) In not : why? Is it so different?

    5) In the same idea what permits ICSP connector and what are the strange seeked golden pads wholes relative to ICSP on the board?

    6) ICSP : Is it for output to external boards or input from external boards.

     

    Or may i am completly out of subject but i really don't understant what this miracle board could do.

    Really Sorry!

     

    I builded a programmer/tester by  and for my own and have a Chipkit PI at home since 2 month but do not know yet if it will be usable for my needs.

     

    Any help would be appreciable

     

    Thank you very much in advance.

     

    jeanyves.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 11 years ago in reply to Former Member

    1) It can definitely work stand-alone - just supply electrical power. It can be programmed from any platform that runs MPIDE - such as Raspberry Pi, Windows, Linux and Mac OS.

    2) The ChipKit Pi can plug onto a Raspberry Pi, but does not need this to work. It also has arduino compatible connectors that allow arduino shields to be plugged in. The MPIDE is virtually the same as the standard arduino IDE, so it is just like programming an arduino. As far as I know, the arduino IDE does not run on an arduino or a ChipKit Pi - it needs a bigger host computer.

    3) Any arduino or ChipKit Pi can be used as a programmer for PIC or AVR microcontrollers, but this is an application you would need to implement or copy from many examples on the internet.

    5) The ICSP connector on ChipKit Pi is not populated (you have to install the connector if you want to use it)

    6) This ICSP connector is to program the ChipKit Pi - it is NOT to allow the ChipKit Pi to program other targets.

     

    The ChipKit Pi is a powerful arduino compatible computer (much faster than arduinos) so it can do anything an arduino can do and do it faster plus it can connect directly to a raspberry pi and add an expanded I/O scheme and allow the pi to use arduino shields.