Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Introducing The New Raspberry Pi 5 - 3x Faster, 2.4GHz, VideoCore VII GPU, RTC, Gigabit Ethernet, 1GB, 2GB, 4GB, 8GB RAM
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 28 Sep 2023 7:54 PM Date Created
  • Views 32668 views
  • Likes 12 likes
  • Comments 9 comments
Related
Recommended
  • raspberry pi 5 mipi connectors
  • raspberry pi 5 board layout
  • rp1 southbridge
  • raspberry pi 5 pre-order
  • raspberry pi 5
  • raspberry pi os bookworm
  • raspberry pi
  • raspberry pi 5 features
  • raspberry pi 5 specifications

Introducing The New Raspberry Pi 5 - 3x Faster, 2.4GHz, VideoCore VII GPU, RTC, Gigabit Ethernet, 1GB, 2GB, 4GB, 8GB RAM

e14phil
e14phil
28 Sep 2023

Introducing the Raspberry Pi 5

Meet the New Raspberry Pi 5! It represents a leap in performance, with many widely-requested quality of life features, including an RTC battery connector and an onboard power button! 

Pre-order the Raspberry Pi 5 4GB and 8GB now, and the product will ship at the end of October. 
The Raspberry Pi 5 1GB and 2GB will be coming in the next few months. 

Raspberry Pi 5 Top Down

Raspberry Pi 5 Specifications 

• 2.4GHz quad-core, 64-bit Arm Cortex-A76 CPU, with 512KB L2 caches and a 2MB shared L3 cache
• VideoCore VII GPU
• LPDDR4X-4267 SDRAM (4GB and 8GB SKUs available at launch)
• 2.4 GHz and 5.0 GHz 802.11ac Wi-Fi
• Bluetooth 5.0 / Bluetooth Low Energy (BLE)
• Micro SD card slot, with support for high-speed SDR104 mode
• 2 × USB 3.0 ports, supporting simultaneous 5Gbps operation
• 2 × USB 2.0 ports
• Gigabit Ethernet, with PoE+ support (requires PoE+ HAT)
• 2 × 4 lane MIPI camera/display transceivers
• PCIe 2.0 x1 interface for fast peripherals
• 5V/5A DC power (PD enabled)
• Raspberry Pi standard 40-pin header
• Real-Time Clock (RTC), powered from external battery
• On-board power button!!

What's New with the Raspberry Pi 5? 

The Raspberry Pi 5 comes with the fastest processor yet, as well as a much-requested on/off button, for safely booting and shutting down. 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Raspberry Pi 5 Silicon Custom-developed In-house

Raspberry Pi 5 is the first full-sized Pi computer that uses silicon developed completely in-house.

The RP1 Southbridge provides the majority of the I/O capabilities for the Raspberry Pi 5, delivering a step up in peripheral performance.

Raspberry Pi R1 IO Chipset

- The combined USB bandwidth has been doubled, giving you faster transfer speeds.

- Two individual 4-lane MIPI interfaces support any combination of two cameras or displays.

- SD Card performance has been doubled, with the addition of SD104 High Speed Mode. 

- A new Single-Lane PCI Express 2.0 interface supports higher bandwidth peripherals, increasing expansion capabilities.

Board Layout 

You might have noticed that the Ethernet and USB ports have switched sides, back to where they were on the Raspberry Pi 3 B+.  The PoE hat is different, as well. All of these changes make space for the PCI Express, Dual MIPI, RTC, UART, and fan connectors. 

Raspberry Pi Board Layout Pointing

Raspberry Pi 5 Cameras, Displays, and the New MIPI Connectors

 Raspberry Pi 5 Mipi Screen and Camera Connectors

The Raspberry Pi 5 provides two four-lane MIPI connectors, each of which can support either a camera or a display.

These connectors use the same 22-way, 0.5mm-pitch “mini” FPC format as the Compute Module Development Kit.  They require adapter cables to connect to the 15-way, 1mm-pitch “standard” format connectors on the current camera and display products.  Mini-to-standard adapter cables for cameras and displays in 200mm, 300mm and 500mm lengths.

NOTE: The camera cable should not be used with a display, and vice versa. They are not cross compatible. 

Raspberry Pi Mipi cable

The Raspberry Pi 5 Real-Time Clock

The Raspberry Pi 5 comes with hardware for an onboard Real-Time Clock (RTC), which keeps time when the main power is down. The connector is included in every Raspberry Pi 5 and the RTC Battery is available for sale separately. 

Raspberry Pi 5 RTC Battery

What Raspberry Pi 5 Do I Have?

For the first time, the Raspberry Pi 5 has a silk screen method for showing what memory size your board has.  Along with the Raspberry Pi 5 logo, there are also the 1GB, 2GB, 4GB, and 8GB pads that are bridged by a resistor, showing the model. 

Raspberry Pi what RPi do I have

Raspberry Pi 5 Wi-Fi and Bluetooth

The Raspberry Pi 5 comes with 2.4 GHz and 5.0 GHz 802.11ac Wi-Fi in the modular can we all know, with the very distinctive PCB Antenna.

Raspberry Pi 5 Wifi can

Active Cooling and Fan in the Raspberry Pi 5 Official Case 

The Active Cooler provides an alternative cooling solution for using the Raspberry Pi 5 under sustained heavy load without a case. It combines a large metal heatsink with a variable-speed blower, powered and controlled via the fan connector.  It attaches via sprung pins into a pair of mounting holes.

The new case is a refinement of the Raspberry Pi 4 case, with improved thermal features to support the higher peak power consumption of Raspberry Pi 5. It integrates a variable-speed fan, powered and controlled from a dedicated connector on the Raspberry Pi 5 PCB.

Raspberry Pi 5 Active Cooler

Raspberry Pi OS Bookworm

Raspberry Pi OS launches in mid-October and will be the sole supported first-party operating system for Raspberry Pi 5.  Check back here: we will keep you posted on the new OS, including how to download it shortly before the Pi 5 arrives on the shelves in late October.

Read more about the Raspberry Pi 5 below:

 Raspberry Pi 5 4GB 

 Raspberry Pi 5 8GB ;

  • Sign in to reply
Parents
  • DAB
    DAB over 2 years ago

    Very nice upgrade, I will have to add this to my toy list.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 2 years ago

    Very nice upgrade, I will have to add this to my toy list.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data