Blog Introducing the NEW Raspberry Pi Compute Module
  • Blog
  • Forum
  • Documents
  • Events
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Raspberry Pi requires membership for participation - click to join
Blog Post Actions
  • Subscribe by email
  • More
  • Cancel
  • Share
  • Subscribe by email
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: lbittner
  • Date Created: 7 Apr 2014 11:59 AM Date Created
  • Views 1119 views
  • Likes 7 likes
  • Comments 25 comments
  • raspberry
  • applications
  • raspberry_pi_compute_module_development_kit
  • industrial
  • pi
  • compute
  • embedded
  • raspberry_pi
  • io_board
  • raspberry-pi
  • development
  • kit
  • design-in
  • module
Related
Recommended

Introducing the NEW Raspberry Pi Compute Module

lbittner
lbittner
7 Apr 2014

Designing in the Future: Raspberry Pi Compute Module Development Kit

 

Coming Summer 2014!

 

The new Raspberry Pi Compute Development Kit enables design engineers

to harness the power of the Raspberry Pi for embedded applications.

 



  • Small and Powerful. SODIMM sized (6.5cm by 3cm) Raspberry Pi board contains the BCM2835 chip with 512MB RAM with an on board 4GB eMMC Flash memory for booting the OS.
  • Flexible and Rapid Prototype Development. A fully functional IO board is part of the development kit which supports an extensive GPIO and multiple connectors to help foster rapid prototype development with access to all of the BCM2835 functionality.
  • Custom Hardware and Software Solutions. Benefit from fully functional Linux server running on your ‘design-in’ hardware solution. This unique combination of services will help define the next generation of the ‘Internet of Things’


Compute Module Development Kit Technical Specifications:


Compute Module:

  • SODIMM sized 6.5cm by 3cm board
  • BCM2835 chip with 512MB RAM
  • On board 4GB eMMC Flash memor
  • 200 pin edge connector


IO board:

  • Multiple GPIO interfaces
  • 1 x micro USB connector type B
  • 1 x USB connector type A
  • 2 x CSI ports for camera boards
  • 2 x DSI ports for display boards
  • Full size HDMI port


Harness the power of the Raspberry Pi for your embedded applications!

 

Request Consultation...

Complete this form and one of our Design Representatives will call you to discuss your embedded design.

 

You don't have permission to edit metadata of this video.
Edit media
x
Upload Preview

 

See schematics for:

Compute Module

Io Board

Anonymous

Top Comments

  • raspberrystore
    raspberrystore over 8 years ago in reply to Former Member +2

    Its just who develops an IO-board first, with only ethernet, GPIO (USB?) and power (on the same side). Sadly not me, Id really like to test them!

  • lbittner
    lbittner over 8 years ago in reply to jamodio +1

    Thanks for alerting us, jamodio! The two links will now take you and other members to separate documents.

     

    Best,

    Lauren

  • Former Member
    Former Member over 8 years ago +1

    Ethernet port?

Parents
  • Former Member
    Former Member over 8 years ago

    Ethernet port?

    • Cancel
    • Up +1 Down
    • Reply
    • More
    • Cancel
  • jamodio
    jamodio over 8 years ago in reply to Former Member

    The Broadcom SoC does not have an integrated Ethernet controller and no external controller is shown on either schematic, so the answer is no ethernet.

     

    Also it is a shame that they didn't expose the eMMC/SD interface on the SODIMM socket, unless there is a second SD interface on the other GPIO pins,  while you can disable the on board eMMC and force the BCM2835, to boot from USB.

     

    Note that with announced IO board you will have only one USB port, then we won't have the option to use an external SD card (bigger than the included 4GB eMMC) and override the eMMC.

     

    Glad to see they put together a smarter more efficient design for the power supply on the IO board.

     

    -J

    • Cancel
    • Up 0 Down
    • Reply
    • More
    • Cancel
  • raspberrystore
    raspberrystore over 8 years ago in reply to jamodio

    On the type B the Ethernetport and extra USB is provided by the extra controller. This controller uses the USB-port, and is actually a USB-hub with ethernet-port. So, add a USB hub and add an USB-ethernet-adapter, and you have the same specs. The whole compute-board is designed to let you create your own board, so you can add the devices you want... You can also add an extra SD-adapter on the i2c bus, if you really need extra storage on the board. Personally I'd mount a SAN to get to really much data. With wifi I think that wouldn't be that big of a problem.

     

    The new board is indeed quite awesome. Really want one,.. Also for the dual cam input.

    • Cancel
    • Up 0 Down
    • Reply
    • More
    • Cancel
  • jamodio
    jamodio over 8 years ago in reply to raspberrystore

    Thanks I'm aware of it. Have several Rpis in different projects and I was the culprit of discovering the error of the 1.8V power supply in the Rev 1 PCB.

     

    BTW is called "Model B" not "type B"

     

    And you can't connect a SD card via I2C.

     

    -J

    • Cancel
    • Up 0 Down
    • Reply
    • More
    • Cancel
  • jamodio
    jamodio over 8 years ago in reply to jamodio

    Seems that the second SD interface (SD1) can be available on the GPIO22-27 pins, so if the hooks are on the kernel it would be possible to add a second SD card socket on the carrier board, leave the bootloader on the eMMC and point to the kernel image on the external SD card.

     

    I don't think that the BCM2835 can be set to boot directly from it, most of this type of SoC only boot from channel 0. Unfortunately complete documentation for the BCM2835 is still NOT available :-(

     

    Cheers

    Jorge

    • Cancel
    • Up +1 Down
    • Reply
    • More
    • Cancel
Comment
  • jamodio
    jamodio over 8 years ago in reply to jamodio

    Seems that the second SD interface (SD1) can be available on the GPIO22-27 pins, so if the hooks are on the kernel it would be possible to add a second SD card socket on the carrier board, leave the bootloader on the eMMC and point to the kernel image on the external SD card.

     

    I don't think that the BCM2835 can be set to boot directly from it, most of this type of SoC only boot from channel 0. Unfortunately complete documentation for the BCM2835 is still NOT available :-(

     

    Cheers

    Jorge

    • Cancel
    • Up +1 Down
    • Reply
    • More
    • Cancel
Children
  • Former Member
    Former Member over 8 years ago in reply to jamodio

    this is the best news i've heard all day, it would be cake to connect an sdcard to gpio. any chance we can get someone to confirm that this would be possible?

     

    myself though, i like the idea of having the 4gb onboard for os and programming and then being able to add a large capacity sdcard for data storage. (i've got me an idea see)

     

    regarding alternate booting though it does say on page 3 of the schematic "BCM2835 will fail to boot from eMMC if EMMC_DISABLE_N is LOW and will therefore fall back to booting from USB." so you should at least be able to use usb.

     

    by any chance could ethernet/wifi also be made available through gpio?

    • Cancel
    • Up 0 Down
    • Reply
    • More
    • Cancel
  • Former Member
    Former Member over 7 years ago in reply to jamodio

    jamodio wrote:

     

    Seems that the second SD interface (SD1) can be available on the GPIO22-27 pins, so if the hooks are on the kernel it would be possible to add a second SD card socket on the carrier board, leave the bootloader on the eMMC and point to the kernel image on the external SD card.

    Where did you learn this? I would really like to have this ability, but I wasn't able to find any mention of a second SD interface in the BCM2835 datasheet or the Compute Module announcement. Booting from eMMC and using external SD for data would be good for a project I have in mind.

    • Cancel
    • Up 0 Down
    • Reply