Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Raspberry Pi 2 - Plex Media Server
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: biglesp
  • Date Created: 3 Mar 2016 1:15 PM Date Created
  • Views 10932 views
  • Likes 4 likes
  • Comments 40 comments
Related
Recommended
  • plex_media_server_software
  • rpiintermediate
  • project
  • rpibeginner
  • internet_of_things
  • pi2_project
  • raspberrypi_project
  • raspberrypi
  • iot
  • raspberrypi2
  • media_library
  • plex
  • raspbian
  • multi_room_audio
  • pi2
  • home_entertainment

Raspberry Pi 2 - Plex Media Server

biglesp
biglesp
3 Mar 2016

With our ever increasing media libraries containing movies, TV shows, music and pictures we need something that can serve this content to any of our devices.

 

25100202219_0e81f79d0e_b_d.jpg

 

If you fancy opera in the kitchen, jazz in the bathroom and the latest Hollywood blockbuster in your pocket, then you need a media server and the Raspberry Pi 2 is the ideal low cost candidate.

To replicate this project you will need:

 

  • A Raspberry Pi 2
  • A laptop running Windows/Mac or Linux
  • A minimum of 8GB SD card
  • A 2A power supply
  • An Ethernet cable connected to a router.
  • An external USB hard drive

 

16249575259_467b219fb4_k_d.jpg

 

We start the project by installing the latest version of Raspbian on to an 8GB or greater SD card. The best tutorial on how to do this is provided by the Raspberry Pi Foundation and can be found on their blog

With Raspbian installed we now need to boot our Raspberry Pi. Insert the microSD into the Raspberry Pi, then attach any peripherals such as keyboard, mouse, HDMI, Ethernet to the Pi. Lastly attach the power cable to boot the Pi.

When your Pi has booted to the desktop, click on the menu to the top left of the screen and go to the Preferences menu. From there select the Raspberry Pi Configuration application.

In this application we need to change the boot behaviour so that the Pi boots to the terminal and is logged in. We’ll also change the memory for the GPU to only use 16MB of RAM, and overclock the Pi 2 to 1GHz.

With these changes made, save and exit the application. You will be asked to reboot, do so before progressing.

With our Pi rebooted we now find ourselves at the terminal. It may seem a little scary at first but the terminal is the best way to work with a Linux computer.

Setup software

Our next goal is to install the software necessary for our Pi.

First we update our list of available software. In the terminal type.

 

sudo apt-get update

 

The update will take a few moments to complete. When the terminal is returned to you enter the next command to install the HTTPS transport package to enable access to HTTPS content over the Internet.

 

sudo apt-get install apt-transport-https -y --force-yes

 

Next we shall download a key that will authenticate our downloads to ensure they are safe

 

wget -O - https://dev2day.de/pms/dev2day-pms.gpg.key  | sudo apt-key add -

 

With the key downloaded we now add a new repository to our list, this repository is provided by dev2day.de who has worked on the packages that will power our Plex install.

In the terminal type

 

echo "deb https://dev2day.de/pms/ jessie main" | sudo tee /etc/apt/sources.list.d/pms.list

 

We now update our list again, to ensure that we now have the latest updates for the Plex Media Server.

 

sudo apt-get update

 

Lastly we install the Plex Media Server software.

 

 

sudo apt-get install -t jessie plexmediaserver -y

 

The install will only take a few minutes and once completed the Plex Media Server will automatically start as a background service on your Pi.

Fix IP address of the Pi

To ensure that we can discover our Pi on a network we will now fix the IP address of the Pi.

First we need to find out the IP address, in the terminal type.

 

 

hostname -I

 

Write down your IP address!

Now let's fix the IP address, in the terminal type

 

sudo nano /boot/cmdline.txt

 

At the very end of the line we will add the IP address that we earlier wrote down. So type

 

ip=THE IP ADDRESS YOU WROTE DOWN

 

With the IP entered press CTRL + O, then Enter to save your changes.

Now press CTRL + X to close the file.

Now reboot your Pi to make the changes permanent.

 

sudo reboot

 

With your Pi rebooted we shall now test that we can access the Plex server. On your laptop or desktop PC open a web browser and type your IP address followed by :32400/web so for example I typed.

 

192.168.0.90:32400/web

 

24841031413_78331093d4_b_d.jpg

 

This will now open the Plex Media Server software and we will need to read and accept the Terms and Conditions before progressing.

Once Plex has loaded take a few moments to get familiar with the interface. Specifically the libraries, which will house your media collection.

The SD card of our Raspberry Pi is rather small, so let's add an external hard drive and store our media there.

Plug in your USB drive. Nothing will happen in Plex until we mount the drive. In Linux, mounting a drive means that it is ready to be used. On your Raspberry Pi, in the terminal type

 

dmesg

 

You will see a lot of text whizz up the screen but keep a look out for your hard drive.

So now lets create somewhere to link our hard drive to the Raspberry Pi this will be a directory called “library”. In the terminal type

 

sudo mkdir /mnt/library

 

Now we shall open a text editor and add a line of code to mount the drive on boot. For our drive we used a FAT32 formatted drive. As this is the only USB drive it will be given the assignment “sda” and if the drive has one partition, where our data is stored, then it will be “1”. This gives us the location of our media which is “sda1”.

 

sudo nano /etc/fstab

 

25467761615_c0b2d45027_b_d.jpg

 

So now we shall mount our drive, got to the last line which starts with a “/” and make a new line under it. Enter the following and try and keep your spacing similar to those above.

 

/dev/sda1    /mnt/library   vfat   defaults    0    0

 

To save your work press CTRL + O followed by Enter. Then to exit press CTRL + X.

Reboot your Raspberry Pi.

 

sudo reboot

 

Once the Pi has booted back up navigate to your content by typing.

 

cd /mnt/library

 

Now we need to see where our content is, so to find it type

 

ls

 

You should see lots of directories and files, just as you arranged them on your main computer.

Our next step involves enabling access to the files for any user. As our server will be in our home we shall enable access to all of the content for all of the users. Typically this is not the done thing for big servers in production but for our server this is fine. So to enable access we need to type

 

sudo chmod 777 -R /mnt/library

 

Now this might take some time so be patient.

 

25349753862_c979d92f73_h_d.jpg

 

So now that we our drive ready to serve our media, let's start using it!

Back to our laptop/PC and open your web browser to your Plex Media Server.

You will be prompted to add a library, so go ahead and do so. Now which library you add depends on what you have. I chose to add a couple of TV series. When ready click on “Add Library” to import the media.

 

24837201614_aacabb5271_b_d.jpg

24841031493_351b6b9f21_b_d.jpg

 

Depending on the amount of media that you have to import this process may take minutes or hours, so please be patient and wait for the process to finish.

When the media is imported, Plex will try its best to grab the metadata, the information about the content such as genre, IMDB data, actor details etc.

 

24841467453_b9cea3a480_h_d.jpg

Multi User Access

The huge benefit of Plex is that any user on the home network can access any of the media in the library. So children can watch their favourite films on the mobile device, parents can listen to music or podcasts or share their family photos on their laptops.

Plex can also be streamed to a chromecast device, enabling high definition movies to be enjoyed on the big screen.

Listen to all of your music across your entire home and all you need is a Raspberry Pi and a little Linux know how.

  • Sign in to reply

Top Comments

  • spannerspencer
    spannerspencer over 10 years ago +2
    My smart TV has Plex, but it makes my old NAS crawl to run the server. This'd be a good way to effectively update the NAS and start using Plex again! Nice work!
  • Matt
    Matt over 10 years ago +1
    Awesome. I've heard really good things about Plex.. thanks for putting together all these instructions for how to get it working on a Pi
  • biglesp
    biglesp over 10 years ago in reply to clem57 +1
    Hi Clem Plex is a product that comprises of a server providing content to clients on a network.
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hmmm followed exactly the installation instructions, including first expanding the file system, and turned off my firewall, I can see that the plex server has started see attached but when I point my chrome browser at  http://192.168.0.251:32400/web  as advised I get .....

     

    This site can’t be reached

    192.168.0.251 refused to connect.

     

    • Search Google for 192 168 251 32400 web

     

    Where do I go from here ?

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Did you ever fix this issue? I am having the same problem. I am not an expert in Plex or Rasbian so I am not sure where to go. I have tried Googling it but I keep heading down some rabbit holes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Did you ever fix this issue? I am having the same problem. I am not an expert in Plex or Rasbian so I am not sure where to go. I have tried Googling it but I keep heading down some rabbit holes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Nope I cannot get it to work, if I do .....

     

    pi@raspberrypi:~ $ service plexmediaserver status

    ● plexmediaserver.service - LSB: Plex Media Server

       Loaded: loaded (/etc/init.d/plexmediaserver)

       Active: active (exited) since Tue 2016-06-28 12:13:15 UTC; 5 days ago

      Process: 355 ExecStart=/etc/init.d/plexmediaserver start (code=exited, status=0/SUCCESS)

     

    So it appears to be running but I get This site cant be reached when i try http://192.168.0.251:32400/web  or  http://192.168.0.251:32400/web/index.html#!/settings

     

    In reality I don't understand why I need to configure port forwarding because the pi and my desktop are on the same same network although I have set port forwarding up, but I cannot get it to work so I am a bit fed up.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to e14 Contributor

    I'm having the same issue. It's not running (code=exited), but it was never bound to any ports or leave any error logs.