Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Raspberry Pi 3 HTML User Interface part.1
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Former Member
  • Date Created: 10 Oct 2016 6:59 PM Date Created
  • Views 2181 views
  • Likes 1 like
  • Comments 4 comments
Related
Recommended
  • rpi3
  • ras pi 3
  • raspberrypi3

Raspberry Pi 3 HTML User Interface part.1

Former Member
Former Member
10 Oct 2016

I've always loved the idea of being able to access popular single board computers and their hardware using a HTML browser. Nearly every gadget we own e.g. mobile phones, ipods, tablets, laptops etc.. all have web browser functionality so it stands to reason that if we were to make a user interface that is based around web browsers then all of these gadgets will be able to use it. Many people have at least some knowledge of writing programs for web browsers that they can build upon, most school children are leaving secondary education with some ability to make their own web page too so it's a great way for people to interact with their Raspberry Pi!!

 

Things I have done to prepare the Raspberry Pi 3 before commencing the steps in this blog are:

 

1) Setting up the wireless network adapter with a static ip address (required for simplicity)

2) Installed and configured Lighttpd (A lightweight webserver that is an excellent choice for the Raspberry Pi)

 

--------------------------------------------------------------------------------------------------------

 

This interface is in it's very early stages, currently the rpi3 is able to serve a webpage out to any device with a web browser on the same network as itself, once the webpage loads up there's a button to start live updates and a button to stop live updates. When the start button is pressed, a Javascript module polls a Python script on the rpi3 at 1 second intervals. The Python script returns the current time on the Raspberry Pi to the javascript and that information is displayed on the webpage. - SEE VIDEO BELOW FOR EXAMPLE

 

There might not seem like a great deal of point in just getting and displaying the time remotely but it can be expanded to send/receive data from/to the i2c or spi bus, set/clear gpio pins etc.. any data processing can be done either on the server side using python (raspberry pi) or the processing can be done on the client side using javascript (any device with webbrowser).

 

There are just 2 files used to make this system work at the minute, a standard index.html file and a basic.py file below.

 

index.html

 

<html>
<body>
Raspberry Pi Network Interface Test

<p>
<input type="button" onClick="startLiveUpdates()" value="Begin Updates">
<input type="button" onClick="stopLiveUpdates()" value="Stop Updates">
</p>

<div id="outputarea">output area</div>

<script>

var timer_interval

function getPiTime(){
var req = new XMLHttpRequest();
req.onreadystatechange = function() {
        if (this.readyState == 4 && this.status == 200) {
            document.getElementById("outputarea").innerHTML = this.responseText;
        }
    };
req.open("POST","/cgi-bin/basic.py",true);
req.send();

}

function startLiveUpdates(){
getPiTime();
timer_interval=setInterval(getPiTime,1000);
}
function stopLiveUpdates(){
clearInterval(timer_interval);
}
</script>

</body>
</html>

 

basic.py

 

#! /usr/bin/python
#

import os
import threading
import time
import subprocess

localtime = time.asctime( time.localtime(time.time()) )

print "Content-Type: text/html\n\n"
print '<html><head><meta content="text/html; charset=UTF-8" />'
print "time on rapsberry pi: ", localtime
print "</body></html>"

 

most of the imports in the basic.py file arent required in the code, they are future relics!!

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • Former Member
    Former Member over 9 years ago in reply to DAB +1
    Im not sure how the raspberry pi would cope with multiple devices using the interface, a small number wouldnt cause any issues but it could soon become overloaded resource wise. The basic operation of…
  • Former Member
    Former Member over 9 years ago +1
    Interesting approach and useful for someone else as a starter kit to build on for another application. You could really run the Pi side on almost any model - like one that is gathering dust in a drawer…
Parents
  • Former Member
    Former Member over 9 years ago

    Interesting approach and useful for someone else as a starter kit to build on for another application.  You could really run the Pi side on almost any model - like one that is gathering dust in a drawer having been replaced by a more powerful Pi.

     

    I developed a Raspberry Pi based web server for a different purpose (Do-It-Yourself Certificate Authority on a Raspberry Pi).  It got complicated enough that I resorted to using a Python package called "Flask" to provide the web server infrastructure.  Maybe I overkilled this but my users in Asia are far away and I did not want them calling me in the middle of their afternoon (I'm in Texas USA).  Note that this could run on almost any model - maybe every model (only tested on models 2 and 3 so far in Hong Kong and here in Texas).

     

    If you follow-up this project with an enhancement or a "left-turn" to the approach, please publish.  Thank you.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Former Member
    Former Member over 9 years ago

    Interesting approach and useful for someone else as a starter kit to build on for another application.  You could really run the Pi side on almost any model - like one that is gathering dust in a drawer having been replaced by a more powerful Pi.

     

    I developed a Raspberry Pi based web server for a different purpose (Do-It-Yourself Certificate Authority on a Raspberry Pi).  It got complicated enough that I resorted to using a Python package called "Flask" to provide the web server infrastructure.  Maybe I overkilled this but my users in Asia are far away and I did not want them calling me in the middle of their afternoon (I'm in Texas USA).  Note that this could run on almost any model - maybe every model (only tested on models 2 and 3 so far in Hong Kong and here in Texas).

     

    If you follow-up this project with an enhancement or a "left-turn" to the approach, please publish.  Thank you.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data