Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Raspberry Pi Facial Recognition
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: sharib123
  • Date Created: 11 Feb 2019 6:18 AM Date Created
  • Views 19462 views
  • Likes 19 likes
  • Comments 61 comments
Related
Recommended
  • face_recognition
  • iot security
  • open cv
  • machine_learning
  • artificial intelligence
  • raspberry pi
  • ai
  • ai project
  • computer vision

Raspberry Pi Facial Recognition

sharib123
sharib123
11 Feb 2019

This project is done with Open Source Computer Vision Library (OpenCV). OpenCV was designed for computational efficiency and with a strong focus on real-time applications. So, it's perfect for real-time face recognition using a camera. To create a complete project on Face Recognition, we must work on 3 very distinct phases:Face detection and data gathering, train the recognizer and face recognition. we will simply create a data-set, where we will store images for each id, a group of photos that are used for face detection.

 

Requirements:

I. Raspberry Pi 4 model BRaspberry Pi 4 model B                       

II. Raspberry Pi 4 Power SupplyRaspberry Pi 4 Power Supply     

III. Raspberry pi Touch Screen Display 7 inchRaspberry pi Touch Screen Display 7 inch

IV. Raspberry Pi NoIR CameraRaspberry Pi NoIR Camera        

 

 

Raspberry Pi 4 Pin Configuration

image

 

Connection:

i.Connect Ribbon cable from Display to Raspberry Pi

ii. Connect SDA to Raspberry Pi SDA pin and connect SCL from Display to Raspberry Pi SCL pin

image

 

iii. Connect Ribbon cable from camera to Raspberry Pi

image

iv. Connect GND from Display to Raspberry Pi GND

v. Connect 5V from Display to Raspberry Pi 5V

 

Procedure for installing opencv and facial recognition libraries

Step #1: Expand file system

 

$ sudo raspi-config

In the “Advanced Options” menu select “Expand Filesystem”, select the first option, “A1. Expand FileSystem”, click “<Finish>” button, and then reboot your Pi

 

image

$ sudo reboot

 

Step #2: Install dependencies

$ sudo apt-get update && sudo apt-get upgrade  
$ sudo apt-get install build-essential cmake pkg-config  
$ sudo apt-get install libjpeg-dev libtiff5-dev libjasper-dev libpng-dev
$ sudo apt-get install libavcodec-dev libavformat-dev libswscale-dev libv4l-dev  
$ sudo apt-get install libxvidcore-dev libx264-dev  
$ sudo apt-get install libgtk2.0-dev libgtk-3-dev  
$ sudo apt-get install libfontconfig1-dev libcairo2-dev
$ sudo apt-get install libgdk-pixbuf2.0-dev libpango1.0-dev
$ sudo apt-get install libhdf5-dev libhdf5-serial-dev libhdf5-103
$ sudo apt-get install libqtgui4 libqtwebkit4 libqt4-test python3-pyqt5
$ sudo apt-get install libatlas-base-dev gfortran  
$ sudo apt-get install python2.7-dev python3-dev 
$ sudo apt-get install python3-pil.imagetk

 

Step #3: Download the OpenCV source code

$ cd ~
$ wget -O opencv.zip https://github.com/opencv/opencv/archive/4.1.1.zip
$ unzip opencv.zip
$ wget -O opencv_contrib.zip https://github.com/opencv/opencv_contrib/archive/4.1.1.zip
$ unzip opencv_contrib.zip

Step #4: Install Pip

$ wget https://bootstrap.pypa.io/get-pip.py
$ sudo python3 get-pip.py

 

step #5: Installing NumPy on your Raspberry Pi

$ pip3 install numpy

 

Step #6: Compile and Install OpenCV

$ cd ~/opencv-4.1.1/  
$ mkdir build 
$ cd build
$ cmake -D CMAKE_BUILD_TYPE=RELEASE \
    -D CMAKE_INSTALL_PREFIX=/usr/local \
    -D OPENCV_EXTRA_MODULES_PATH=~/opencv_contrib-4.1.1/modules \
    -D ENABLE_NEON=ON \
    -D ENABLE_VFPV3=ON \
    -D BUILD_TESTS=OFF \
    -D INSTALL_PYTHON_EXAMPLES=ON \
    -D OPENCV_ENABLE_NONFREE=ON \
    -D CMAKE_SHARED_LINKER_FLAGS=-latomic \
    -D BUILD_EXAMPLES=ON ..

 

step #7 Configure your swap space size before compiling

if you are not increasing the swap size then there is a chance that opencv will not compile

 

Open your /etc/dphys-swapfile  and then edit the CONF_SWAPSIZE  variable:

 

sudo nano /etc/dphys-swapfile

 

The default value in Raspbian is:

CONF_SWAPSIZE=100

Change this to:

CONF_SWAPSIZE=1024

Stop and start the service that manages the swapfile on Rasbian:

 

$ sudo /etc/init.d/dphys-swapfile stop
$ sudo /etc/init.d/dphys-swapfile start

 

step #8 Build and install OpenCV

$ make -j4
$ sudo make install
$ sudo ldconfig

 

Step #9: Testing your OpenCV  install

$ python3
>>> import cv2
>>> cv2.__version__
'4.1.1'

step #10 Change your swap size back

If swap size is not restored back the memory card will not last longer.

Open your  /etc/dphys-swapfile  and then edit the  CONF_SWAPSIZE  variable:

CONF_SWAPSIZE=100

To revert to the smaller swap space, restart the swap service:

$ sudo /etc/init.d/dphys-swapfile stop
$ sudo /etc/init.d/dphys-swapfile start

 

step #11 Installing libraries required for facial recognition:

$ pip3 install dlib
$ pip3 install face_recognition
$ pip3 install imutils

 

Executing the code

The source files for this project are attached with this blog, simply extract and run the code.

 

step #1

Run the file faceDataset.py, a dialog window will open, enter the name of the person whose images are to be stored. If the name is not entered the folder will not be created. This is the folder where all the images of that particular person will be stored and is required for further processing.

 

$ python3 faceDataset.py

 

Click on create and then click start capture.

 

image

 

 

An image capturing window will open click on Snapshot to take the photos of the person. It will store a single image every time you click on Snapshot. Take at least 6-7 images in the different face position, for example straight, tilt and side pictures. Close the window when done.

image

 

To create the multiple person data repeat the previous step

NOTE: If numerous person data are stored, the encoding time will increase, as the raspberry pi is a low power computer it will take more time to process, and the facial recognition will run slower.

 

step #2

Run the file face_recognize.py .

 

$python3 face_recognize.py

 

A window will open and shows the processing image. The processing time depends on the number of images stored.

image

 

After processing the images, the "Frame window" will open, when the camera detects the person's face, it will show the name of the person if its matches with the images in the database. Press Q on the keyboard to close the Frame window.

 

image

Attachments:
facepi.zip
  • Sign in to reply

Top Comments

  • sharib123
    sharib123 over 7 years ago in reply to fmilburn +4
    Hi Frank, faceDataset.py is built using tkinter framework and hence it is required. You can do manually also, without using it. You can create folder of your name manually inside the dataset folder, and…
  • sharib123
    sharib123 over 7 years ago in reply to fmilburn +3
    Dear Frank, Thank you for correcting me, it is faceDataset.py. The attached source files are for above blog only. you are getting error because there is some problem with your tkinter. Type this in terminal…
  • DAB
    DAB over 7 years ago +2
    Nice post. You can use a memory stick with your Rpi to transfer files between machine types. DAB
Parents
  • fmilburn
    fmilburn over 7 years ago

    Hi Sharib,

     

    Thanks for posting this as I have been wanting to try OpenCV for some time.  I was able to install it following your directions but have not been able to open a database.  I don't use a Pi or Python often but it appears your attached source file may be different than the description in the blog above.  For example, there is not a file named face_dataset.py but there is one called faceDataset.py.  However, when I attempt to run it I get an error "No module named tkinter".  But I know that tkinter is present as I can import it if I start a new python script.  I presume I need to set up a path for a module in python?  Thanks again for posting.

     

    Frank

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fmilburn
    fmilburn over 7 years ago

    Hi Sharib,

     

    Thanks for posting this as I have been wanting to try OpenCV for some time.  I was able to install it following your directions but have not been able to open a database.  I don't use a Pi or Python often but it appears your attached source file may be different than the description in the blog above.  For example, there is not a file named face_dataset.py but there is one called faceDataset.py.  However, when I attempt to run it I get an error "No module named tkinter".  But I know that tkinter is present as I can import it if I start a new python script.  I presume I need to set up a path for a module in python?  Thanks again for posting.

     

    Frank

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • sharib123
    sharib123 over 7 years ago in reply to fmilburn

    Dear Frank,

     

    Thank you for correcting me, it is faceDataset.py. The attached source files are for above blog only. you are getting error because there is some problem with your tkinter. Type this in terminal

    $ python3

    >>import tkinter

    >>tkinter.TkVersion

    >>8.6

    make sure it is 8.6.

     

    Python 3 uses the module name tkinter whereas Python 2 uses Tkinter

     

    Also you have to connect Raspberry Pi Camera otherwise the stream will not start. when you extract the file you will see one database folder, inside that database folder one folder with my name and pictures is there. when you run faceDataset.py the app will create the folder for you and also the snapshot will automatically get stored inside your created folder.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to sharib123

    Thanks for your response... I checked python3 as you suggested and can confirm that the tkinter verision is 8.6.

     

    I am able to successfully run face_recognize.py (from the command line), but not faceDataset.py.  In the text from a command line session below the directory where FaceDatasetGui/ is placed is shown and the contents listed.  The python3 script faceDataset.py is then invoked and fails.  Lastly, recognize.py is invoked and succeeds.

     

    pi@raspberrypi:~ $ cd FaceDatasetGui/
    pi@raspberrypi:~/FaceDatasetGui $ dir
    build    faceclass      haarcascade_frontalface_default.xml
    dataset    faceDataset.py     __pycache__
    dist    faceDataset.spec   setup.py
    encode_faces.py   faceDataset.zip
    encodings.pickle  face_recognize.py
    pi@raspberrypi:~/FaceDatasetGui $ python3 faceDataset.py
    Traceback (most recent call last):
      File "faceDataset.py", line 5, in <module>
        from faceclass.faceapp import FaceApp
      File "/home/pi/FaceDatasetGui/faceclass/faceapp.py", line 4, in <module>
        from PIL import ImageTk
    ImportError: cannot import name 'ImageTk'
    pi@raspberrypi:~/FaceDatasetGui $ python3 face_recognize.py
    [INFO] quantifying faces...
    [INFO] processing image 1/2
    [INFO] processing image 2/2
    [INFO] serializing encodings...
    [INFO] loading encodings + face detector...
    [INFO] starting video stream...
    [ INFO:0] Initialize OpenCL runtime...

     

    If I try to run faceDataset.py with Geany I get the following response in the shell window:

    Traceback (most recent call last):
      File "faceDataset.py", line 5, in <module>
        from faceclass.faceapp import FaceApp
      File "/home/pi/FaceDatasetGui/faceclass/faceapp.py", line 5, in <module>
        import tkinter as tki
    ImportError: No module named tkinter
    
    ------------------
    (program exited with code: 1)
    Press return to continue

     

    This could easily be something I am doing fundamentally wrong as I have not used python in a long time and am not a knowledgeable user of Linux.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sharib123
    sharib123 over 7 years ago in reply to fmilburn

    Hi Frank,

     

    faceDataset.py is built using tkinter framework and hence it is required. You can do manually also, without using it. You can create folder of your name manually inside the dataset folder, and store some of your images in it, after that run face_recognize.py.

     

    For tkinter to work try removing python2 including tkinter from your system. I think it is taking default path for python2 tkinter and therefore it is not finding it, and then fresh install for python3 by command

    $ sudo apt-get install python3-tk.

     

    you can also modify the code where it is importing tkinter. Try changing from

    1. import tkinter as tki //this is for python3
    2. to
    3. import Tkinter as tki //this is for python2

     

    I have used Raspbian Stretch operating system for raspberry Pi. Other operating system i am not sure.

    I hope this helps.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to sharib123

    Thanks Sharib,

     

    I am using Raspbian Stretch and have it working now by just taking the pictures manually using raspistill from the command line.  Thanks for helping me out and I will be playing around with it a bit more.  I thought I would also try using matlab.  Thanks again!

     

    Frank

    • Cancel
    • Vote Up +2 Vote Down