Blog Raspberry Pi lapdock tricks
  • Blog
  • Forum
  • Documents
  • Events
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Raspberry Pi requires membership for participation - click to join
Blog Post Actions
  • Subscribe by email
  • More
  • Cancel
  • Share
  • Subscribe by email
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fustini
  • Date Created: 11 Sep 2012 9:57 PM Date Created
  • Views 590 views
  • Likes 3 likes
  • Comments 19 comments
  • android
  • raspberry_pi
  • rpi
  • atrix
Related
Recommended

Raspberry Pi lapdock tricks

fustini
fustini
11 Sep 2012

I learned a couple tricks for the Atrix lapdock last night during our Raspberry Pi / embedded interest group at my hackerspace.  One of our members, Jay, had a super capacitor hooked up his Pi:

Why would he do this?  Well, the power supplied from the Atrix lapdock drops for a few seconds when the lapdock lid is closed.  The super cap keeps the Pi running in the meantime.

You can click on these pictures to enlarge, but there probably still isn't enough detail to know how to hook it up.  Therefore, I'm hoping to get the complete details and will post here. 

 

In the meantime, here's another trick Jay came up with where he uses a small USB battery pack to act as a buffer:

The charging input for the battery pack is connected to the lapdock while it's output goes to the Raspberry Pi (or Android MK802 mini-PC in these pictures):

 

Cheers,

Drew

Anonymous

Top Comments

  • Former Member
    Former Member over 8 years ago +1

    Surgery free supercap mod for pi/lapdock

    I wired two 2.5 volt 1.0F supercaps in serial, cut the end off a usb plug and soldered the cap to the appropriate red & black wires on the usb plug. Some hot glue…

Parents
  • Former Member
    Former Member over 7 years ago

    is Pi 2 capable of using the dock? 

    • Cancel
    • Up 0 Down
    • Reply
    • More
    • Cancel
Comment
  • Former Member
    Former Member over 7 years ago

    is Pi 2 capable of using the dock? 

    • Cancel
    • Up 0 Down
    • Reply
    • More
    • Cancel
Children
  • johnbeetem
    johnbeetem over 7 years ago in reply to Former Member

    Miriam Laskey wrote:

     

    is Pi 2 capable of using the dock?

    The answer is probably yes.  I've read of people using RasPi Model B+ with Lapdock, and RasPi 2 should have the same external interfaces.  One thing you can't do with an unmodified B+ (and therefore RasPi 2) is to back-power through a RasPi USB A port.  This is because of the B+ USB Vbus circuitry.  You need a "Y" cable that provides power through RasPi's Micro USB power jack and data through a RasPi USB A port.

     

    I'll come back and provide some links -- I've got to run now.

     

    Update: Here's the RasPi Forum thread where I read that B+ works with Atrix Lapdock, but not if you backpower:

    Raspberry Pi • View topic - I made a Raspberry PI Laptop.  I suspect RasPi 2 would work the same as B+ since they are basically the same design except for SoC innards and non-PoP DRAM.  A+ works with back-powering if you want a really small, cheap solution and can get by with an ARM11 and 256MB DRAM.  Atrix and Droid Bionic work with no trouble.  Lapdock 100 and 500 are problematic, so look at the linked thread to see how people have worked around the issues.  It's not pretty

     

    For general Atrix Lapdock lore, see the RasPi Hardware Wiki: RPi Screens - eLinux.org

    • Cancel
    • Up 0 Down
    • Reply
    • More
    • Cancel
  • peteroakes
    peteroakes over 7 years ago in reply to johnbeetem

    The 2B+ does have decent / imporved support for small drives etc though which is a welcome upgrade, I will be testing this as soon as mine arrives as I am still concerned about crappy USB cables feeding into that tiny micro USB connector at 2 amps or more + the use of the PI itself pulling the volts below 4.75V

     

    Well see

    • Cancel
    • Up 0 Down
    • Reply