Blog Raspberry Pi laptop
  • Blog
  • Forum
  • Documents
  • Events
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Raspberry Pi requires membership for participation - click to join
Blog Post Actions
  • Subscribe by email
  • More
  • Cancel
  • Share
  • Subscribe by email
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fustini
  • Date Created: 7 Sep 2012 10:48 PM Date Created
  • Views 2246 views
  • Likes 6 likes
  • Comments 48 comments
  • rpibeginner
  • motorola
  • raspberry_pi
  • lapdock
  • rpi
  • atrix
Related
Recommended

Raspberry Pi laptop

fustini
fustini
7 Sep 2012
 Want to build this project?
View Parts

 

My last post showed how I assembled a portable Pi using a 3.5" composite LCD.  Well, I've got a better option this time around, the Motorola Atrix lapdock!

The Atrix lapdock was originally intended for Motorola's Atrix Android smartphone.  It didn't sell very well for it's original purpose, so you can pick one up for around to $50 to $100 on eBay and Amazon.  I ordered mine from eBay for $50 (shockingly my seller is now listing at $199).  It was listed as refurbished but is in great condition.  The beauty of its 11.6" HD display is a stark constrast to my 3.5" composite LCD:

I recommend checking out this insightful blog which details how to use it with the Pi: Raspberry Pi and Atrix Lapdock.  Adafruit also has a helpful video from Becky Stern on how to hack together an appropriate USB cable:

 

You don't have permission to edit metadata of this video.
Edit media
x
Upload Preview

 

However, the USB cabling described in the above blog and video is only needed for Raspberry Pi's that have F1/F2 polyfuses.  "Fresher" Pi's now have either 0-ohm resistors on F1/F2 (Model B Revision 1.0 + ECN0001) or no F1/F2 pads at all (Model B Revision 2.0).  More info on the board revisions is on the Foundation's blog.  I got a Pi from MCM Electronics last week, and it has 0-ohm resistors (labelled "000" in the upper right corner of the board):

With those polyfuses gone, the Pi can be powered via it's USB host ports as an alternative to the micro USB jack.  This is great for the Atrix lapdock as it was designed to both power the Atrix phone and connect it to USB devices over the same connected.  This means that no USB cable modifications are needed at all.  Here's my setup:

A close-up of the back of the lapdock with micro HDMI on the right and micro USB on the left:

My cables and connectors (from left to right):

  • male micro to full-size male HDMI cable
  • female to female micro HDMI coupler (little black rectangle at top)
  • female micro type B to female USB type A USB cable
  • male Type A to male Type A USB cable

I highly recommend buying an Atrix lapdock while they are still available for cheap.  Beyond the Pi, it can be used as a HDMI display for an array of other devices, too.

 

[UPDATE: check out Raspberry Pi lapdock tricks]

 

[UPDATE: I received a male Type A to male Type A adapter from Amazon and a HDMI Male to Micro HDMI Female Adapter from DealExtreme.  Along with the micro HDMI extension cable that came with my lapdock, the result is a more compact setup without long HDMI or USB cabling:


 

Cheers,

Drew

http://twitter.com/pdp7

 

 

 

Product Name*DescriptionSupplier
Raspberry Pi Model B Raspberry Pi model BRaspberry Pi
Buy Now
Pre-Programmed 4GB SD Card 4GB Class 4 SD card preloaded with Debian 6 LinuxSamsung
Buy Now
Motorola Atrix Lapdock w/included cablesSelf contained battery powered unit with display, keyboard and trackpadMotorola
HDMI Male to Micro HDMI Female AdapterMale standard HDMI to female micro HDMI adapterImported
USB A to A Male CouplerUSB type A to A male couplerDistributed By MCM
Buy Now

 

*Products and resources listed are listed to help members build their own Pi Projects. They are suggestions and listed for educational purposes. For substitutions of any parts, please post a question asking the original author.

Anonymous

Top Comments

  • Former Member
    Former Member over 9 years ago +2

    Earlier I posted a note about mounting a Pi on the back of a Lapdock with magnetic sheet. After that I set about making a much smaller and neater Pi. You can see the current result at http://www.kappa…

  • Former Member
    Former Member over 9 years ago +2

    Here's one of the images:

    http://kappa.me.uk/Raspberry_Pip/general_view.jpg

  • Former Member
    Former Member over 7 years ago +2

    I have got to thank you big time. I read the information you provided and it was very helpful! I had an Atrix 4G for quite some time and tried different methods of getting the Pi to work with it. When…

Parents
  • johnbeetem
    johnbeetem over 9 years ago

    Very nice setup!  I really don't understand why the lapdock didn't catch on.  It seem like a really nice solution.  Of course, if they were really trying to sell it for US$500 that would explain it.

     

    I've been intrigued by the Atrix Lapdock for some time, but haven't done anything about getting one mostly because I can't seem to find detailed specs anywhere.  Amazon.com (USA) has an AT&T Laptop Dock for Motorola ATRIX 4G - Retail Packaging listed for US$100, but I can't tell if it's the same thing you have.  Maybe you could check the model number 65242 and/or ASIN = B004M17D62.

     

    One detailed spec that's missing is the screen resoluton.  Would you know what it is?

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • More
    • Cancel
  • fustini
    fustini over 9 years ago in reply to johnbeetem

    Yup, that is the SKU I have: 65242.  The resolution appears to be 1366 x 768 per "xwininfo -root".  Here's some pics I just took:

     

    (also in https://picasaweb.google.com/117542001281850354871/AtrixLapdockForRaspberryPi)

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 9 years ago in reply to fustini

    Thank you -- that's very helpful.

     

    EDIT: and thank you for providing the links to accessories.  I couldn't find some of those gadgets anywhere else.  Now I just need to wait for the slow boat from China... at least I'm on the Left Coast.

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • More
    • Cancel
Comment
  • johnbeetem
    johnbeetem over 9 years ago in reply to fustini

    Thank you -- that's very helpful.

     

    EDIT: and thank you for providing the links to accessories.  I couldn't find some of those gadgets anywhere else.  Now I just need to wait for the slow boat from China... at least I'm on the Left Coast.

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • More
    • Cancel
Children
No Data