Blog Raspberry Pi speaks 1-wire with Adafruit's Occidentalis image
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fustini
  • Date Created: 8 Aug 2012 5:45 PM Date Created
  • Views 3637 views
  • Likes 0 likes
  • Comments 14 comments
Related
Recommended
  • ladyada
  • raspberry_pi
  • 1wire
  • raspberrypi
  • adafruit

Raspberry Pi speaks 1-wire with Adafruit's Occidentalis image

fustini
fustini
8 Aug 2012

Adafruit recently released their own Raspberry Pi image, Occidentalis v0.1:

http://learn.adafruit.com/system/assets/assets/000/001/532/medium800/occidentalis.png?1343962191

This is our first distro,  Occidentalis v0.1. Rubus occidentalis is the black raspberry.  It is derived from Raspbian Wheezy July 15


We have made a few key changes to make it more hardware-hacker friendly!

  • Updated to Hexxeh firmware
  • 4 Gig SD image (will not fit in 2 G cards!)
  • I2C and hardware SPI support
  • I2C/SPI modules initialized on boot
  • sshd on boot
  • ssh keygen on first boot
  • runs ahavi daemon (Bonjour client) and is called raspberrypi.local
  • Realtek RTL8188CUS wifi support
  • One wire support on GPIO #4 when loaded

 

I thought that looked like a nice list of improvements.  I'd already been using I2C with bootc.net's image, but the new 1-wire support piqued my interest.  I downloaded & flashed the Occidentalis image onto a SD card and then booted up:

image

The login is the usual pi/raspberry.  Before I tested out 1-wire, I thought I would check to see if my Asus USB-N13 was supported as Adafruit compiled the driver it needs, rtl8192cu, into the kernel in their image.  To my delight, the USB-N13 was immediately recognized (unlike with the "regular" Raspbian Wheezy image):

image

Alright, on to some electronics!  The Occidentalis page states about 1-wire:

One wire is most commonly used for DS18B20 temp sensors. The Pi does not have 'hardware' 1-wire support but it can bitbang it with some success.

The page also highlights the commit that makes it possible:

 

Dallas one wire interface with the Linux w1 GPIO bitbanging implementation on GPIO 4

 

I already had the DS18B20 temperature sensors, so I just hooked it up as the page described:

Connect a DS18B20 with VCC to 3V, ground to ground and Data to GPIO #4. Then connect a 4.7K resistor from Data to VCC.

image

(note: I'm using the Adafruit Pi Plate on top of Raspberry Pi to make the connections; FTDI cable for serial console is also pictured)

 

I continued to follow the documentation:

Then run as root: modprobe w1-gpio and then modprobe w1-therm to attach the temperature submodule. Then you can run cat /sys/bus/w1/devices/28-*/w1_slave to read the temperature data from the bus


The first line has the CRC, if its "NO" then the data is corrupted. If you get a good CRC check, the second line has t=temperature in 1/100 of a degree Centigrade. For example, below, the temperature is 24.5°C


Since 1-wire is bitbanged, its flakier than SPI or I2C.  We do not have any 1-wire tutorials for the RPi at this time

Here is a screenshot of my results:

image

The temperature value was 34000 which I believe would mean 34 C or 93 F.  This seems hotter than it actually was, so I'm planning to verify the results with the I2C TMP102 temp sensor next to the DS18B20.

 

Cheers,

Drew

  • Sign in to reply

Top Comments

  • morgaine
    morgaine over 13 years ago +1
    It was very interesting for me to see your article Drew, as I've had a soft spot for 1-Wire and iButtons since the early 90's and have lots of such devices here, mostly early serial number and storage…
Parents
  • daloele
    daloele over 13 years ago

    Anyone interested in 1-wire ought to be aware of owfs, a long-running project supporting 1-wire networks. People have reported running it on a raspberry pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fustini
    fustini over 13 years ago in reply to daloele

    Yeah, I kinda of remember that from when I used to have a 1-wire temp sensors in a server room hooked up to a Linux server.  This 1-wire support I'm describing above is just bit-banged so maybe not the most robust solution (good for a single DS18B20 for simple temp sensing though).  This site posted about what's probably a more "proper" solution of interfacing 1-wire to the Pi by using 1-wire bus ICs: http://raspberrypi.homelabs.org.uk/category/1-wire/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fustini
    fustini over 13 years ago in reply to daloele

    Yeah, I kinda of remember that from when I used to have a 1-wire temp sensors in a server room hooked up to a Linux server.  This 1-wire support I'm describing above is just bit-banged so maybe not the most robust solution (good for a single DS18B20 for simple temp sensing though).  This site posted about what's probably a more "proper" solution of interfacing 1-wire to the Pi by using 1-wire bus ICs: http://raspberrypi.homelabs.org.uk/category/1-wire/
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.