Blog The Road to Raspberry Pi4B/ PoE Hat RoadTest Review (comparison Pi3B+)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: colporteur
  • Date Created: 19 Apr 2020 12:47 AM Date Created
  • Views 2450 views
  • Likes 5 likes
  • Comments 6 comments
Related
Recommended

The Road to Raspberry Pi4B/ PoE Hat RoadTest Review (comparison Pi3B+)

colporteur
colporteur
19 Apr 2020

While in a holding pattern, waiting for power supply deliveries for both the PoE and Pi4B, I started some parallel work that was proposed in the RoadTest application. Since the specification indicated the PoE Hat was compatible with the Pi3B+, I figure I could start laying out a RoadTest Review framework using the Pi3B+. When the Pi4B is ready I will run the same tests.

 

Some observation were discovered while Installing the PoEHat on the Pi3B+.

  • Raised heat sinks on a Pi may conflict for space. The heat sink (purple ellipse) had to be installed off center of the chip, in order to leave sufficient clearance for the PoE Hat transformer. Moving the heat sink to the left put it dangerously close to an SMD component (green ellipse) on the Pi motherboard. To alleviate both issues the heat sink is installed shifted down and to the left, resulting in it not completely covering the chip.

 

image

  • The PoEHat completely consumes all the GPIO pins leaving them in accessible. The GPIO pins (red ellipse) are not long enough to extend through the PoEHat.

image

I have ordered (MORE SHIPPING COSTS!) a stacking header to extend the pins on the Pi. I'm not confident the existing space is sufficient for this to work. The plan to load up the Pi with a LED array detailed in The Road to Raspberry Pi4B/ PoE Hat RoadTest Review (Testing) will not be possible if the GPIO pin cannot be extended. Let's see what the stacking header does.

image

 

  • PoEHat and Pi3B+ combination exceeds the size of a standard case.

image

I carved a hole in a plastic case I had available to enable the paired assembly to fit.

 

Let's test:

With the PoEHat installed and a new SD card loaded with a current Raspbian image I used a Pi power supply to fire up the combo. Wait, can you run a Pi with a PoE Hat using the Pi power supply? A look at the documentation on the raspberrypi.org site for the PoE Hat wasn't helpful. The documentation is more of a travel brochure with pretty picture than a manual that has useful information.

 

Truth be told, Yes Dorothy you can run a PoEHat'd Pi with a local power supply! Well it did in this example. I would assume the answer to the question you would find in the documentation. Not the case.

 

With a working Pi3B+ & PoEHat combo a stress test was used to establish a load on the devices. I followed the instructions provided in this link https://core-electronics.com.au/tutorials/stress-testing-your-raspberry-pi.html to establish a load and take measurements.

image

On the left there is a terminal output with the stress application running along with an htop output displayed on the bottom. On the right wthere is the terminal output of cpuburn application running along with an htop output displayed on the bottom. Both tests drive the CPU's, the cpuburn application claim to fame is to really heat up the CPU's. The test setup and performance matched what was in the documentation. There was some concern about the link be relevant because of date but that didn't prove to be a problem.

 

Discovery:

  1. PoE Hat fan turns on at when the screen displays a temperature of approximately 50 Degrees Celsius.
  2. The video in the link suggested the fan sound changed as cpuburn was engaged indicating an increased load on the power supply. The power supply voltage on GPIO pin 2, drop from 5.11 to 4.78-4.83 volts DC when the cpuburn test was running.

 

The voltage change using the cpuburn test makes it an ideal application to use for further testing as described in The Road to Raspberry Pi4B/ PoE Hat RoadTest Review (Testing) . It provides a setup that will put a strain on the PoE Hat power. I especially want to do this when the combo is attached to a maximum length of CAT 5.

 

I'm limited on further testing that can be performed at the moment, while I await parts delivery. This initial round of tests using a Pi3B+ has definitely provided some insights that will prove useful going forward. My updated plan is to confirm if the discoveries that were made using a Pi3B+ exist in the Pi4B. I will use the official RoadTest Review posting to document those findings.

  • Sign in to reply
Parents
  • mp2100
    mp2100 over 5 years ago

    Very useful information Sean, things that I would have expected to be in the documentation.  The idea of the PoE hat always sounded good, but as with so many upgrades, there's often a lot of "fiddling" with things physically to get it to work the way you want it to.  The dual-powering item is an important one.  It would be good to know that the PoE hat works nicely with the normal power supply, switching safely between the two choices.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 5 years ago in reply to mp2100

    My application pitch, indicated I had little knowledge in the field of PoE. For that reason the RoadTest would motivate me to learn. What I wanted to uncover was the practical aspects of PoE. What does the layman need to know if they are thinking of using PoE on the Pi.

     

    I plan to construct my own cables as well as use a variety of commercial cables. So far I've learned the PoE HAT & Pi combo eliminates the use of standard cases and things like the placement of heat sink on the Pi matter, if you want the Hat to fit. As it stands the Pi GPIO pins are unusable. I am hoping to resolve this with a header but I don't thing there is sufficient room. I would like to know I can't use GPIO pins with this Hat wouldn't you.

     

    My goal is to pull the lessons learned from experimenting with device into a compendium of deploying PoE Hat. Thank you for your kind words.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • stevesmythe
    stevesmythe over 5 years ago in reply to colporteur

    You can certainly use the GPIO pins if you get the right stacking header (which it looks like you will have), but you will also need an additional (standard) header for the four PoE pins otherwise you'll have no power!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • stevesmythe
    stevesmythe over 5 years ago in reply to stevesmythe

    Product LinkProduct Link

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 5 years ago in reply to stevesmythe

    Thanks for the heads up. I have a board picture of the PoE header difference between Pi3B, Pi3B+ and Pi4B I'm going to use in the RoadTest post. I actually ordered extra 40 pin headers thinking I can carve up in order to get the PoE header.

     

    The PoE Hat documentation doesn't indicate any limitations on GPIO. I see this as a short coming. An "Hey folks you can't use the GPIO pins with our board" would have been nice or a caveat if you plan on using the GPIO pin, why not include the header. This causes me to question can the GPIO pins actually be used? It is a question I hope to answer. My plan is to connect an LED to every GPIO using a cable and external board. Only if my header solutions come through in the end.

     

    You confidence that the header appears to be correct may be misplaced. The gap left after I sandwich the Pi & PoE Hat doesn't appear to be large enough to accommodate the header. I'm thinking I may need to replace the standoffs with a longer version to create the necessary space.

     

    These are all details I rather enjoy finding out about so they can be shared.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • stevesmythe
    stevesmythe over 5 years ago in reply to colporteur

    Yes, obviously you will need longer standoffs. 15mm instead of the 9mm ones provided. I say "need" because electrically you don't need then, but mechanically it is advisable depending on your application/casing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • stevesmythe
    stevesmythe over 5 years ago in reply to colporteur

    Yes, obviously you will need longer standoffs. 15mm instead of the 9mm ones provided. I say "need" because electrically you don't need then, but mechanically it is advisable depending on your application/casing.
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.