<?xml-stylesheet type="text/xsl" href="https://community.element14.com/cfs-file/__key/system/syndication/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:slash="http://purl.org/rss/1.0/modules/slash/" xmlns:wfw="http://wellformedweb.org/CommentAPI/"><channel><title>P42 Pico M.2: A RPI Pico RP2040 board in new form factor.</title><link>/products/raspberry-pi/b/blog/posts/p42-pico-m-2-a-rpi-pico-rp2040-board-in-new-form-factor</link><description>So, after carrying this idea around since October last year, I finally got my act together and designed/built my RPI Pico RP2040 M.2 dev-board. It is a M.2 2230 card with A and E key and has as many communication interfaces to the M.2 side as possibl</description><dc:language>en-US</dc:language><generator>Telligent Community 12</generator><item><title>RE: P42 Pico M.2: A RPI Pico RP2040 board in new form factor.</title><link>https://community.element14.com/products/raspberry-pi/b/blog/posts/p42-pico-m-2-a-rpi-pico-rp2040-board-in-new-form-factor</link><pubDate>Thu, 07 Nov 2024 02:53:57 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:56460b29-fa5b-497c-b666-f32a2c1bc30d</guid><dc:creator>wolfgangfriedrich</dc:creator><slash:comments>1</slash:comments><description>&lt;p&gt;As it happens too often, this revision 1 board has its issues. With my RadXA ROCK 3A SBC not arrived yet, I was going for the fly-wire test approach.&lt;/p&gt;
&lt;p&gt;&lt;a href="data:image/gif;base64,R0lGODlhAQABAIAAAP///wAAACH5BAEAAAAALAAAAAABAAEAAAICRAEAOw==" target="_blank" data-e14adj="t"&gt;&lt;img src="/resized-image/__size/1280x720/__key/commentfiles/f7d226abd59f475c9d224a79e3f0ec07-56460b29-fa5b-497c-b666-f32a2c1bc30d/pastedimage1730947910846v1.png" alt=" " /&gt;&lt;/a&gt;&lt;a href="data:image/gif;base64,R0lGODlhAQABAIAAAP///wAAACH5BAEAAAAALAAAAAABAAEAAAICRAEAOw==" target="_blank" data-e14adj="t"&gt;&lt;img src="/resized-image/__size/1280x720/__key/commentfiles/f7d226abd59f475c9d224a79e3f0ec07-56460b29-fa5b-497c-b666-f32a2c1bc30d/pastedimage1730947910846v2.png" alt=" " /&gt;&lt;/a&gt;&lt;/p&gt;
&lt;p&gt;USB and power through an external 3.3 V regulator are working flawlessly. Power LEDs are on and the user LED is blinking away. Nice! UART on the m.2 and on GPIOs are doing simple loopback and the USB/UART is running a simple command line already.&lt;/p&gt;
&lt;p&gt;Things that did not work out of the box: I2C (of course). I should pay more attention to the pin mapping. I cannot use I2C1 at the same time on the m.2 and the QWIIC connector. Also pin4 on the QWIIC is SCL, not SDA. Nothing a few cuts and wires cannot fix. Now I have a loop-back from the m.2 end to the QWIIC connector. One port is master, one is slave. Mint. &lt;br /&gt;More wires will be required to test the uSD card, the SPI signals are connected up-sidedown to the SPI port on the RP2040. Pin mapping again! I blame this one on the schematic symbol, not showing all pin functions.&amp;nbsp;&lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=28255&amp;AppID=86&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item><item><title>RE: P42 Pico M.2: A RPI Pico RP2040 board in new form factor.</title><link>https://community.element14.com/products/raspberry-pi/b/blog/posts/p42-pico-m-2-a-rpi-pico-rp2040-board-in-new-form-factor</link><pubDate>Thu, 15 Aug 2024 00:46:36 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:56460b29-fa5b-497c-b666-f32a2c1bc30d</guid><dc:creator>wolfgangfriedrich</dc:creator><slash:comments>1</slash:comments><description>&lt;p&gt;I managed to solder pin headers to the castellated holes, but only barely. Had to use a lot of hot glue to hold the header in place and still managed to rip off one pad &lt;img src="/resized-image/__size/40x40/__key/commentfiles/f7d226abd59f475c9d224a79e3f0ec07-56460b29-fa5b-497c-b666-f32a2c1bc30d/pastedimage1723682712130v1.png" alt=" " /&gt; .&lt;br /&gt; Real holes would work much better, I give this idea a -1 out of 10. Would not recommend.&lt;br /&gt; Even better is probably adding wires and have the pin headers somewhat strain-relieved from the 0.8mm PCB.&lt;/p&gt;
&lt;p&gt;&lt;img src="/resized-image/__size/1280x720/__key/commentfiles/f7d226abd59f475c9d224a79e3f0ec07-56460b29-fa5b-497c-b666-f32a2c1bc30d/pastedimage1723682725502v2.jpeg" alt=" " /&gt;&lt;/p&gt;
&lt;p&gt;&lt;img src="/resized-image/__size/1280x720/__key/commentfiles/f7d226abd59f475c9d224a79e3f0ec07-56460b29-fa5b-497c-b666-f32a2c1bc30d/pastedimage1723682743239v3.jpeg" alt=" " /&gt;&lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=28255&amp;AppID=86&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item><item><title>RE: P42 Pico M.2: A RPI Pico RP2040 board in new form factor.</title><link>https://community.element14.com/products/raspberry-pi/b/blog/posts/p42-pico-m-2-a-rpi-pico-rp2040-board-in-new-form-factor</link><pubDate>Sun, 11 Aug 2024 00:56:21 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:56460b29-fa5b-497c-b666-f32a2c1bc30d</guid><dc:creator>shabaz</dc:creator><slash:comments>1</slash:comments><description>&lt;p&gt;Hi Wolfgang,&lt;/p&gt;
&lt;p&gt;Very interesting board! And great to see there&amp;#39;s space for plenty of storage with the micro SD too!&lt;/p&gt;
&lt;p&gt;Regarding castellated pins, I think it works on your board, because it&amp;#39;s so small there are no through-hole pins. In that case, people can still use normal pin headers, and simply solder to the sides.&lt;/p&gt;
&lt;p&gt;I recently saw a different module (not related to Pico) where they did a slightly similar thing, having castellated pads since they had no space for through-hole option, and then also containing a flat flex connector (instead of the edge connector since it wasn&amp;#39;t an M.2 module), so that users could chose either option.&lt;/p&gt;
&lt;p&gt;Nice idea with the &amp;#39;poor-mans castellated connections&amp;#39;, I can imagine for sure they will be very welcome when prototyping, even if they are slightly more difficult to solder to.&lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=28255&amp;AppID=86&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item></channel></rss>