Hi, I am trying to connect the PM4222-09 stepper motor I have to gertboard motor controller.
Can anyone help me with this? The motor has 6 wires (red is common) and it is a unipolar 12VDC-24VDC 4PH. I appreciate you help.
Hi, I am trying to connect the PM4222-09 stepper motor I have to gertboard motor controller.
Can anyone help me with this? The motor has 6 wires (red is common) and it is a unipolar 12VDC-24VDC 4PH. I appreciate you help.
You can't connect it to the Gertboard's motor controller. A stepper motor needs, depending on the type, more then one driver.
Your stepper motor,(I just downloaded a datasheet) needs either two full bridges or 4 hal bridges or 4 open-collector drivers,
The gertboard has 6 open collector drivers but the current requirements of your stepper motor (0.24A) are at the
absolute limit of what the ULN2803A can handle. So you have the risk of damaging it.
-- Gert
Thank you very much for you answer. I have a Raspberry Pi that the gertboard connects to. What will be the best stepper motor to connect to the motor controller on the gertboard, in order to test a python script for the motor? I am connecting to my raspberry pi remotely from my computer. Thank you very much for your help.
Oh yeah I'm same opinion.
If it is just for trying, you can put a series resistor in the wires. That will limit the current but your stepper motor will PROBABLY still work (but will have less force/strength)
You may have to try several values, to see which one works, in the range of 80-20 ohms. (About 0.5W..1W)
Just, belatedly, for the record (and for beginners like me): I used a 5V stepper motor (28BYJ-48) via the Gertboard, using 4 of the built-in OCD channels, the 5V supply on the board, and the instructions on the Adafruit website (which uses the same IC), and it worked perfectly first time.