Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum AEC / DSP code on Wolfson audio card for Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 676 subscribers
  • Views 2413 views
  • Users 0 members are here
  • wolfson
  • raspberry
  • pi
  • aec
  • raspberry_pi
  • raspeberry_pi_accessories
Related

AEC / DSP code on Wolfson audio card for Pi

Former Member
Former Member over 11 years ago

I have successfully compiled the Kernel and have the Wolfson audio card for Pi up and running. Took some time but I am quite happy with the audio quality.

 

Now, I would like to use the WM5102 with acoustic echo cancellation. According to the data sheet this can be enabled. Page 156, in the WM5102 documentation says:

"The WM5102 incorporates loopback signal path, which is ideally suited as a reference for Acoustic Echo Cancellation (AEC) processing. Any of the output signal paths may be selected as the AEC loopback source. When configured with suitable DSP firmware, the WM5102 can provide an integrated AEC capability."

 

My question is, does anyone know where "suitable DSP firmware" can be found and where/how it is possible to write code for the DSP?

 

I assume page 108 in the data sheet is a hint on that this must be licensed separately , it says:

"Note that the WISCETM evaluation board control software provides support for easy loading of Program, Coefficient and Data content onto the WM5102. Please contact your local Wolfson representative for more details of the WISCETM evaluation board control software."

 

Best Regards,

Joacim

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    Hi,

    I found a half solution for your problem.

    "Please contact your local Wolfson representative for more details of the WISCE evaluation board control software."

    You can download this WISCE software.

    And the evaluation software WM5102EV1M.

    Link: http://www.wolfsonmicro.com/support/wisce/

     

    With this software you can configure the whole DSP very easy.

    Then you can generate a C code.

     

    BUT I don't know how does the code comes the board. Normally is the board connected with USB, I2C or SPI.

    The problem is the connection between the board and the PC.

     

    I've already written to this forum, a better description of the problems can be found here:

    Link: Configure the DSP with WISCE

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Marki555
    0 Marki555 over 11 years ago in reply to Former Member

    I have tried the WISCE software and it only allows you to configure the EQ and LHPF filters and to generate their coefficients.

    For the DSP it only allows you to upload a binary microcode. But that is done very easily just by writing to the WM5102 registers (either via the driver and SPI, or via i2c on the expansion header). Then you can route any signal though the DSP. The AEC loopback is only another signal path, which can route signal from any output back to the digital core (DSP, or EQ, ...)

    The DSP comes empty (without any code) on the Wolfson card. I guess Wolfson sells some ready DSP microcodes (like AEC or wind/noise suppression), but you can program them yourself. However I don't know if the Programming Guide is available anywhere.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Marki555

    Marki555

    Sorry, I don't understand really...

    How could you load the binary microcode from the Wisce to the Soundcard ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to Marki555

    Marki555

    Sorry, I don't understand really...

    How could you load the binary microcode from the Wisce to the Soundcard ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Marki555
    0 Marki555 over 11 years ago in reply to Former Member

    You don't need WISCE to load the DSP microcode. WISCE just helps you during development to load it repeately, but WISCE alone cannot develop the DSP microcode.

     

    If you have the microcode (we don't have it and don't know how to get/develop it), you just write it to the WM5102 registers either via SPI or I2C. That is as simple as writing to other I2C devices like temperature sensors. No rocket science in this part image