Raspberry Pi Forum Raspiberry pi Camera module ERROR - mmal: mmal_vc_component_enable: failed to enable component: ENOSPC
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 677 subscribers
  • Views 10061 views
  • Users 0 members are here
  • raspberry
  • pi
  • enspc
  • camera
Related

Raspiberry pi Camera module ERROR - mmal: mmal_vc_component_enable: failed to enable component: ENOSPC

will.mendil
will.mendil over 11 years ago

Hi,

 

I don't know if this is the best place to ask this kind of question, but I am following tbhs' directives. I need help with the raspberry pi camera. I have been looking all other google for help but nothing seems to work although a lot of people seem to meet the same problem.

 

I basically intent to use a raspberry pi camera ask a surveillance camera but I cannot seem to get it to work on the last version of raspbian 3.12.28.

Whenever I type

 

raspistill -v

 

I get this response

 

 

raspistill Camera App v1.3.8

Width 2592, Height 1944, quality 85, filename image.jpg
Time delay 5000, Raw no
Thumbnail enabled Yes, width 64, height 48, quality 35
Link to latest frame enabled  no
Full resolution preview No
Capture method : Single capture

Preview Yes, Full screen Yes
Preview window 0,0,1024,768
Opacity 255
Sharpness 0, Contrast 0, Brightness 50
Saturation 0, ISO 0, Video Stabilisation No, Exposure compensation 0
Exposure Mode 'auto', AWB Mode 'auto', Image Effect 'none'
Metering Mode 'average', Colour Effect Enabled No with U = 128, V = 128
Rotation 0, hflip No, vflip No
ROI x 0.000000, y 0.000000, w 1.000000 h 1.000000
mmal: mmal_vc_component_enable: failed to enable component: ENOSPC
mmal: camera component couldn't be enabled
mmal: main: Failed to create camera component
mmal: Failed to run camera app. Please check for firmware updates

 

I tried changing the /etc/modules but nothing seems to work, I tried changing /etc/modprobe.d/raspi_blacklist.conf etc... nothing.

 

I read somewhere that downdating the version of raspberry pi worked so I did so

 

sudo rpi-update 8234d5148aded657760e9ecd622f324d140ae89

 

then raspistill works but I get another error that prevents me from using motion or RPi_Web_cam_interface. The error displays right at the beginning

 

raspberrypi login : Error: Could not set annotation

 

and persists if I use RPi_Web_Interface. This error does not seem to be in any forum.

 

I'm pretty upset of having bought the module if it does not work at all...

 

Anyway if anyone has any idea on what I could do to get it to work, I would be very grateful

 

Cheers

 

Will

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 11 years ago

    I think the problem is likely that you have not set camera support to 'on' using "sudo raspi-config". Without this, I get similar (but not identical) errors.


    All works fine with the latest Raspian  as obtained using:

    sudo apt-get update

    sudo apt-get dist-upgrade


    If I DISABLE camera support I get:

     

    <<Early Parts Deleted>>

    mmal: mmal_vc_component_create: failed to create component 'vc.ril.camera' (1:ENOMEM)

    mmal: mmal_component_create_core: could not create component 'vc.ril.camera' (1)

    mmal: Failed to create camera component

    mmal: main: Failed to create camera component

    mmal: Camera is not enabled in this build. Try running "sudo raspi-config" and ensure that "camera" has been enabled

     

    But if I ENABLE camera support I get the following, with a preview picture on the monitor for several seconds as it runs:

     

    <<Early Parts Deleted>>

    Camera component done

    Encoder component done

    Starting component connection stage

    Connecting camera preview port to video render.

    Connecting camera stills port to encoder input port

    Closing down

    Close down completed, all components disconnected, disabled and destroyed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Now to go back on my own post ... that's not what this is at all!

     

    The error message is the one that is created when 2 processes try to access the camera module simultaneously (ie, 2nd  one starts before 1st has COMPLETELY ended).

     

    I can suimulate that by entering at the command prompt in quick succession:

    raspistill -v &

    raspistill -v

     

    This gives the following output (the 2 sets mixed together .. but see the error messages. I've tried to distinguish the 2 mixed up output streams using Italics

     

    pi@Pi-3 ~ $ raspistill -v &

    [1] 5943

    pi@Pi-3 ~ $

    raspistill Camera App v1.3.8

    Width 2592, Height 1944, quality 85, filename (null)

    Time delay 5000, Raw no

    Thumbnail enabled Yes, width 64, height 48, quality 35

    Link to latest frame enabled  no

    Full resolution preview No

    Capture method : Single capture

    Preview Yes, Full screen Yes

    Preview window 0,0,1024,768

    Opacity 255

    Sharpness 0, Contrast 0, Brightness 50

    Saturation 0, ISO 0, Video Stabilisation No, Exposure compensation 0

    Exposure Mode 'auto', AWB Mode 'auto', Image Effect 'none'

    Metering Mode 'average', Colour Effect Enabled No with U = 128, V = 128

    Rotation 0, hflip No, vflip No

    ROI x 0.000000, y 0.000000, w 1.000000 h 1.000000

    raspistill -v &

    [2] 5949

    pi@Pi-3 ~ $

    raspistill Camera App v1.3.8

    Width 2592, Height 1944, quality 85, filename (null)

    Time delay 5000, Raw no

    Thumbnail enabled Yes, width 64, height 48, quality 35

    Link to latest frame enabled  no

    Full resolution preview No

    Capture method : Single capture

    Preview Yes, Full screen Yes

    Preview window 0,0,1024,768

    Opacity 255

    Sharpness 0, Contrast 0, Brightness 50

    Saturation 0, ISO 0, Video Stabilisation No, Exposure compensation 0

    Exposure Mode 'auto', AWB Mode 'auto', Image Effect 'none'

    Metering Mode 'average', Colour Effect Enabled No with U = 128, V = 128

    Rotation 0, hflip No, vflip No

    ROI x 0.000000, y 0.000000, w 1.000000 h 1.000000

    Camera component done

    mmal: mmal_vc_component_enable: failed to enable component: ENOSPC

    mmal: Encoder component done

    Starting component connection stage

    Connecting camera preview port to video render.

    camera component couldn't be enabled

    mmal: main: Failed to create camera component

    mmal: Failed to run camera app. Please check for firmware updates

    Connecting camera stills port to encoder input port

    Closing down

    Close down completed, all components disconnected, disabled and destroyed

     

    So have you got something else running that is using the camera? Either deliberately, or something that has not closed down properly?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hanif99
    0 hanif99 over 4 years ago

    Hello brother, finally i can solve this problem after a lot of hours troubleshooting.

     

    I already share it in my YouTube (https://youtu.be/on8UlkRvLok)

     

    This problem only occur in camera raspberry pi V2.1 (IMX219) from Element14. But in camera raspberry pi V2.1 from OKdo, i don't get this error

     

    So, the solution when error

    "mmal: mmal_vc_component_enable: failed to enable component: ENOSPC

    mmal: camera component couldn't be enabled

    mmal: main: Failed to create camera component

    mmal: Failed to run camera app. Please check for firmware updates"

     

    You need some initialization with a works camera (me camera from OKdo).

    So, the step is

    1. Plug your works camera to Raspberry Pi (me using Raspberry Pi 4B)

    2. Turn on your Raspberry Pi

    3. check

    Code: Select all

    vcgencmd get_camera

    to make sure your hardware is detected the camera

    4. capture image using

    Code: Select all

    raspistill -v

    and camera will capture the image

    5. Then replace the works camera with ENOSPC Error Camera (from Element14)

    6. then try to capture the image

    Code: Select all

    raspistill -v

    and the ENOSPC Error will not occur

     

    Notes:
    - But, after the ENOSPC Error Camera works, and then you restart/shutdown the raspberry pi, the error will occur again :(

     

    OS Raspberry Pi 4 Model B (4GB)

    - Linux raspberrypi 5.10.60-v7l+ #1449 SMP Wed Aug 25 15:00:44 BST 2021 armv7l GNU/Linux