Raspberry Pi Forum Raspberry Pi Pico 2 MicroPython problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 669 subscribers
  • Views 2847 views
  • Users 0 members are here
  • coding
  • graphics
  • pico 2
  • micropython
  • .uf2
Related

Raspberry Pi Pico 2 MicroPython problem

tonygo
tonygo over 1 year ago

I've got hold of the new Pico 2 and have tried a graphics program to make use of the extra memory. I'm using a Waveshare 2" Pico display with 320 by 240 pixels and the latest available MicroPython uf2 (v1.24.0-preview.201.g269a0e0e1 (2024-08-09) .uf2) and have hit a snag. The Waveshare display driver is included in the code and works perfectly.

To get this loop to terminate I have to include an 'unnecessary' print statement.

for i in range(r, 0, -1):
    print(i) # <==================== WHY IS THIS NEEDED? ==================
    LCD.ellipse(centre_x, centre_y,i+1, i+1,colour(i*5,i*3,i*4), 1)
    LCD.show()
    time.sleep(0.1)
    

If I leave it out the Pico 2 locks up at the end of the loop and if I click on the STOP icon in Thonny I get the message:


Unable to connect to COM3: could not open port 'COM3': PermissionError(13, 'Access is denied.', None, 5)

If you have serial connection to the device from another program, then disconnect it there first.

Process ended with exit code 1.


If I include the print statement it runs through to the following code as expected.

The full code can be found here:
https://pastebin.com/Fmk5iQ18

I wonder what is going on.

I know this is a 'preview' version of the UF2 but I was not expecting a problem with a counted for loop! Any ideas?
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.