Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 4 GPIO Leakage Voltage (1.2V) When LOW on Relay Module
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 699 subscribers
  • Views 692 views
  • Users 0 members are here
Related

Raspberry Pi 4 GPIO Leakage Voltage (1.2V) When LOW on Relay Module

emreeyy
emreeyy 1 month ago

Hi everyone,

I am using a Raspberry Pi 4 Model B to control industrial 24V relay modules. However, I am not using an external 24V power supply; instead, I am routing the Pi's own 3.3V pin to the common power rail of the relays to use them as simple mechanical switches for 3.3V signals.

I have wired the Raspberry Pi GPIO pins directly to the relay signal inputs via a simple terminal block breakout board (no transistors or optocouplers are used yet).

The Problem:

 When the GPIO pin is ⁠HIGH⁠, I read exactly 3.3V on the line, which is correct.

 When the GPIO pin is set to ⁠LOW⁠, instead of 0V, I see a constant 1.2V leakage/floating voltage on the multimeter.

There is currently no common ground (GND) connection between the Raspberry Pi and the panel's internal structure. I suspect this 1.2V is due to a floating ground issue or feedback leakage through the relay's internal coil/status LED.

What is the best way to eliminate this 1.2V leakage and get a clean 0V when the pin is LOW? Should I use an optocoupler module (like PC817) or a transistor driver?

Thanks in advance!

  • Sign in to reply
  • Cancel
Parents
  • geralds
    0 geralds 1 month ago
    emreeyy said:

    Wenn der GPIO-Pin HOCH ist, messe ich genau 3,3 V auf der Leitung, was korrekt ist.

    Wenn der GPIO-Pin auf LOW statt 0V eingestellt ist, sehe ich eine konstante 1,2V-Leck-/Schwimmenspannung am Multimeter.

    Look here: https://www.raspberrypi.com/documentation/computers/raspberry-pi.html#gpio-pads-control

    most of the port pin are tri-stated pins.

    Yes, it means that the pin can have 1.2V - the middle of the supply voltage as well as meaning this state is in "high-Z".

    This is NOT a "leakage".  Wink

    Z = Impedance in (k)Ohm.

    This function is a very important function if you want to use that pins with different jobs.

    Such port can be driven in: "switched on" (sending high to the output), "h-Z" (the software let the port "swimming"), "switched-off (sending low to the output)

    Gerald
    ---

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • geralds
    0 geralds 1 month ago
    emreeyy said:

    Wenn der GPIO-Pin HOCH ist, messe ich genau 3,3 V auf der Leitung, was korrekt ist.

    Wenn der GPIO-Pin auf LOW statt 0V eingestellt ist, sehe ich eine konstante 1,2V-Leck-/Schwimmenspannung am Multimeter.

    Look here: https://www.raspberrypi.com/documentation/computers/raspberry-pi.html#gpio-pads-control

    most of the port pin are tri-stated pins.

    Yes, it means that the pin can have 1.2V - the middle of the supply voltage as well as meaning this state is in "high-Z".

    This is NOT a "leakage".  Wink

    Z = Impedance in (k)Ohm.

    This function is a very important function if you want to use that pins with different jobs.

    Such port can be driven in: "switched on" (sending high to the output), "h-Z" (the software let the port "swimming"), "switched-off (sending low to the output)

    Gerald
    ---