• Helmet mounted HUD design

    I am currently working on a project that uses a helmet mounted HUD which will show a camera view with overlays for health percentage, GPS map location, shield percentage and target markers using the raspberry pi 2 like the HUD's in video games for use…

  • Wireless Raspberry Pi camera

    Is there any way i can connect the raspberry pi camera wirelessly to the pi? I know that there is a ribbon connector but it is coming out to be short in length for my project. Is there any ready made circuit available in the market that would make my…

  • Can a Rasbery motherbord control many cameras in a house? How to emplement?

    Can a Rasbery motherbord control many cameras in a house? How to emplement?

  • controlling 6+ motors with the raspberry pi?

    I'm looking to make a robot with my raspberry pi model B and have been researching controlling motors.

    I need something cool to show off at an upcoming Comp Sci career fair at my school.

     

     

    So far all of the boards I have looked at only easily allow the…

  • Pi Camera CCD

    I Was thinking about a project idea and wondered how long I could continuously (for video or long exposure) run the camera module without overhearing the CCD.

     

    Does anyone know or done any experimenting with this?

  • I Need Help connecting an adafruit touchscreen to my pi B+

    I am building a PiPhone and can't figure out what cable will connect my adafruit touchscreen to my raspberry pi B+.  Please help me!!!! @Pi

  • Camera screen as a mini monitor for a RPi?

    I was wondering if anyone knows how to convert a 3" LCD display from an Insignia NS-DCC5HB09 camcorder so that it can be used with a Raspberry Pi. I'm new to electronics, so it would be very helpful to get some suggestions.

  • Raspiberry pi Camera module ERROR - mmal: mmal_vc_component_enable: failed to enable component: ENOSPC

    Hi,

     

    I don't know if this is the best place to ask this kind of question, but I am following tbhs' directives. I need help with the raspberry pi camera. I have been looking all other google for help but nothing seems to work although a lot of people seem…

  • Raspiberry pi Camera module ERROR - mmal: mmal_vc_component_enable: failed to enable component: ENOSPC

    Hi,

     

    I don't know if this is the best place to ask this kind of question, but I am following tbhs' directives. I need help with the raspberry pi camera. I have been looking all other google for help but nothing seems to work although a lot of people seem…

  • Raspberry Pi Camera not working (v3.12.28) - mmal: mmal_vc_component_enable: failed to enable component: ENOSPC

    Hi,

     

    I don't know if this is the best place to ask this kind of question, but I am following tbhs' directives. I need help with the raspberry pi camera. I have been looking all other google for help but nothing seems to work altough a lot of people seem…

  • Raspberry pi camera

    I have got a raspberry pi camera and know the command line code but not how to activate it by using python. I would use this to have when you press a button it take a picture of who pressed the button. Please help!!!

  • Raspberry Pi Speed Camera

    Is there anyone out there that has built a speed camera using a Raspberry Pi, I would love to build one that includes a speed display for on coming cars to see as they speed passed my house.  I have no idea how to start but I have a Raspberry Pi and no…

  • Raspberry Pi Android Smart Phone with GPIO

    I'm pretty new to Raspberry Pi and seen some really intresting things you can do with it via The Ben Heck Show.  I was wondering if there is any development out there to make it in to some sort of SIM compatable (preferbally on T-Mobile's Network)…

  • Interface old laptop camera with RasPi

    Hey guys,

     

    I have recently salvaged two old laptops and got my hands on two webcam modules, but I cannot find out the pinouts for these modules.

    1. How could I determine which connections are which without destroying the modules ??

    2. Does anyone have information…

  • Camera terminal code/instruction order

    Greetings, I have started my Pi learning by adding to my photographic skills but have encountered a few difficulties, and after searching the forum posts feel a need to call on the community for assistance.

    My first project is to develop the time-lapse…

  • Disable camera LED

    Is there any way to disable the LED on the pi camera board?

  • Raspberry pi zero camera with a battery?

    Hey guys, just bought a raspberry pi zero v 1.3. In this version I'm able to connect the camera module with an special adapter cable. Do you know how to build a small and tiny camera? My project is to build a camera which could run itselfs. With its own…

  • Fabriquer un kinect-like autonome pour mobile (Android/IOS)

    Bonjour,

     

    j'aimerais lancer la fabrication d'un "kinect autonome" pour les plateformes mobiles (android et IOS si possible) dans le but d'intégrer le positionnal tracking au jeux Google cardboard.

     

    voici les exigence que j'ai sur ce…

  • Encore Express Cam II for RPI2B

    First of all I would like to thank this community in helping me find the light of my project. I am a complete beginner when it cams to raspberry pi and programming with python and I am taking things one-step-at-a-time.

     

    I've been learning a lot by having…

  • raspberry-pi-camera-board

  • Raspberry Pi Camera not working (v3.12.28) - mmal: mmal_vc_component_enable: failed to enable component: ENOSPC

    Hi,

     

    I don't know if this is the best place to ask this kind of question, but I am following tbhs' directives. I need help with the raspberry pi camera. I have been looking all other google for help but nothing seems to work altough a lot of people seem…

  • Motion software problem for IP web camera

    Hi guys

     

    I am using motion software on the pi to monitor video in a room.

    I am having some problems. whenever the raspberry pi camera board detects motion, the red light on the camera board flashes, and the video feed on the browser tries to refresh, but…

  • Idea: Piface CAD + Camera example

    Wouldn't it be great to provide a example to use the piface to take photos with the camera module? One of the buttons take photos, another start recording video and th other end recording.

  • camera over the internet

    I am trying to broadcast the camera over the internet I have done as it says and no errors come up but all that happens is I get a image preview on the pi for about a second and then it quits and nothing else happens

  • Iguana webcam - Photography Competition