Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Building SDR++ from source code on a Raspberry PI 4 4GB
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: TekMaker
  • Date Created: 8 Aug 2022 6:44 PM Date Created
  • Views 14572 views
  • Likes 7 likes
  • Comments 9 comments
  • raspberry pi 4
  • SDR software
  • SDR++
  • sdr
Related
Recommended

Building SDR++ from source code on a Raspberry PI 4 4GB

TekMaker
TekMaker
8 Aug 2022

SDR++, The bloat-free SDR software

Here is the link to my video for this 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

This assumes that you have already installed your SDR drivers, for the RTL-SDR I use the Osmocom ones from https://www.rtl-sdr.com/rtl-sdr-quick-start-guide/

Having found how good SDR++ is on Windows 11, I wanted it on my Raspberry PI 4 too. I did find a YouTube article from 2021 by Kevin Loughin 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 who used Alexandre Rouma's install script and source code https://github.com/AlexandreRouma/SDRPlusPlus/

Kevin was using an older version of Raspberry Pi OS and also discovered that the installation script had been written blind (untested) and had a couple of issues, he referred to cloning direct from GitHub which is common practice, but that command was simply missing. No matter, I managed to change the commands script as below and started to compile it myself discovering that the Volk software v1.0 was no longer available. A helpful bash message informed me that v2 was available and I changed the script for that.  I also had to include sudo and a mkdir for the CMake folder and set those permissions for it to work. After a very long wait and a few edits as I am running the current version of Raspberry PI OS 32 bit Buster. I compiled it for an RTL-SDR, but you can change one command and compiling for other versions should be really straightforward.

My script for the RTL-SDR is below, I will put this on my GitHub too. 
https://github.com/TekMaker/SDRplus

#!/bin/sh
set -e

[ $(id -u) = 0 ] && echo "Please do not run this script as root" && exit 100

echo "Installing dependencies"
sudo apt update

sudo apt install -y build-essential cmake git libfftw3-dev libglfw3-dev libglew-dev libvolk2-dev libsoapysdr-dev libairspyhf-dev libairspy-dev \
libiio-dev libad9361-dev librtaudio-dev libhackrf-dev librtlsdr-dev libbladerf-dev liblimesuite-dev p7zip-full wget

git clone https://github.com/AlexandreRouma/SDRPlusPlus

cd SDRPlusPlus

echo "Preparing build"
sudo mkdir -p build

cd build
sudo mkdir -p CMakeFiles

cmake .. -DOPT_BUILD_RTL_SDR_SOURCE=ON

echo "Building"
make

echo "Installing"
sudo make install

echo "Done!"

Save this file as rpi_install.sh

then chmod +x rpi-install.sh

./rpi_install.sh

If it doesn't go smoothly try entering the commands one line at a time into the terminal, you can skip the echo commands. I have built this on two installs so far with no problems.

If you want to compile for other radios either edit or add extra lines like this one "cmake .. -DOPT_BUILD_RTL_SDR_SOURCE=ON", for more information about this go to the Module List, and look for the Sources list on the github page https://github.com/AlexandreRouma/SDRPlusPlus/blob/master/readme.md.

Let me know how you get on with this!

  • Sign in to reply

Top Comments

  • mitchy93
    mitchy93 over 2 years ago +1
    also, you made a typo here where we go to execute the code, you used _ instead of - "then chmod +x rpi-install.sh ./rpi_install.sh" i picked it up, but the beginners may not
Parents
  • mitchy93
    mitchy93 over 2 years ago

    would this work on the 64 bit version of raspberry pi OS? the 32 bit version is quite slower so i stick to 64 bit on my pi 4 4GB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mitchy93
    mitchy93 over 2 years ago

    would this work on the 64 bit version of raspberry pi OS? the 32 bit version is quite slower so i stick to 64 bit on my pi 4 4GB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • radiolistener
    radiolistener over 2 years ago in reply to mitchy93

    yes I just installed it on 2023-05-03-raspios-bullseye-arm64.img, but at first attempt original script was failed because there is missing dependency, you can install it with "sudo apt-get install libzstd-dev", you can also add it into library list in the rpi_install.sh script. With this library it is installed ok on RPI 4 arm64 and works with RTL-SDRv3 dongle.
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.