Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Continuous sampling with the Data Acquisition Board for Pi Pico
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 25 Nov 2023 4:09 PM Date Created
  • Views 2359 views
  • Likes 10 likes
  • Comments 12 comments
  • ADC (Analog-to-Digital Converter)
  • pico
  • data acquisition
  • ads1115
  • rp2040
  • daq
  • pico-eurocard
  • raspberry_pi_projects
  • adc
  • test&measurement
Related
Recommended

Continuous sampling with the Data Acquisition Board for Pi Pico

Jan Cumps
Jan Cumps
25 Nov 2023
Continuous sampling with the Data Acquisition Board for Pi Pico

 shabaz designed a Data Acquisition Board for Pi Pico . In this post, I'm using it in continuous sample mode. Goal: get 1 second worth of samples, in 860 samples per second mode.

There are several options to trigger the reading of the samples. You could set up a timer that fires every 1162 µs. Then let it kick off a read. There is a 10% variation though - my device clocks at 850 samples, approx 2% slower. 

I've used another option that isn't dependent on the exact data rate: the ADS1115 has a RDY pin. I've configured it to pulse each time a sample is ready.

image

I modified the PCB, and connected the RDY pin to GP13 with a bodge wire.

image

The RDY pin needs a pull-up. I tested if the RP2040 internal pull-up has enough oomph: yes.

image

In my code, I attached an interrupt to the rising edge of GP13. Each time, it 'll initiate a read over i2c.

image

Highlights of the code (it's attached, with *.uf2 firmware precompiled)

volatile bool rdy = false;

void rdy_callback(uint gpio, uint32_t events) {
    rdy = true;
}

// board initialisation
void
board_init(void) {
    // ...
    
    // listener for ADC RDY
    gpio_init(13);
    gpio_pull_up(13);
    gpio_set_dir(13, false);
    gpio_set_irq_enabled_with_callback(13, GPIO_IRQ_EDGE_RISE, true, &rdy_callback);


    // ...
}

void adc_enable_rdy(uint8_t boardnum) {
    uint8_t buf[3];
    
    buf[0] = ADS1115_REG_LO_THRESH;
    buf[1] = 0x00;
    buf[2] = 0x00; //Lo_thresh MS bit must be 0
    i2c_write_blocking(i2c_port, adc_addr[boardnum], buf, 3, false);

    buf[0] = ADS1115_REG_HI_THRESH;
    buf[1] = 0x80;
    buf[2] = 0x00; //Hi_thresh  MS bit must be 1
    i2c_write_blocking(i2c_port, adc_addr[boardnum], buf, 3, false);
}

// ************ main function *******************
int main(void) {
    stdio_init_all();

    board_init();

    build_data_rate(BOARD0, DR_860);
    build_gain(BOARD0, AIN1, GAIN_2_048); // +- 2.048V

    #define SAMPLES 860

    uint16_t buf[SAMPLES];
    
    build_cont_conversion(0);
    adc_set_mux(BOARD0,0,false);
    adc_enable_rdy(0);

    uint8_t* buf8_ptr = (uint8_t*)buf;
    *buf8_ptr = ADS1115_REG_CONVERSION;
    i2c_write_blocking(i2c_port, adc_addr[BOARD0], buf8_ptr, 1, false);

    uint8_t* buf8_end_ptr = ((uint8_t*)buf) + (sizeof buf);
    rdy = false;

    while (buf8_ptr < buf8_end_ptr) {
        if (rdy) {
            rdy = false;
            i2c_read_blocking(i2c_port, adc_addr[BOARD0], buf8_ptr, 2, false);
            buf8_ptr += 2;
        }
    }

    uint16_t* buf16_ptr = buf;
    uint16_t* buf16_end_ptr = buf + (sizeof buf) / 2;
    
    while (buf16_ptr < buf16_end_ptr) {
        *buf16_ptr = *buf16_ptr >> 8 | *buf16_ptr << 8; // swap bytes
        printf("AIN1 = %.3f V\n", to_volts(BOARD0, 0, *buf16_ptr));
        buf16_ptr++;
    }

    while (FOREVER) {}
}

I didn't include the definitions and functions of shabaz ' source code example. They are available in the download.

The data collection loop is made as short as possible. I set the i2c baud rate to 1 MM. And removed the bit swapping and voltage conversion from the sample loop. I made a second loop that does these conversion activities once all data is collected.
This isn't needed for timekeeping. There's enough time for slower i2c , and to do bit swapping and voltage conversion.
What we can gain by taking them out, is to let the controller go low power while waiting for a next pulse. Not implemented, but worth investigating.

image

Enjoy!

Source and firmware: 
adc_board_test_20231125.zip

  • Sign in to reply
Parents
  • Jan Cumps
    Jan Cumps over 1 year ago

    OO version follow-up:  OO example for the Data Acquisition Board for Pi Pico: deep dive into the sample data buffer 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 1 year ago

    OO version follow-up:  OO example for the Data Acquisition Board for Pi Pico: deep dive into the sample data buffer 
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.