Learn more about the Cirrus Logic Audio Card here.
Learn more about the Cirrus Logic Audio Card here.
I've used the https://github.com/CirrusLogic/rpi-linux/wiki/Building-the-code guide and successfully got my Cirrus Logic Audio Card / Raspberry Pi 2 almost working, but there is a problem with sample rates.
I've run the CL scripts Playback_to_Lineout…
Hi all
I got my PI working with a kernel build as described in https://github.com/CirrusLogic/rpi-linux/wiki/Building-the-code and the mmap-Patch applied.
./wiki-content/scripts/Playback_to_Lineout.sh /usribn/jackd -alsa -Dhw:sndrpiwsp -r44100
I see these…
I am trying to run the cirrus logic audio card with the raspberry Pi 2 and it seems that there is still problem with kernel, any suggestion?
Hello, I was recently making a research about an enclosure option for the Raspberry Pi Model B+ with the Cirrus Logic audio card but I couldn't really find anything. I was wondering if any of you could have seen something that might work? I own the Pi…
Dear Sirs,
Is real time play back of digital audio signal recieved through the SPDIF input of the Cirrus Audio Card through an USB DAC connected to the Raspberry Pi possible?
If yes, than what kind of OS version, drivers, software, patches or settings are…
Today I received my new Rpi 2 and sound card.
First I tried to install OpenElec from my windows PC on a SD-card, which worked fine (no use of sound card of course).
Then I updated it with a .tar from Index of /~hias/tmp/openelec-wolfson
It just showed a…
Hello, Can the Cirrus Logic audio card take an SPDIF input from an external source and play it on the analogue outputs? If so, is there likely to be much latency? Does the audio data have to pass through the Raspberry Pi or can this be handled by the…
Hi,
I am working on a project where I use a Cirrus Logic Audio Card with a Raspberry Pi to implement a reverberation effect for a guitar. The idea is to use the line in port of the Cirrus card to capture the data one sample at a time, put that sample through…
Hi everyone,
My current project is to run constant FFT on an audio stream and output the data to a 3D LED Array. Google 3D LED cubes if you don't know what they are. My cube is more of a rectangular prism, 24x8x8=1536 LED's. I am new to the world of PI…
I was hoping to use the Cirrus board as a digital effects guitar pedal. I was planning on using line in and line out since the connections make things very simple. However, I have run into some problems with the line out to guitar amplifier connection…
Wolfson Audio Card | Cirrus Logic Audio Card | |
Compatible | ||
Raspberry Pi Model A and B | Yes | No |
Raspberry Pi Model A+ and B+ | No | Yes |
Technical Features | ||
26pin GPIO Connector | Yes | No |
40pin GPIO Connector | No | Yes |
Back powering Raspberry Pi | No | Yes |
Render… |
Cirrus Logic Audio Card for B+ and A+ Onwards Schematics
Cirrus Logic Audio Card Safety Leaflet
I just bought a new copy of the Cirrus Logic Audio Card. I'm still waiting on delivery of the quadcore Pi 2, so my fallback option is to start off using it on my B+.
Rather than downloading and installing the Cirrus Audio linux os image, I'd prefer…
Hi all!
As you might know, Cirrus Logic's main kernel source branch recently switched to 3.18.
My first thought was "Hmm, that means the Cirrus Logic card could finally work on the RPi2..."
I have built a couple of 3.18 kernels for my B+ and…
I'm not sure if it's related to the card (maybe I installed it wrong or something), but I was wondering if anyone on here could help me out.
I'm having some mixed results with the arecord command in the terminal. The hardware I'm using consists…
New Cirrus Audio Board available no drivers however.
Element 14 stated that this board is compatible with Raspberry Pi 2.
I'm looking for a…
Hello all. I'm new to the Raspberry Pi (just got my first Pi, an RPi 3 Model B). I am looking to create an high-quality audio+video recorder out of my Raspberry Pi. (In a way, I'm basically trying to make a camcorder.) I want to add the Raspberry Pi Camera…
Has anyone got Jasper working with the cirrus logic audio card and a raspberry pi 2? I am trying to use spkout speakers and the DCIM microphones with Jasper.
I manually installed Jasper ontop of the cirrus audio card image as per the instructions from…
Dear Forum.
I am new to this thread so sorry if the question seems maybe stupid. But.
As following what's inside the manual at page 2 at FEATURE voice :
I was wondering if anyone…
After downloading and installing cirrus_logic_audio_card_all_pi_versions.img on my RPi 2, I've had nearly a month's worth of trouble-free operation with the Cirrus audio card. However, after doing an apt-get update and upgrade today, the Cirrus audio…