• No output.  What next?

    New Element14 Raspberry Pi 3 Model B out of box:  Per instructions, formatted (FAT32) successfully a MicroSD card, inserted it, connected USB keyboard, USB mouse, HDMI monitor, Ethernet, and lastly power.  --> No video output, no sign of life aside from…

  • Requesting help with Eth0 issue on Raspbian Jessie

    Good evening,

     

    This has been an issue that has bothered me for quite a while now. I'm trying to set up my raspberry pi 3 to work via ethernet at my workplace, but it does not seem to work. However, on any windows machine that I have, I get issued an IP…

  • WiFi questions with the Raspberry Pi 3 Model B

    While the Raspberry Pi 3 Model B has a builtin WiFi module, does it have an option of connecting an external antenna to it?

  • Setting up Bluetooth on the Raspberry Pi 3

    Wireless at Last!

     

    Now that it has been a few weeks since the release of the Raspberry Pi 3Raspberry Pi 3, support for the WiFi and Bluetooth chip has settled and you can use it with Raspbian. Support with Windows 10 IoT Core will be available in the early…

  • Raspberry Pi 3 Model B Frequently Asked Questions (FAQs)

     NEW! Raspberry Pi 3 Model B
    Comparison ChartTechnical SpecificationsUnboxing Video
    40 Pin OutPi3 Video Arcade Project

     

    If you have a question that is not answered in this FAQ, please ask it below in the comments.  If your question is specific to your order…
  • Raspberry Pi 3 Model B Technical Specifications

     NEW! Raspberry Pi 3 Model B
    Comparison ChartFrequently Asked QuestionsUnboxing Video
    40 Pin OutPi3 Video Arcade Project

     

             

                                                                          
       

    NEW! Raspberry Pi 3 Model B

       

    Buy NowBuy NowBuy NowBuy Now

       

    Learn More

       

     

       

    Key Improvements from Pi 2 Model B to Pi 3 Model B:

     Next Generation…

  • Raspberry Pi USB Output Power

    I was recently surprised by a characteristic of the RPi 3B's USB Output ports.  I don't usually monitor the voltage at the USB port, but I was trying a new setup with an Arduino Uno connected via USB while running Windows 10 IoT Core on a headless…

  • TOTAL NEWB NEED PLEASE HELP PROFESSIONALS WANTED

    Im trying to connect the NTSC/PAL TFT 3.5" Display to my Pi 3 buti broke off one of the connectors that i was gonna connect it to which i beleive is ground. Is there another spot i can connect it to (ground and 5v).

    Also are these correct?

    Also is…

  • Strange problem: GPIO PWM only working when connected to WiFi

    Hello,

     

    I've got a strange problem.

    I wrote a python script to send an PWM signal to GPIO1 of my Raspberry Pi 3 using the wiringpi library.

    While writing the script, the Pi was connected to WiFi so that I could do it all via ssh from my notebook.

    I connected…

  • Pi Desktop very disappointing

    I had high hopes for this but it doesn't appear to be very good.  The build quality seems fine and it looks good - just a shame it doesn't actually work.  Or doesn't actually work yet.

     

    The instructions aren't up to much either.

     

    I have a perfectly…

  • Ultimate Guide for Raspberry Pi 3 Performance and Cooling

    There are alot of threads and youtube videos on how to get the best performance out of the Pi 3, This is mine.

    https://youtu.be/KuEZV0WsRLg

     

    For everything you see in this video, regarding updating, benchmark Installation and Mods, see:

    https://drive.google…

  • What Will You Do With Your New Raspberry Pi 3?