Hi everyone.
I am actually working on real time image / video processing..?
What versions / models of Raspberry Pi are suitable for this..?
Is that be possible on Raspberry Pi Model B element 14 ..?
Kindly please help.
Hi everyone.
I am actually working on real time image / video processing..?
What versions / models of Raspberry Pi are suitable for this..?
Is that be possible on Raspberry Pi Model B element 14 ..?
Kindly please help.
I have started this poll as I am interested to screen in the most possible complete way what is the various languages you are approaching to develop on the Raspberry PI. I have explicitly added raspbian as the most Debian-like Linux distribution supporting…
Hi to all.
I have got just today the 120 Gb SSD SATA disk that will be the definitive external storage support for the PI master of the Meditech project. At home I have some SATA to USB converter boards recovered from old external USB HDD boxes that hosted…
Hi to all,
discussing with a friend that has recently bought a PI (B 2) he told me that he has found on aliexpress (see the link below: Online Shop X300 Raspberry Pi Expansion Board Adds Bluetooth, Microphone input, stereo audio output, WiFi, RTC, IR recei…
I have investigated here and there without success until now. There is a lot of (good) documentation about the usage of the PiFace CAD display but I can't find what are the really used PINs on the Raspberry PI. In fact I see that this add-on board can…
Hi,
I am a very new beginner to the Raspberry Pi, and I am wondering how I can programmatically detect if there is a current flowing through the circuit I built, connected to my Raspberry Pi 2 Model B. My circuit consists of a wire connected to the 3.3V…
Hi to all,
I have a doubt about the use of a IR receiver connected to the Raspberry PI GPIO. Is it sufficient to connect the data pin to the GPIO port and power the sensor of some pull resistor is the worth to use?
I am using the TSOP312 hat is 3.3V compatible…
Hi,
I am new to the Raspberry Pi and I was wondering how I would connect door contact switches (or any kind of switch) to the pins on my Raspberry Pi. I have a Raspberry Pi 2, Model B. The purpose of this so that I could read if the door switches are together…
Just registered and after a long research...
The set:
The history:
I have successfully installed Qt 5.3 on raspbian and it works fine. This will be definitely the environment I will develop the Meditech main interface. The problem is that I was not able to install in any way the QtQuick / QML environment. Does someone…
I have a project where my Raspberry Pi starts taking pictures at 4:30AM and stops at 7:30AM everyday. Then MENCODER or AVCONV should turn on to stitch them together into a movie. Then a Dropbox Uploader uploads the movie to my dropbox account, and another…
This is half a question and half to start a discussion open for any kind of suggestion. If I have the need to start the Raspberry PI raspian with a customized desktop, including some parts and reoving others. Does someone has this kind of experience?…
It's just an idea and before trying to make tests i'd like to ask your vision.
The power of the PI Face Digital is that there are a certain number of elements, including a couple of good quality relays, ready to use. Then there is a missing component…
How do someone of you has setup the Raspberry-PI (no matter the model) to run the MPIDE under Raspian to program and manage the Chipkit PI ? I have read in various places about a raspian version with the preinstalled MPIDE but the few links I have found…
pi@raspberrypi ~ $ free -m
total used free shared buffers cached
Mem: 371 331 40 0 18 198
-/+ buffers/cache: 114 257
Swap: 99 15 84
pi@raspberrypi ~ $
and there should be 1GB. Totally puzzled. I formatted the SD card and wrote Raspbian to it ...NOT NOOBS.…
I am very basic with the language of python but I am trying out a project which is an electronic lock.
But the problem is that I cant seem to work out how to make a program that asks for a four digit number password and when the correct digits are entered…
I have built a birdhouse, with a Raspberry Pi and NoIR in it. But I am having issues with sealing it from the elements.
I had an IR Led light ring that burned out part of circuit. Not sure if it was because of elements.
Also looking to seal up the PiCam…
I have been trying to figure out if I could use my NiMH battery while it is in use for my current project. If it is possible, how would I go about doing this?
I am currently making a handheld retrogaming system using Raspberry Pi, a rear view camera monitor…