Learn more about the Cirrus Logic Audio Card here.
Learn more about the Cirrus Logic Audio Card here.
Hi all
I got my PI working with a kernel build as described in https://github.com/CirrusLogic/rpi-linux/wiki/Building-the-code and the mmap-Patch applied.
./wiki-content/scripts/Playback_to_Lineout.sh /usribn/jackd -alsa -Dhw:sndrpiwsp -r44100
I see these…
On the box and on the sales material it says the audio I/O card is available for rev B and onwards. This is incorrect. Current 2 versions do not have the 5-pin header needed and have an expanded GPIO connector. Is there a revision of the audio board in…
Hello, I was recently making a research about an enclosure option for the Raspberry Pi Model B+ with the Cirrus Logic audio card but I couldn't really find anything. I was wondering if any of you could have seen something that might work? I own the Pi…
Dear Sirs,
Is real time play back of digital audio signal recieved through the SPDIF input of the Cirrus Audio Card through an USB DAC connected to the Raspberry Pi possible?
If yes, than what kind of OS version, drivers, software, patches or settings are…
Hi, I already see the comparison chart between the Wolfson Audio Card and the new Cirrus Logic.
I liked the new one allows to connect more GPIOs because the new RPi B+ have more pins available.
Since i still have the earlier Model B and the original Wolfson…
Hi to all,
I have ordered 2 of these cards and plan to experiment with them to create wireless battery operated sound systems.
Although it should work, eventually, I do miss info on the power needs of this card at this moment.
And I assume when we have got…
Hello,
I'm on pidora, I should like to compile the kernel with the driver of the wolfson audio card but I don't find the patch for the kernel 3.12, I finded just for the 3.10.
Anybody knows where they are ?
how do i use Wolfson Audio Card to identy sound signature. I want to record some sound & compare with unkown to detect the match presantage like DTW function
I would like to know how to get to the record and playback audio buffers to I can put the audio data into UDP packets for transmission/reception off board via ethernet/IP.. If anyone knows how to get the the Rapian ethernet buffers, that would also be…
Been trying since 6/15 to download:
http://downloads.element14.com/wolfson/wolfson_3.10_master.zip?COM=WolfsonAudioCard
All IE, Firefox and Chrome get is 408MB
Today I tried wget from the PI and get 408MB.
Gave up on wget and tried curl, I get less, 398MB…
Hi,
Completely new to this fascinating world of Raspberry Pie, I have to pose a simple question: does the new Wolfson sound card improve the sound through HDMI, or do I need to use the jack connection?
Thanks for answering....
PjotrB
Hi everyone,
My current project is to run constant FFT on an audio stream and output the data to a 3D LED Array. Google 3D LED cubes if you don't know what they are. My cube is more of a rectangular prism, 24x8x8=1536 LED's. I am new to the world of PI…
I was hoping to use the Cirrus board as a digital effects guitar pedal. I was planning on using line in and line out since the connections make things very simple. However, I have run into some problems with the line out to guitar amplifier connection…
Wolfson Audio Card | Cirrus Logic Audio Card | |
Compatible | ||
Raspberry Pi Model A and B | Yes | No |
Raspberry Pi Model A+ and B+ | No | Yes |
Technical Features | ||
26pin GPIO Connector | Yes | No |
40pin GPIO Connector | No | Yes |
Back powering Raspberry Pi | No | Yes |
Render… |
Click on the links below to get the appropriate data sheet:
Important Note: Please be aware that the Wolfson Audio Card is only compatible with Raspberry Pis which feature the P5 pads, which can…
Cirrus Logic Audio Card for B+ and A+ Onwards Schematics
Cirrus Logic Audio Card Safety Leaflet
Important Note: Please be aware that the Wolfson Audio Card is only compatible with Raspberry Pis which feature the P5 pads, which can be found on Revision 2 Raspberry Pis onwards.
Important Note: Please be aware that the Wolfson Audio Card is only compatible with Raspberry Pis which feature the P5 pads, which can be found on Revision 2 Raspberry Pis onwards.
![]() |
This audio card will push your Pi.
The Wolfson Audio CardWolfson Audio Card has taken a good amount of time to come forth from Wolfson Microelectronics and with decent reason. They want to make sure that they have it right and something that you can work… |
The size of a sd card is not fixed - a 8GB card can contain less than 7.5 GB - and you normally don't see this. Flashing the image on such a card needs a lot of time and ends up with an error message and a unbootable card. Please shrink the system image…