Hi,
I am having problems understanding how to resolve/work around the PFC update race condition that leads to the garbled screen. I am using the python3 libraries, and have made sure I am back at 700Mhz.
The code can be found in github : https://github…
Is this compatible with Raspberry Pi model B+?
If it is, are there any cases that'd hold it with B+?
Hi guys,
I'm planning to buy Wolfson audio card for my rpi, and play with volumio (http://volumio.org).
I'm interested also in PiFace CAD; is there a way to make those two product work together?
Thanks, bye bye!
Moin,
ich bin verzweifelt auf der Suche nach einer Lösung.
Ich habe ein Raspberry Pi Mod. B 512MB und habe mir das Piface Control & Display dazu gekauft, um den Raspberry um einen IR-Empfänger und ein Display zu erweitern. Ich habe RaspBMC installiert.…
I Just wanted to know that of what frequency IR sensor is used in PiFace CAD ???
Got my PiFace working straight away.. I'd like to have a proper schematic like the one that came with my Raspberry-Pi.
Thanks,
JQ
I have pifacecad and an ir control. This connects and generates the expected characters. However when I try to use it with the radio.py example I get no response. Does anyone have a working example of all the files (radio.py radiolircrc etc) It is driving…
Hello,
I'm trying to get pifacecad working on raspbmc.
I have installed python3-pifacecad from raspbian repositories, but when I try to launch the example script /usr/share/doc/python3-pifacecad/examples/sysinfo.py i'm getting the error "No PiFace Control…
Hi,
I want to use the Pyface CAD shield together with other things. It probably isn't using all the pins.
But which ones does it use and which could I divert to other things? Most importantly are the pins for any of the UARTs free?
Yours,
Goswin
PS: It…
There's a 60 second update time written into the code but is not used. How does this sample display updates ? Does it update at all, even?
I've followed the instructions at Installation — PiFace Control and Display (CAD) 2.0.6 documentation to install the libraries an example code. When I try to run the sys info example, using python3 /usr/share/doc/python3-pifacecad/examples/sysinfo…
Have you successfully writen a python script supporting the switch event from the PiFace CAD?
I can't get it to work.
The display is fine, and I can poll the state of the switches satisfactorily.
Also no success with infrared events, although again the…
2 October 2014, element14 and the team that designed the PiFace TM has launched a new series of exclusive Raspberry Pi accessories and updated the popular PiFace Digital and Control & Display following the launch of the Raspberry Pi model B+ this July…
Yesterday the media lab in our Leeds office was taken over by a strange TARDIS looking pod. People walking past seemed very interested in the flurry of activity going on within the strange structure. It was actually Andrew Robinson of PiFacePiFace fame…
Dr Andrew Robinson, creator of the PiFace Control and DisplayPiFace Control and Display is visiting the element14 offices tomorrow and has kindly agreed to answer your questions about the PiFace DigitalPiFace Digital, Control and Display and also the…
LAST WEEK the team at PiFace Digital unveiled this epic project, which used the Control and DisplayControl and Display to create a bullet time effect using a number of Raspberry Pi camerasRaspberry Pi cameras, boards and control units. Whilst this project…
So what do you get when you combine 48 Raspberry Pis48 Raspberry Pis, 48 PiFace Control and DisplaysPiFace Control and Displays, 48 Pi Cameras48 Pi Cameras and half a kilometer of network cable? The answer is your own DIY bullet time camera rig and arguably…
From the initial design sketch a specification began to emerge. Top of the list it had to be easy to use. Despite not using a full keyboard I wanted the user to find it easy to interact with the Raspberry Pi. Selecting a menu option needed to take seconds…
Guys,
what is the difference between PiFace Control and Display version 1 and PiFace Control and Display version 2 ?
Thanks,
teo