Raspberry Pi
  • Products
  • More
Raspberry Pi
Documents PiFace Home Timeswitch - turning a light on and off
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: PEarle
  • Date Created: 23 May 2013 8:29 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 5:29 AM
  • Views 4690 views
  • Likes 1 like
  • Comments 46 comments
Related
Recommended

PiFace Home Timeswitch - turning a light on and off

** Update**

 

I've now implemented this using an Energie Pi Controlled mains Socket - see my blog at Home Automation using ENERGENIE - ENER002-2PI

 

For details on the Energie socket see ENER002-2PI - ENERGENIE - RF CONTROLLED MAINS SOCKETS, FOR | CPC


 

 

One of the things I wanted to do with my Pi from the outset was to be able to use it as a timer, to turn a light on and off at night when I was out, as a simple form of home security. Being something of a newbie when it comes to electronics, my biggest problem was how to wire it up to be able to turn the power on and off.

 

The Pi relays are rated at a maximum of 20v and 5amps - therefore I cannot connect the Pi directly to the 'mains powered' light !!!

 

What I am planning on doing is investigating using a to a commercial relay which can cope with the current. When I've done that I shall update this blog again with details of the how the Pi can safely control a mains powered device.

 

However, the rest of the blog is still valid as it explains how the relay on the PiFace is operated and will be used for the Timer application, when completed.

 

I've written a java program to control the light switching on and off which does the following;

 

  • Calculate a random wait time between two values that I have supplied (2 and 20 minutes at the moment)
  • Wait for that period of time to elapse
  • At the end of the wait time, toggle the relay - switch it on if it was already off, and vice-versa.
  • repeat the above ad infinitum

 

The result is that the light will keep turning on and off in a random pattern making it look as if someone is using the room even when I'm not there !

 

 

Java Code

I've already written a document about using Java on the Pi - see http://www.element14.com/community/docs/DOC-54112/l/java-on-the-raspberry-pi. The code that I used for this project is attached to this document (e.g. timeswitch.zip)

 

 

Running Automatically

My intention is really to have this as a 'black box' function so that the TimeSwitch application will run as soon as the Pi is switched on. This is accomplished quite easily - all I need to do is write a script to run the java application, and then add it to the initialisation script.

 

The script to run the java application is as follows ;

cd /opt/pi4j/examples
java -classpath .:classes:/opt/pi4j/lib/'*' com.phe.datetime.TimeSwitch

To run at start up I have edited  /tec/rc.local and added the following line

 

/opt/pi4j/examples/timeswitch.sh > /opt/pi4j/examples/timeswitch.log

 

This will execute the java app at start up and also pipe any log messages to timeswitch.log.

Attachments:
timeswitch.zip
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to Problemchild +2
    Maybe a DANGER rating from Bunny minion through to Skeleton minion
  • mcb1
    mcb1 over 11 years ago in reply to michaelkellett +1
    If you look at the RCSwitch there is a RPi solution. Frederick also used these to interface as an I2C device. http://www.element14.com/community/community/design-challenges/forget-me-not/blog/2014/08/11…
  • mcb1
    mcb1 over 11 years ago in reply to eatojg +1
    This adds a piece for the RPI and while it suits the UK, there are many others using a similar 433 or 315 MHz RF control. The code in the Watts Clever have a 24 bit data stream, but in reality it only…
Parents
  • eatojg
    eatojg over 11 years ago

    Why not do switch mains voltage perfectly safe with one of these. They work absolutely great

     

    Energenie ENER002-2PI remote control sockets with Raspberry Pi controller board - white: Amazon.co.uk: DIY & Tools

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to eatojg

    I've recommended that people hack radio controlled sockets in the past  -  it's nice to see that there is a ready made RPi solution. You say these work well which is nice to hear. Do they come with software ?

    I agree that this approach (no mains work at all) is best for the inexperienced and possibly cheaper even if you know how to do it (no boxes, clamps etc needed).

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 11 years ago in reply to eatojg

    I've recommended that people hack radio controlled sockets in the past  -  it's nice to see that there is a ready made RPi solution. You say these work well which is nice to hear. Do they come with software ?

    I agree that this approach (no mains work at all) is best for the inexperienced and possibly cheaper even if you know how to do it (no boxes, clamps etc needed).

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 11 years ago in reply to michaelkellett

    If you look at the RCSwitch there is a RPi solution.

     

    Frederick also used these to interface as an I2C device.

    http://www.element14.com/community/community/design-challenges/forget-me-not/blog/2014/08/11/elro-coco-with-openhab

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down