Documents Five Things You Need to Know About the Raspberry Pi Zero
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: spannerspencer
  • Date Created: 25 Nov 2015 2:02 PM Date Created
  • Last Updated Last Updated: 6 Oct 2021 8:43 PM
  • Views 7029 views
  • Likes 7 likes
  • Comments 34 comments
Related
Recommended

Five Things You Need to Know About the Raspberry Pi Zero

It's always exciting with the Raspberry Pi Foundation launches a new board, and we know that you're bursting with questions about the all-new Pi Zero. We certainly were.

 

So here are our top five questions about the Pi Zero that we're anticipating you'll have, along with their answers, of course.

 

1) What are the technical specifications of the Raspberry Pi Zero?

    • CPU: Broadcom BCM2835, can be overclocked up to 1GHz.
    • RAM: 512MB on board.
    • Power: 5V, supplied via micro USB connector, drawing160mA (even when connected to an HD display).
    • Dimensions: 65mm x 30mm x 5mm
    • Storage: MicroSD card.
    • Video & Audio: 1080P HD video output. Audio output via mini-HDMI connector.
    • Operating System: Linux, installed via NOOBS.
    • Click here for an exploded image of the Pi Zero's features.

 

 

2) Where can I buy a Raspberry Pi Zero?

    • The new Raspberry Pi Zero is available to order from Thursday, 26th November. Initial stocks are extremely limited, with small pockets of availability in the US and UK. Unless you're one of the lucky few to get your hands on one of the first batch, the next deliveries are due towards the end of December.
    • You'll be able to order the new Pi Zero in the majority of countries as more stock becomes available.
    • Click the Buy Now buttons here to check for availability.

 

3) Does it still run Linux?

    • Yes, it does indeed. You install it the same way as always:
      • Download NOOBS and unzip it to a microSD card; connect the Pi Zero to a monitor, USB hub, keyboard and mouse; power it up and follow the on-screen prompts to install the Linux build of your choice.
      • element14 is offering a Pi Zero package that includes a NOOBS microSD card to make your installation quicker and easier.

 

4) What's the difference between the Raspberry Pi 2 Model B and the new Pi Zero?

    • The Pi Zero uses the single-core BCM2835 processor with 512MB RAM as used in the Raspberry Pi 1 series, versus the newer, faster BCM2836 quad-core processor on the latest high performance Raspberry Pi 2.
    • To save space the following products have been replaced with alternative solutions or removed completely:
      • 4 USB ports and Ethernet port have been replaced with one Micro USB data port on the Pi Zero.

      • 40 pin GPIO still contains the same pin out on both boards, but the connector remains unpopulated on the Pi Zero.

      • The full size HDMI port on the Raspberry Pi 2 has now been replaced with a Mini HDMI port on the Pi Zero. This requires an adapter to be fitted before connecting the Pi Zero to your TV. The Pi Zero still supports full HD 1080P output.

      • The camera and display interfaces have been removed as well as the 4-pole stereo and composite video port.

 

5) Why did the Raspberry Pi Foundation create the Pi Zero?

    • The Pi Zero follows the same philosophy that gave birth to the Raspberry Pi platform in the first place; low cost computing for everyone. The Pi Zero complements the other models in the Raspberry Pi family by providing an entry-level model with stripped down components to target users with specific solutions in mind.
    • Is it the same as the other Raspberry Pis? Yes and no. It's still a fully functioning Linux-based computer with 1080P video output, but it's also much more closely related to the small, efficient, single-purpose world of IoT.

 

Got any other questions or observations about the Raspberry Pi Zero? Ask them in the comments below.

 

Find out more about the Raspberry Pi Zero right here.

  • raspberry_pi
  • pi_zero
  • raspberrypi
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • skspurling
    skspurling over 10 years ago in reply to johnbeetem +4
    Got the Pi zero. Booted it up on the lapdock with an Ethernet dongle. Same old Raspbian WiFi glitchy-ness with some of my cheap WiFi modules. Other than that, it is good. If you develop on the Pi2, it…
  • mconners
    mconners over 10 years ago in reply to balearicdynamics +3
    It seems like the point of this $5 module is to allow you to develop on another Pi platform and then dump the finished product onto this board. I would suspect you could even move the entire sd card, so…
  • shabaz
    shabaz over 10 years ago in reply to alysson +3
    Hi Alysson, I think there is a higher chance of destroying a Pi Zero than other Pi models, because the 'Zero uses surface-mounted MicroUSB (although there are holes for the shell, they have no pins inside…
Parents
  • Former Member
    Former Member over 10 years ago

    3 main questions.

     

    Where can I get the schematic diagram and parts list for the PI zero? You can not do a proper design-in without these

     

    What is the policy on design continuity and compatibility as the product evolves (ie move from [say] model A to model B)?

     

    What is the likely availability of Pi Zero and all its descendants or will the "genre" be discontinued once the basic CPU is discontinued?

     

    Basically can I design a gadget with it knowing that I will be able to repeat the design with something similar but  with the same physical structure in [say] 1,2,4 .... years?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to Former Member

    To get answers to those questions (which are perfectly reasonable for  a commercial product) you will need a direct relationship with the supplier (ie RPi Org) which I don't think is likely to happen unless you are buying vast numbers of parts. Normally you would expect a supplier of  a key component to provide some answers but it would not be uncommon for the answers to be no,none,zero,no (same order as you asked them). If it is life and death for your business to get positive answers you will need to either make your own boards or pay a great deal more. To be fair to the RPO (not my strongest suit, I'll admit) they are offering a consumerish product at a rock bottom price so you can't really expect the same kind of support that you would get if you went to one of the "industrial" type board suppliers.

    If it really matters to you then ask yourself if the Pi is the right part - (I'll offer an opinion/alternative if you want to describe your project in more detail).

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 10 years ago in reply to Former Member

    To get answers to those questions (which are perfectly reasonable for  a commercial product) you will need a direct relationship with the supplier (ie RPi Org) which I don't think is likely to happen unless you are buying vast numbers of parts. Normally you would expect a supplier of  a key component to provide some answers but it would not be uncommon for the answers to be no,none,zero,no (same order as you asked them). If it is life and death for your business to get positive answers you will need to either make your own boards or pay a great deal more. To be fair to the RPO (not my strongest suit, I'll admit) they are offering a consumerish product at a rock bottom price so you can't really expect the same kind of support that you would get if you went to one of the "industrial" type board suppliers.

    If it really matters to you then ask yourself if the Pi is the right part - (I'll offer an opinion/alternative if you want to describe your project in more detail).

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Former Member
    Former Member over 10 years ago in reply to michaelkellett

    Perhaps you are right this is the wrong organ to address my queries to.

     

    Again your logic is correct but I would council that the RPi zero is probably meant to be a "super" Arduino intended to be the heart of a programmed gadget rather than a programmable PC. The very existence of unpopulated header sites suggests that the intention is that solder connections should be made as required. Once you introduce soldering into the mix you are in a wholly different ball game and the "project" becomes both software and hardware orientated. If this is the case you need to know much  more about the actual physical  implementation mainly around the peripheral circuits (switch mode power converter etc). This is most certainly the true if you are trying to support youngsters in their projects. The 5$ tag certainly would indicate this.

     

    Now, it may be, (please excuse the cynicism but I have been designing and using chips since before the Intel 8008 and had my fingers burnt quite a few times and not due to over dissipation!!!) that RPi org have a commercial relationship and contract for a certain quantity of processors which when they are gone they are gone. On the other hand the RPi zero may just be a new genre of controller that RPi org have introduced and will pursue with compatible (where possible) evolved product.

    If it is the latter case then there is sense in putting some effort into support material. If the former "when its gone its gone" then OK that is a perfectly legitimate approach and I have no complaint but it is as well to know.

    Certainly if the latter is true then the RPi zero will have a huge interest for commercial applications where the volume does does not justify a custom design. Put the RPi zero together with a simple 2 layer pcb with the extra bits on (eg 12 bit ADC,  WiFi module  or ....) and you end up with a very powerful solution that will reach beyond the IoT. RPi org will certainly get a high volume flow of the basic semiconductor  devices. As I said a "super" Arduino.

     

    A bit like the intentions of the 9$ computer but supplied by probably an organisation with a sounder commercial footing.

     

    Anyway that is my tuppence worth.

     

    CH

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • alysson
    alysson over 10 years ago in reply to Former Member

    My own take on the Zero is that it is intended to fulfil two market niches -

     

    First is the educational computing market where students are able to work on a programmable PC-like platform without fear of destroying their main computer (at $5, the Zero is almost a disposable commodity)

     

    While not a PC, the machine is sufficiently PC-like to give a real taste of real-world programming - including all of the hardware that you tend to be insulated from with larger systems.

     

    The second niche is that of an embedded front end for electronic 'projects' - where a moderately powerful system provides all of the user interface, communications etc. for a piece of equipment that may have a mass of slave subsystems. Indeed, I currently have a project on the go which utilises Arduinos as the prime data capture devices and a headless RPi (currently a B, but a Zero will replace it ASAP) to handle the data display, multiple data-stream consolidation and logging. Yes, effectively a super Arduino/Yún but without the hassle of user interface development of the Arduino or cost of the Yún.

     

    Again, the Pi is here providing an intermediate step between micro-controller and host system

     

     

    Having followed the Raspberry Pi story from its earliest public announcement, I have to say that the early response was beyond amazing, and the continued (and increasing) demand speaks of a device family which may well be with us for a very long time.

     

    Where the Raspberry Pi range will be in 10 years time, I cannot say, but I would hazard a guess that it will still be going strong and providing a consistent platform for project and educational development.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to alysson

    Hi Alysson,

     

    I think there is a higher chance of destroying a Pi Zero than other Pi models, because the 'Zero uses surface-mounted MicroUSB (although there are holes for the shell, they have no pins inside, at least for the 'Zero that I examined) in contrast to the larger, better-secured full-size USB connectors on all other Pi models.

    Furthermore, the B+ model introduced a polarity protection circuit which is missing on the 'Zero (I see no MOSFET near the power cicuitry on the 'Zero). We have already seen the effect of this with some experimentation that bwelsby did.

    For education it doesn't save cost either in some ways, just hides cost on ancillary devices. For example more expensive wireless keyboards and mice would be needed with the 'Zero, unless a USB hub was also purchased (not needed with the full-size Pi). And those small wireless dongles may go missing, so spares will be needed. Plus we know that a HDMI monitor is needed (and an unusual HDMI cable or adapter that not many people will possess). For students to use bits of functionality, they will need to solder up a header to the bare pins, which is another cost. And for all that, the end result is a Pi which is 6 times slower than its bigger brother.

     

    I think there is less chance of destroying a regular sized Pi because the soldering iron and blobs of solder never need to get close to the regular Pi. Any connections are done on the end of jumper cables or ribbon cables. This gives the teacher the option of visual inspection of projects (or a quick buzzer test to ensure the supply pins are not shorted to any other pins) before students plug it into the Pi.

     

    I think the 'Zero is great for hardware enthusiasts/hackers who wish to create fun and interesting projects though. Why this was something the Pi Foundation decided was in educational interest I don't know - why should a charity fund development for products for hardware enthusiasts/hackers who are already educated enough to know how to program and how to use a soldering iron, and have the money for a full-sized Pi to meet educational needs for themselves. Sounds bizarre to me. Perhaps they should have concentrated on cost-reducing (e.g. sourcing cheaper parts) for the full-sized Pi now that it is a mature product, since that would have directly impacted school educational need spending. We know that cost reduction is possible on the full-size Pi, since the Orange Pi costs less than $18 all-in, delivered from China to the UK, and by many accounts has similar hardware technical specification to the Pi 2. It is fine that the Pi is manufactured in the UK and provides UK jobs, but with cost-reduction more kids in the UK and around the world would have access to a fully functional Pi than the 'Zero. It surely outweighs the number of jobs created today at Sony UK. Just an opinion though!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mconners
    mconners over 10 years ago in reply to shabaz

    You're just a crank. image  j/k all good points. Maybe the low price point will get kids to not be scared to bring a soldering iron near it, though. If my kid burned up a $5 board trying to learn to solder on a dev board, I wouldn't think twice about giving him a way to earn another $5 buy another one. Are they subsidizing me? I don't know.

     

    I had a discussion with a co worker recently, I grew up in a time of great technological advancement, my parents were technologically incompetent, even though my dad was a professional auto mechanic. When it came time to hook up cable, when it was invented, or the vcr, when it was invented, or the stereo, or adding a new 8 track deck to the car, I figured all that stuff out, game consoles, whatever and my parents encouraged me, and I learned a lot. Without google, now in my house, I wouldn't dare let my kids do that stuff, and they suffer for it. So getting these dev boards into their hands and giving them an opportunity to play, with my encouragement is a good thing.

     

    Just my opinion. BTW, love you shabaz :-)

     

    Mike

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to mconners

    My dad was the same! He didn't know what I was doing, but had the engineering spirit. He always encouraged me, even if it meant travelling miles just to find a store that sold an LED.

    The throwaway cost is a good point - would make people less scared to approach a PCB.

    I often nowadays purchase boards if they are a throwaway cost, since I might learn something from them, and no harm if I don't.

    This is the latest addition: It is a radio receiver board, I've no idea what it was used for but looks fairly ancient.

    Worth some experimentation time at some point!

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • alysson
    alysson over 10 years ago in reply to shabaz

    I'm not going to argue against any of that, Shabaz.

     

    Where I was last working (with teenaged students with complex needs), one of my students was learning the electronics-side of computer tech. If things had gone as planned, he would have been building projects on the Pi B the next term - soldering iron and all.

     

    USB hubs - tesco have a micro hub for about £6 - and there is no problem putting a dab of cyanoacrylate on the connector shell of a wireless dongle in order to keep it attached. This is (more or less) how I use my Pi's (albeit headless)

     

    I don't believe that the Zero is a replacement for the original Pi, but a tool for the more advanced user/student.

     

    I agree wholeheartedly about the SMT µUSB connector, which is why my original post mentioned the test point pads that may or may not represent a breakout point for a hard-wired USB and power wiring (which I use on my original Pi's, too).

     

    Having entered the workforce working with computers that had to be fixed with a soldering iron and a fistful of parts, I have no qualms about butchering circuit boards.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • alysson
    alysson over 10 years ago in reply to shabaz

    Ahhhh .... the same thing that I do. Picking up scrap stuff for spares or repairs - or for experimenting with is a brilliant approach - and quite satisfying, too.

     

    The last radio receiver board I tinkered with was entirely discrete components.