• Experts & Guidance
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
    • Or choose another store...
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
Documents Overview of the Raspberry Pi Zero
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Raspberry Pi requires membership for participation - click to join
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: spannerspencer
  • Date Created: 25 Nov 2015 2:07 PM Date Created
  • Last Updated Last Updated: 2 Nov 2016 12:49 PM
  • Views 3882 views
  • Likes 8 likes
  • Comments 23 comments
Related
Recommended

Overview of the Raspberry Pi Zero

Two models of Raspberry Pi inside 12 months spells an exciting year for hackers, makers, coders and tech heads around the world, and there are certain questions that immediately spring to mind when we hear about a brand new board.image

 

We'll get into a lot more detail about the Pi Zero in coming days, weeks and months, but right now here's a quick guide to get you up to speed as fast as possible.

 

What is the Raspberry Pi Zero?

While the Raspberry Pi 2 marks the top end of the platform's tech specs, the Pi Zero takes the opposite approach. This is, for all intents and purposes, an entry-level model that's been reduced both in price and size (being three times smaller than the original Raspberry Pi 1 series).

 

The Raspberry Pi Zero: Technical Specifications

  • CPU: Broadcom BCM2835, which can run at up to 1GHz.
  • RAM: 512MB
  • Power: 5V, supplied via micro USB connector, drawing 160mA (even when connected to an HD display).
  • Dimensions: 65mm x 30mm x 5mm
  • Video & Audio: 1080P HD video output. Audio output via mini-HDMI connector.
  • Storage: MicroSD card.
  • Operating System: Linux, installed via NOOBS.

image

The Raspberry Pi Zero: Inputs and Outputs

  • MicroSD Card Slot: The Pi Zero gets its storage space from a MicroSD card, which you'll need to install the operating system on.
  • Mini HDMI: Video output for the Pi Zero is by way of a mini-HDMI connector. In terms of their operation, these connectors perform identically to their larger versions. N.B. A mini-HDMI to standard HDMI adapter is included with the Pi Zero from element14.
  • Micro USB: You'll notice there are two micro USB connectors on the Pi Zero. One is for data (the connector on the left, if the MicroSD card slot is on the left), and one is for power. Don't get them mixed up. A micro USB "On the Go" to USB adapter is included with the Pi Zero from element14 so you can connect a USB hub, and therefore all your peripherals (keyboard, mouse etc).
  • GPIO: The Pi Zero has the same 40 pin General Purpose Input/Output connections as the Model A+, B+ and RPi2, but the connector pins are unpopulated. So if you want to use the GPIO, you'll either have to solder the required pins in place, or solder your connections directly to the Pi Zero.
  • RUN Mode Pins: There are two unpopulated RUN mode pins, which can be used to connect a reset button to the Pi Zero. Again, you'll either have to add the pins yourself, or solder a button straight to the board.
  • Composite Video: Here's an interesting one. There's an RCA composited video output via two (unpopulated) pins, so you can hook the Pi Zero up to older display equipment that accepts a phono plug as an input. You can check out the RCA video output in use in our Raspberry Pi Zero Retro Gaming System project right here.

 

More about the Raspberry Pi Zero

  • raspberry_pi
  • pi_zero
  • raspberrypi
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • ipv1
    ipv1 over 8 years ago +3
    This is excellent and is going to be a craze with people who want to replace their arduinos with something a little more juicy. The arduino YUN was something that ran linux and had WiFi. This would be…
  • rew
    rew over 8 years ago in reply to seulater +2
    I think you're wrong. The Raspberry pi Zero is NOT intended to be used with keyboard and mouse. It is intended to be tucked away somwhere and "do something" that you have developed on your "desktop" pi…
  • SGarciaV
    SGarciaV over 8 years ago in reply to ipv1 +2
    Although a higher end solution than the Arduino, cost is not everything. Lots of people like the Arduino because you can open up the IDE, whip up a program, and run it on the board. There is no operating…
Parents
  • ipv1
    ipv1 over 8 years ago

    This is excellent and is going to be a craze with people who want to replace their arduinos with something a little more juicy. The arduino YUN was something that ran linux and had WiFi. This would be something between the YUN and the Nano with a small enough form factor to hack it into small places.

    Brilliant!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ipv1
    ipv1 over 8 years ago

    This is excellent and is going to be a craze with people who want to replace their arduinos with something a little more juicy. The arduino YUN was something that ran linux and had WiFi. This would be something between the YUN and the Nano with a small enough form factor to hack it into small places.

    Brilliant!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • SGarciaV
    SGarciaV over 8 years ago in reply to ipv1

    Although a higher end solution than the Arduino, cost is not everything. Lots of people like the Arduino because you can open up the IDE, whip up a program, and run it on the board. There is no operating system to deal with. For people who want to start learning about embedded systems, micro controllers and SOCs, the Arduino is hard to beat.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 8 years ago in reply to SGarciaV

    Isn't there a Wiring  clone/implementation on the RPI if so you wouldn't really need to worry too much about the lack of easy IDE

    • Cancel
    • Vote Up 0 Vote Down
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
An Avnet Company © 2023 Premier Farnell Limited. All Rights Reserved.