Documents Raspberry Pi 3 Model B Technical Specifications
  • Blog
  • Forum
  • Documents
  • Events
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Raspberry Pi requires membership for participation - click to join
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 22 Feb 2016 8:38 PM Date Created
  • Last Updated Last Updated: 10 May 2021 7:23 PM
  • Views 5467 views
  • Likes 15 likes
  • Comments 65 comments
Related
Recommended

Raspberry Pi 3 Model B Technical Specifications

 NEW! Raspberry Pi 3 Model B
Comparison ChartFrequently Asked QuestionsUnboxing Video
40 Pin OutPi3 Video Arcade Project

 

         

                                                                     
   

NEW! Raspberry Pi 3 Model B

   

Buy NowBuy NowBuy NowBuy Now

   

Learn More

   

 

   

Key Improvements from Pi 2 Model B to Pi 3 Model B:

 Next Generation QUAD Core Broadcom BCM2837 64bit processor

 Processor speed has increased from 900MHz on Pi 2 to 1.2Ghz

 BCM43438 WiFi on board

 Bluetooth Low Energy (BLE) on board

 Upgraded switched power source up to 2.5 Amps (can now power even more powerful devices over USB ports)

 

Other Technical Specification:

 40pin extended GPIO

 4 x USB 2 ports

 4 pole Stereo output and Composite video port

 Full size HDMI output

 CSI camera port for connecting the Raspberry Pi cameraRaspberry Pi camera

 DSI display port for connecting the Raspberry Pi touch screen displayRaspberry Pi touch screen display

 Micro SD port for loading your operating system and storing data

 Upgraded switched Micro USB power source (now supports up to 2.5 Amps)

 The same form factor as the Pi 2 Model BPi 2 Model B, - the only difference is the location of the onboard LEDs

  • tech specs
  • pi3
  • raspberry_pi_space
  • raspberry pi 3
  • technical specifications
  • Share
  • History
  • More
  • Cancel
Anonymous

Top Comments

  • spannerspencer
    spannerspencer over 6 years ago in reply to madshenriksen +3

    There's dedicated hardware for lots of things, but I'd certainly be interested in seeing if the Pi3 can be put to this kind of purpose -- my NAS is getting kind of old, and uses a lot more juice than a…

  • madshenriksen
    madshenriksen over 6 years ago in reply to spannerspencer +3

    Exactly Spanner Spencer.

     

    The Raspberry approach was chosen because it could fill my need at a very low cost, and with low power (I haven't look at the power consumption of other NAS hardware).

     

    I haven…

  • Problemchild
    Problemchild over 6 years ago in reply to cstanton +3

    Yes Chris. to be honest the software RAID under Linux has surpassed the speed of the HW implementations for years at least under x86 ...

    Obviously the ability to off load that function to some H/W is good…

Parents
  • rdcell@141
    rdcell@141 over 4 years ago

    hello friends, i am using rpi 3 for serial communication with my communicating device which works at 300 baud rate with computer. But when i access my device with rpi 3 with putty software ( on serial port only) it gives garbage value. why is it so? please help.

    • Cancel
    • Up 0 Down
    • Reply
    • More
    • Cancel
  • mconners
    mconners over 4 years ago in reply to rdcell@141

    Roger may very well be correct that the Pi does not go that low. I have not tried it, but there are more things at play than just baud rate, if it can do 300 baud.

     

    There are also start bits, stop bits and parity settings that must match on both sides. You'll often see this denoted as 8N1, which would be 8 data bits, 1 stop bit and no parity. Check the settings on both sides and make sure they are the same.

    Most modern telecommunications programs, such as putty,  will allow you to change the values to match. If your framing is off, your data wil be garbage, even if the baud rate is the same.

     

    Also, realize the pi puts out data at ttl levels, many data communications devices expect to see levels of +12v for a 1 and -12v for a zero.

     

     

    Mike

    • Cancel
    • Up +1 Down
    • Reply
    • More
    • Cancel
  • golddogesmax1
    golddogesmax1 over 3 years ago in reply to mconners

    hi

    • Cancel
    • Up 0 Down
    • Reply
    • More
    • Cancel
Comment
  • golddogesmax1
    golddogesmax1 over 3 years ago in reply to mconners

    hi

    • Cancel
    • Up 0 Down
    • Reply
    • More
    • Cancel
Children
No Data