Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi PoE (Power Over Ethernet) Hat
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 13 Mar 2018 1:45 PM Date Created
  • Last Updated Last Updated: 19 Jun 2020 12:12 PM
  • Views 12823 views
  • Likes 13 likes
  • Comments 41 comments
Related
Recommended

Raspberry Pi PoE (Power Over Ethernet) Hat

image
NEW! Raspberry Pi 3 Model B+

Technical Specifications | Compliance Documentation | GPIO Pin Out | Unboxing Video | Benchmark Tests | Frequently Asked Questions | Comparison Chart | Pi PoE Hat | Pi Accessories | Pi Projects

 

Boot and power your Raspberry Pi 3 B+ or 4 over Ethernet.

 

imageimage

Buy NowBuy NowBuy Now

 

The official Power over Ethernet (PoE) add-on board for the Raspberry Pi 3 Model B+ or Raspberry Pi 4! Use this HAT to power a Raspberry Pi via an Ethernet cable, removing the need for a separate power supply, an ideal solution for embedded and IoT projects. For Raspberry Pi 3 Model B+ and onwards, an 802.3af compliant POE injector, switch, or router device is required (not included).

 

  • Power over Ethernet 802.3af compliant
  • Power over Ethernet Boot (PXE Boot)
  • Class 2 device
  • Fully isolate Switched-Mode Power Supply (SMPS)
  • 36-56V Input Voltage
  • 5V Output Voltage
  • Supplies up to 2.5A
  • Fan Control
  • Plug-and-play compatibility with Raspberry Pi 3 Model B+ or Raspberry Pi 4

 

Best of all, it fits within the official Raspberry Pi Case!

An Alternative Product: Buy NowBuy Now

  • power over ethernet
  • rpi4
  • 3b+
  • raspberry pi 4
  • poe
  • raspberry pi 3 model b plus (b+)
  • power_over_ethernet
  • rpi3b+
  • 4
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 8 years ago +6
    It does seem that this has been designed for the single purpose of powering the RPi over Ethernet. They have provided access to the camera and display connectors, which is nice. HOWEVER the GPIO has been…
  • e14phil
    e14phil over 8 years ago in reply to balearicdynamics +5
    Hey Enrico, This will provide the Pi with its 5V 2.5A needed as if it were plugged into the official power supply. More info about upcoming roadtests and more information on the PoE board will be released…
  • dhussenet
    dhussenet over 8 years ago +4
    Hi Everybody. I'm sorry but it will not use the 40pin GPIO connector. Power is taken directly on the RJ45 connector, and on the Pi3 B+, there's a new 4pin connector (close to the USB connectors) called…
Parents
  • balearicdynamics
    balearicdynamics over 8 years ago

    If the powering is sufficient to run the PI at full speed this is a nice and cheap tool. What is the PI is attached to something else? Need a road test image

     

    Enrico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14phil
    e14phil over 8 years ago in reply to balearicdynamics

    Hey Enrico, 

    This will provide the Pi with its 5V 2.5A needed as if it were plugged into the official power supply.

    More info about upcoming roadtests and more information on the PoE board will be released soon.

    Phil

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14phil
    e14phil over 8 years ago in reply to balearicdynamics

    Hey Enrico, 

    This will provide the Pi with its 5V 2.5A needed as if it were plugged into the official power supply.

    More info about upcoming roadtests and more information on the PoE board will be released soon.

    Phil

    • Cancel
    • Vote Up +5 Vote Down