Raspberry Pi
  • Products
  • More
Raspberry Pi
Documents Raspberry Pi PoE (Power Over Ethernet) Hat
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 13 Mar 2018 1:45 PM Date Created
  • Last Updated Last Updated: 19 Jun 2020 12:12 PM
  • Views 11528 views
  • Likes 13 likes
  • Comments 41 comments
Related
Recommended

Raspberry Pi PoE (Power Over Ethernet) Hat

image
NEW! Raspberry Pi 3 Model B+

Technical Specifications | Compliance Documentation | GPIO Pin Out | Unboxing Video | Benchmark Tests | Frequently Asked Questions | Comparison Chart | Pi PoE Hat | Pi Accessories | Pi Projects

 

Boot and power your Raspberry Pi 3 B+ or 4 over Ethernet.

 

imageimage

Buy NowBuy NowBuy Now

 

The official Power over Ethernet (PoE) add-on board for the Raspberry Pi 3 Model B+ or Raspberry Pi 4! Use this HAT to power a Raspberry Pi via an Ethernet cable, removing the need for a separate power supply, an ideal solution for embedded and IoT projects. For Raspberry Pi 3 Model B+ and onwards, an 802.3af compliant POE injector, switch, or router device is required (not included).

 

  • Power over Ethernet 802.3af compliant
  • Power over Ethernet Boot (PXE Boot)
  • Class 2 device
  • Fully isolate Switched-Mode Power Supply (SMPS)
  • 36-56V Input Voltage
  • 5V Output Voltage
  • Supplies up to 2.5A
  • Fan Control
  • Plug-and-play compatibility with Raspberry Pi 3 Model B+ or Raspberry Pi 4

 

Best of all, it fits within the official Raspberry Pi Case!

An Alternative Product: Buy NowBuy Now

  • power over ethernet
  • rpi4
  • 3b+
  • raspberry pi 4
  • poe
  • raspberry pi 3 model b plus (b+)
  • power_over_ethernet
  • rpi3b+
  • 4
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 8 years ago +6
    It does seem that this has been designed for the single purpose of powering the RPi over Ethernet. They have provided access to the camera and display connectors, which is nice. HOWEVER the GPIO has been…
  • e14phil
    e14phil over 8 years ago in reply to balearicdynamics +5
    Hey Enrico, This will provide the Pi with its 5V 2.5A needed as if it were plugged into the official power supply. More info about upcoming roadtests and more information on the PoE board will be released…
  • dhussenet
    dhussenet over 8 years ago +4
    Hi Everybody. I'm sorry but it will not use the 40pin GPIO connector. Power is taken directly on the RJ45 connector, and on the Pi3 B+, there's a new 4pin connector (close to the USB connectors) called…
Parents
  • dhussenet
    dhussenet over 8 years ago

    Hi Everybody. I'm sorry but it will not use the 40pin GPIO connector.

     

    Power is taken directly on the RJ45 connector, and on the Pi3 B+, there's a new 4pin connector (close to the USB connectors) called PoE. So, 2 pins for the input voltage from the RJ45 connector (35-56V tolerant I think, so conform with 48V of the 802.3af), and 2 pins for the output voltage (5V@2.5A max)

     

    The HAT will be connected to this connector to do the job, leaving the 40pin connector completely free

     

    So, no additional wires like a short RJ45 patch, or whatever.

     

    The "+" : the Pi3 and the Hat will fit in the standard enclosure !

     

    Price should be around 15 euros I think

     

    Hope I helped !

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • nenner
    nenner over 8 years ago in reply to dhussenet

    I think the 4 pins poe hat connector has Rx+ - Tx+ - 

    should be asey to check with voltmeter

    and that output power 5 V goes to GPIO connector .

    Can any one comment ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dhussenet
    dhussenet over 8 years ago in reply to nenner

    Hi Thomas

     

    It's definitely sure it's this connector. But you cannot use a voltmeter directly on it without the PoE HAT : A PoE802.3af injector (a simple module, or a port from a PoE switch, whatever) doesn't deliver 48V "just like this", because you can also plug a no compliant PoE device on it, and if you have 48V on the line.... bzzzzz, ciao your device ! On a PoE compliant device, you have a PD chip which establish a kind of connection with the injector, with a very low voltage, and if the communication is approved by the injector, 48V will be injected.

     

    So :

    no HAT plugged -> no PD chip on the Raspberry side -> no voltage from the injector -> you can keep your voltmeter on your shelf

    HAT plugged -> PD chip present -> 48V will be delivered -> the Pi will boot -> as it will be visible, your voltmeter can still stay on your shelf image

     

    For information, the power is delivered on secondary pairs on the ethernet cable : primary pairs 1-2, 3-6 are commonly used for data transmission up to 100Mb/s (maybe can do gigabit, but not sure). When the 2 others are used (4-5, 7-8), so 1Gb/s is available.

     

    If you want more explanation, don't forget google is your friend image There's a lot of documentation online on this subject

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rew
    rew over 8 years ago in reply to dhussenet

    Thomas,

    For your learning enjoyment:

     

    100 MBPS ethernet has a TX pair and an RX pair. 100 megabits, so every 10ns a new bit on each of the lines.

     

    1 GBPS ethernet uses al four pairs. Bidirectional (i.e. for communications in both directions at the same time!), two bits per bitperiod (4 signal levels), and at 8ns per bit. All this combines to get a 10x higher datarate. (4x from 4x more line pairs, 2x from 2 bits/period and 1.25x from the higher signalling rate). Because the signalling rate is almost the same, most "officially for 100Mbps" cables can also handle 1Gbps without trouble.

     

    I did not know on what pairs of wires the power was transmitted, but a quick readup learns me that you get to chose. Either the (100Mbps) data pairs, or the others. You'd want the first if you have a "one cat5 can transmit two ethernet signals"  construct somewhere. The other might be slightly easier electrically. For 1Gbps both choices result in power and data sharing conductor pairs.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rew
    rew over 8 years ago in reply to dhussenet

    Thomas,

    For your learning enjoyment:

     

    100 MBPS ethernet has a TX pair and an RX pair. 100 megabits, so every 10ns a new bit on each of the lines.

     

    1 GBPS ethernet uses al four pairs. Bidirectional (i.e. for communications in both directions at the same time!), two bits per bitperiod (4 signal levels), and at 8ns per bit. All this combines to get a 10x higher datarate. (4x from 4x more line pairs, 2x from 2 bits/period and 1.25x from the higher signalling rate). Because the signalling rate is almost the same, most "officially for 100Mbps" cables can also handle 1Gbps without trouble.

     

    I did not know on what pairs of wires the power was transmitted, but a quick readup learns me that you get to chose. Either the (100Mbps) data pairs, or the others. You'd want the first if you have a "one cat5 can transmit two ethernet signals"  construct somewhere. The other might be slightly easier electrically. For 1Gbps both choices result in power and data sharing conductor pairs.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • richard_damon
    richard_damon over 8 years ago in reply to rew

    Power over Ethernet uses the fact that the signals are defined to have transformer isolation one each pair. With POE, the voltage is applied between the center taps of the pairs.

     

    You need the transformer coupling because the devices on the two ends likely have differing ground references, so you need the transformers for isolation anyway. By applying the DC bias to the center taps, POE is largely transparent to the data transmission.

    • Cancel
    • Vote Up +1 Vote Down