Documents Raspberry Pi PoE (Power Over Ethernet) Hat
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 13 Mar 2018 1:45 PM Date Created
  • Last Updated Last Updated: 19 Jun 2020 12:12 PM
  • Views 10713 views
  • Likes 13 likes
  • Comments 41 comments
Related
Recommended

Raspberry Pi PoE (Power Over Ethernet) Hat

image
NEW! Raspberry Pi 3 Model B+

Technical Specifications | Compliance Documentation | GPIO Pin Out | Unboxing Video | Benchmark Tests | Frequently Asked Questions | Comparison Chart | Pi PoE Hat | Pi Accessories | Pi Projects

 

Boot and power your Raspberry Pi 3 B+ or 4 over Ethernet.

 

imageimage

Buy NowBuy NowBuy Now

 

The official Power over Ethernet (PoE) add-on board for the Raspberry Pi 3 Model B+ or Raspberry Pi 4! Use this HAT to power a Raspberry Pi via an Ethernet cable, removing the need for a separate power supply, an ideal solution for embedded and IoT projects. For Raspberry Pi 3 Model B+ and onwards, an 802.3af compliant POE injector, switch, or router device is required (not included).

 

  • Power over Ethernet 802.3af compliant
  • Power over Ethernet Boot (PXE Boot)
  • Class 2 device
  • Fully isolate Switched-Mode Power Supply (SMPS)
  • 36-56V Input Voltage
  • 5V Output Voltage
  • Supplies up to 2.5A
  • Fan Control
  • Plug-and-play compatibility with Raspberry Pi 3 Model B+ or Raspberry Pi 4

 

Best of all, it fits within the official Raspberry Pi Case!

An Alternative Product: Buy NowBuy Now

  • power over ethernet
  • rpi4
  • 3b+
  • raspberry pi 4
  • poe
  • raspberry pi 3 model b plus (b+)
  • power_over_ethernet
  • rpi3b+
  • 4
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 7 years ago +6
    It does seem that this has been designed for the single purpose of powering the RPi over Ethernet. They have provided access to the camera and display connectors, which is nice. HOWEVER the GPIO has been…
  • e14phil
    e14phil over 7 years ago in reply to balearicdynamics +5
    Hey Enrico, This will provide the Pi with its 5V 2.5A needed as if it were plugged into the official power supply. More info about upcoming roadtests and more information on the PoE board will be released…
  • dhussenet
    dhussenet over 7 years ago +4
    Hi Everybody. I'm sorry but it will not use the 40pin GPIO connector. Power is taken directly on the RJ45 connector, and on the Pi3 B+, there's a new 4pin connector (close to the USB connectors) called…
Parents
  • davednl
    davednl over 7 years ago

    Hey guys,

    Just got a brand new Pi3B+ with PoE Hat.

    If I plug it in to a PoE injector or to my Ubiquiti PoE switch it does not start at all as in no leds burning.

    If I use the normal power adaptor it boots without problem. I can even see the cpu cooler go on every now and then.

    Do I still need to configure something in raspi-config to enable the PoE hat?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to davednl

    Hi Dave,

     

    Does it work if you disconnect all additional loads (such as USB drives etc)?

    Have you enabled PoE on your switch? What precise model is your switch, does it support standards-based PoE?

    Some PoE injectors are not standards based.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • davednl
    davednl over 7 years ago in reply to shabaz

    Hi Shabaz,

     

    It is just the plain Pi without anything connected to USB.

    I have a Ubiquity 8 Port 150W switch.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • troyfontaine
    troyfontaine over 7 years ago in reply to davednl

    Hi Dave,

     

    Is the PoE Port set to 802.3af (PoE) and not passive 24v?

     

    I believe those switches can do both-but the Pi is only made for 802.3af.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • davednl
    davednl over 7 years ago in reply to troyfontaine

    Hi Troy,

    yup the port is configured for 802.3AF.

    24V would kill the Pi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • davednl
    davednl over 7 years ago in reply to troyfontaine

    Hi Troy,

    yup the port is configured for 802.3AF.

    24V would kill the Pi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • troyfontaine
    troyfontaine over 7 years ago in reply to davednl

    Hi Dave,

     

    Do you have access to any PoE injectors in that case?

     

    The two hats I ordered worked fine off the hop-though I’ve read about concerns with the surface mounted 4-pin connector on the hat.  I’ve used them with a Ubiquiti PoE inejector that came with an UAP-AC-PRO and with a netgear switch, I think I did briefly test one in my US-8-60w without issue.