RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Evaluating Oscilloscope Bandwidth and Rise Time ---R&S RTM3K Oscilloscope Road-Test Review
  • Blogs
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: snidhi
  • Date Created: 23 Jul 2018 4:44 PM Date Created
  • Views 3965 views
  • Likes 11 likes
  • Comments 7 comments
Related
Recommended
  • rtm3004
  • bandwidth
  • rise time
  • intrinsic_risetime
  • rhode&schwarz
  • rhode & schwartz oscilloscope
  • noise measurement
  • rise-time
  • fft
  • rhode-schwarz
  • signal integrity

Evaluating Oscilloscope Bandwidth and Rise Time ---R&S RTM3K Oscilloscope Road-Test Review

snidhi
snidhi
23 Jul 2018

  • Evaluating R&S RTM 3K Oscilloscope Bandwidth and Rise time
    • Calculating the BW of R&S RTM
    • FFT functionality Tests with the R&S Signal Generator
    • Evaluating the fastest Rise time (tr) of R&S RTM 3004

 

Evaluating R&S RTM 3K Oscilloscope Bandwidth and Rise time

 

This blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review

 

Calculating the BW of R&S RTM

 

The generic rule is that the oscilloscope bandwidth should be at-least five times faster than the fastest signal to be measured in the system under test. This allows you to capture the fifth harmonic with minimum signal attenuation and determines the overall shape of the displayed signal.

image

 

An accurate way to measure is to determine the rise and fall times of the fastest signal in the system. And then calculate the maximum " practical" frequency component of this signal also known as the "knee" frequency. All fast edges have an infinite spectrum of frequency components. However, there is an inflection (or “knee”) in the frequency spectrum of fast edges where frequency components higher than fknee are insignificant in determining the shape of the signal.

 

image

Fig: Ref Book Johnson, Dr. Howard W. “High-speed Digital Design – A Handbook of Black Magic

 

After calculating the signal rise time with the above formula the oscilloscope Bandwidth can be chosen depending on the accuracy desired for the measurements.

 

Calculate the oscilloscope bandwidth and the signal measurement accuracy

 

image

Fig: Factors which determine the Oscilloscope BW and measurement

 

Signal Rise time (10%-90%)Fknee SignalScope BW with 20% timing AccuracyScope BW with 3% timing Accuracy
100 ns500 MHz5MHz9.50 MHz
1ns500 MHz500 MHz950 MHz
500ps (RTM 3004 fastest vertical setting)1GHz1.0 GHz1.9 GHz
100 ps5GHz5GHz9.5 GHz

Fig: Theoretical calculations on how the signal rise time can be measured accurately

 

Here one can see that signals with 500 ps rise time can only be measured with low timing accuracy and the best accuracy measurement can be done maximum for a 1ns signal.

 

image

Fig: Rise time of different digital device ICs

 

image

Fig: Digital Protocol Rise times (Tr)

FFT functionality Tests with the R&S Signal Generator

In this setup an R&S signal generator was used to generate a sine wave and sweep across the full BW of the oscilloscope from 100MHz to the 1.5 GHz. And as mentioned in the theory blog one can clearly see that the signal starts to attenuate significantly as it nears the -3dB roll off edge.

image

Fig: Some measurements were taken with 10dBm attenuated signal

 

image

Fig: Test Setup of the RTM 3004 with the Signal Generator

 

image

Fig: Setup of RTM 3004 for FFT Measurement Sweep

 

image

Fig: Averaged Time Domain Measurement for 100MHz sine wave from signal generator

 

image

Fig: FFT Measurement Sweep at 100 MHz at 10dBm

 

image

Fig: FFT Measurement Sweep at 100 MHz Veff Vertical scale

 

image

Fig:  Averaged Time Domain Measurement Signal for 500MHz sine wave from signal generator

 

image

Fig: FFT Measurement Sweep at 500 MHz at 0dBm

 

image

Fig: FFT Measurement Sweep at 714 MHz at 0dBm

 

image

Fig: Time Domain Measurement for 1GHz sine wave from signal generator

image

Fig: FFT Measurement Sweep at 1GHz at 0dBm

 

image

Fig: FFT Measurement Sweep at 1GHz Closer look at the attenuation

 

image

Fig: FFT Measurement Sweep at 1GHz Closer look at the attenuation

 

image

Fig: FFT Measurement Sweep at 1.2GHz Closer look at the attenuation

 

In the measurements above one can clearly see that the amplitude attenuation starts at a frequency shortly after 714 MHz for the input sine signal. And at 1 GHz the signal attenuation has reached -1.8dBm and starts to move towards the -3dBm attenuation at frequencies higher than 1GHz (as can be seen below).

 

image

Fig: Chasing the -3dB roll off Attenuation in the signal at the edge of bandwidth

 

image

Fig: -3dB Attenuation is reached at little after 1.1GHz

 

Hence it can be concluded that the RTM 3004 performs better than its specifications as the -3dB roll off occurs after the oscilloscope bandwidth limit is reached and not before as is the case with many low range oscilloscopes.

 

Evaluating the fastest Rise time (tr) of R&S RTM 3004

 

The rise time measurements as published by Keysight for their 1GHz range of oscilloscope Ref.  The aim of the upcoming tests is to verify rise time for R&S RTM 3004 oscilloscope.

image

Fig: Response of 1 GHz Keysight oscilloscopes

 

In this setup a very fast 20ps signal was input to the RTM 3004 channel 1 set to maximum 5GSa/s sampling rate from a sampling oscilloscope. A sampling oscilloscope is characterized by an architecture which samples the input signal before amplification or attenuation. These scopes have much higher bandwidth than normal oscilloscopes but have a lower input dynamic range and a lower safe input voltage.

image

Fig: Basics how a Sampling Scope works

 

A special 50 ohm highly insulated cable (as short as possible) was used to make the connection between the devices.

 

The experimental test setup

 

image

Fig: Test Setup of the RTM 3004 with the Sampling oscilloscope

 

image

Fig: Specifications and Setup of the 27 ps fast input signal

 

image

Fig: The fastest edge that the RTM 3004 can measure is 345ps

 

image

Fig: Averaging The fastest edge that the RTM 3004 can measure 325 ps

 

image

Fig: The fastest edge the 8GHz Lecroy could measure is 68 ps

 

 

Hence one can conclude that the fastest signal the R&S RTM 3004 can measure is in the range of 320ps therefore performing better in the 1GHz bandwidth range and stretches the bandwidth upto 1.09375 GHz but with 20% timing accuracy(or less even).

  • Sign in to reply

Top Comments

  • three-phase
    three-phase over 7 years ago +4
    I am a bit confused by the statement at the end of your first paragraph; So if you want to see a signal with 100ns rise time the scope rise time should be 500 ns. Wouldn't the scope rise time need to be…
  • danielw
    danielw over 7 years ago +4
    Excellent work and a good read!
  • DAB
    DAB over 7 years ago +3
    Nice update. DAB
Parents
  • three-phase
    three-phase over 7 years ago

    I am a bit confused by the statement at the end of your first paragraph;

    So if you want to see a signal with 100ns rise time the scope rise time should be 500 ns.

     

    Wouldn't the scope rise time need to be 20ns or less to view a signal with a rise time of 100ns?

     

    Kind regards

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • snidhi
    snidhi over 7 years ago in reply to three-phase

    oops yes, its a typo error I correct it now. Thanks for pointing it out

     

    Cheers image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 7 years ago in reply to snidhi

    No worries, doesn't take too much to confuse me these days.

     

    Kind regards

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • three-phase
    three-phase over 7 years ago in reply to snidhi

    No worries, doesn't take too much to confuse me these days.

     

    Kind regards

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • snidhi
    snidhi over 7 years ago in reply to three-phase

    Thanks three-phase for reading it thoroughly and please let me know if anything else has gone haywire. image

     

    Cheers