RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs LED Road Test - Induction Heating Reflow Soldering - Blog 16 Jan12
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: dougw
  • Date Created: 13 Jan 2016 5:09 AM Date Created
  • Views 2292 views
  • Likes 9 likes
  • Comments 6 comments
Related
Recommended
  • induction_heating
  • lighting
  • ledroadtestplus
  • würth
  • reflow_soldering
  • texas_instruments
  • led_road_test

LED Road Test - Induction Heating Reflow Soldering - Blog 16 Jan12

dougw
dougw
13 Jan 2016

Traditional reflow systems use a conveyor that physically moves PCBs through various IR heated zones to achieve the desired time versus temperature profile, but this is not well suited to a (very) small prototype operation like my house. In my last blog I investigated hot air heating of a substrate for reflow soldering of SMT LEDs to metal core PCBs. This time I am investigating the use of induction heating to accomplish the same task. Induction heating is touted as the next great method of cooking, boasting fast, accurate and power efficient cooking. It would seem to be well suited to reflow soldering - fast, simple and precisely controllable without any mess. It turns out to be a bit more complicated than I had envisioned. There is some potential for the inductive fields to generate large currents in some electronics circuitry, but I figure with the geometry involved here soldering LEDs is pretty safe. (If the LED lights up during the process, I'll know I'm inducing unwanted currents). If I have sensitive circuitry, I have some mumetal sheets that I can use to minimize magnetic fields in the PCB. Here is a video showing that it is easy enough to use induction heat for reflowing solder - it was successful on the first try:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The system was set to use 1500 Watts, which is too much for this size of steel plate and the temperature was not controlled well by the system. I am not yet familiar with induction heating systems and this was my first experience with them. I need to investigate if the lower power settings still permit high enough temperatures and how the temperature feedback system works. Maybe the sensor location is not set up for this shape of plate. The system has enough potential to keep experimenting with different heights, plate materials, geometries and power levels to improve performance. Overall this first experiment was successful, although not quite as controlled as I hoped. However the technique is promising and I expect it will get significantly better with a little research and practice.

 

I will wrap up this road test with one more blog summarizing the experience.

 

The LED Road Test page is here:

http://www.element14.com/community/roadTests/1481


The Lighting Group page is here:

Lighting


Here are links to my other blog entries for this road test:

LED Road Test - Proposal - Blog 0 Jan 1, 2016

Light Emitting Diodes Road Test - Blog 1 Nov 1

LED Road Test - 3D Printed Housings - blog 2 Nov 10

LED Road Test - Dodecahedron Light Fixture  Blog 3 Nov12

LED Road Test - Wearable Interactive Lights - Blog 4 - Nov 13

LED Road Test - Interactive Trophy - Blog 5 Nov 16

LED Road Test - Making Household Objects Interactive - Blog 6 Nov 22

LED Road Test - Power LEDs - Up & Running - Blog 7 Nov 24

LED Road Test - Star Wars - The Force Awakens - Blog 8 Nov 28

LED Road Test - Selfie Phenomenon - Blog 9 Nov 29

LED Road Test - MSP EXP430FR4133 Launchpad IDE - Blog 10 Dec 6

LED Road Test - Vehicle Situational Awareness System Blog 11 Dec 14

LED Road Test - Vehicle Situational Awareness System Indoor Demo - Blog 12 Dec 20

LED Road Test - Maple Leaf Christmas Decoration - Blog 13 Dec 24

LED Road Test - Vehicle Situational Awareness System - Detecting the Borg in the Driveway - Blog 14 Dec 26

LED Road Test - Reflow Soldering Power LEDs - Blog 15 Jan 10

LED Road Test - Induction Heating Reflow Soldering - Blog 16 Jan12

LED Road Test - Summary - Blog 17 Jan 15

 

Associated Video Links

LED Road Test Unboxing

MSP-EXP430FR4133 Demo

BLE LED Power On Test

BLE LED 3D Printed Housings 2

Dodecahedron Light Fixture

Creating a Light Fixture using 123D Design

Wearable Interactive Arc Reactor

Interactive Trophy

Interactive Illuminated Household Objects

Power LEDs Thermal Discussion

LED Ring Light

Star Wars - Let The Force Be With The Light

CCS Cloud Basics

UltrasonicDistanceMeter-Boot

VSAS Indoor Demo

Maple Leaf BLE LED Decoration

Maple Leaf CAD design

Vehicle Situational Awareness System in Operation

Vehicle Situational Awareness System Operating at Night

Reflow Soldering SMT LEDs

Induction Heating Reflow Soldering

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago +2
    Hi Doug, You're on fire (not literally ever I hope ) with all these experiments! jw0752 did some experiments a few months ago using the LDC1000 device, and that may help determining the eddy current effect…
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +1
    Would there not be an issue with the induction field acting upon the metal inside the LED as well causeing or potentially causing damage there, I know it worked in the video but this seems to be a potential…
  • jw0752
    jw0752 over 9 years ago +1
    Hi Doug, I have to admit that I do not know much about inductive heating. Very interesting to see your experiment. What is the frequency of the field that is generated by the stove? John
Parents
  • DAB
    DAB over 9 years ago

    Hi Douglas,

     

    There are several issues with induction heating various materials.

     

    You need iron rich material to heat properly.  Stainless steel does not do a good job as the crystal structure inhibits the magnetic fields.

     

    Aluminum is diamagnetic, which means it will do some interesting things in magnetic fields.

     

    Overall, I think if you get an old cast iron skillet, you can probably do a good job of controlling the temperature with your induction stove.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 9 years ago

    Hi Douglas,

     

    There are several issues with induction heating various materials.

     

    You need iron rich material to heat properly.  Stainless steel does not do a good job as the crystal structure inhibits the magnetic fields.

     

    Aluminum is diamagnetic, which means it will do some interesting things in magnetic fields.

     

    Overall, I think if you get an old cast iron skillet, you can probably do a good job of controlling the temperature with your induction stove.

     

    DAB
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.