Traditional reflow systems use a conveyor that physically moves PCBs through various IR heated zones to achieve the desired time versus temperature profile, but this is not well suited to a (very) small prototype operation like my house. In my last blog I investigated hot air heating of a substrate for reflow soldering of SMT LEDs to metal core PCBs. This time I am investigating the use of induction heating to accomplish the same task. Induction heating is touted as the next great method of cooking, boasting fast, accurate and power efficient cooking. It would seem to be well suited to reflow soldering - fast, simple and precisely controllable without any mess. It turns out to be a bit more complicated than I had envisioned. There is some potential for the inductive fields to generate large currents in some electronics circuitry, but I figure with the geometry involved here soldering LEDs is pretty safe. (If the LED lights up during the process, I'll know I'm inducing unwanted currents). If I have sensitive circuitry, I have some mumetal sheets that I can use to minimize magnetic fields in the PCB. Here is a video showing that it is easy enough to use induction heat for reflowing solder - it was successful on the first try:
The system was set to use 1500 Watts, which is too much for this size of steel plate and the temperature was not controlled well by the system. I am not yet familiar with induction heating systems and this was my first experience with them. I need to investigate if the lower power settings still permit high enough temperatures and how the temperature feedback system works. Maybe the sensor location is not set up for this shape of plate. The system has enough potential to keep experimenting with different heights, plate materials, geometries and power levels to improve performance. Overall this first experiment was successful, although not quite as controlled as I hoped. However the technique is promising and I expect it will get significantly better with a little research and practice.
I will wrap up this road test with one more blog summarizing the experience.
The LED Road Test page is here:
http://www.element14.com/community/roadTests/1481
The Lighting Group page is here:
Here are links to my other blog entries for this road test:
LED Road Test - Proposal - Blog 0 Jan 1, 2016
Light Emitting Diodes Road Test - Blog 1 Nov 1
LED Road Test - 3D Printed Housings - blog 2 Nov 10
LED Road Test - Dodecahedron Light Fixture Blog 3 Nov12
LED Road Test - Wearable Interactive Lights - Blog 4 - Nov 13
LED Road Test - Interactive Trophy - Blog 5 Nov 16
LED Road Test - Making Household Objects Interactive - Blog 6 Nov 22
LED Road Test - Power LEDs - Up & Running - Blog 7 Nov 24
LED Road Test - Star Wars - The Force Awakens - Blog 8 Nov 28
LED Road Test - Selfie Phenomenon - Blog 9 Nov 29
LED Road Test - MSP EXP430FR4133 Launchpad IDE - Blog 10 Dec 6
LED Road Test - Vehicle Situational Awareness System Blog 11 Dec 14
LED Road Test - Vehicle Situational Awareness System Indoor Demo - Blog 12 Dec 20
LED Road Test - Maple Leaf Christmas Decoration - Blog 13 Dec 24
LED Road Test - Reflow Soldering Power LEDs - Blog 15 Jan 10
LED Road Test - Induction Heating Reflow Soldering - Blog 16 Jan12
LED Road Test - Summary - Blog 17 Jan 15
Associated Video Links
Creating a Light Fixture using 123D Design
Wearable Interactive Arc Reactor
Interactive Illuminated Household Objects
Star Wars - Let The Force Be With The Light
Vehicle Situational Awareness System in Operation
Top Comments
-
Robert Peter Oakes
-
Cancel
-
Vote Up
+1
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
-
dougw
in reply to Robert Peter Oakes
-
Cancel
-
Vote Up
+1
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
dougw
in reply to Robert Peter Oakes
-
Cancel
-
Vote Up
+1
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children