RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs [RoadTest] pi-top #1: Unboxing and Setup
  • Blogs
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: fvan
  • Date Created: 9 May 2018 5:12 PM Date Created
  • Views 2025 views
  • Likes 10 likes
  • Comments 5 comments
Related
Recommended
  • RoadTest
  • review
  • pi-top

[RoadTest] pi-top #1: Unboxing and Setup

fvan
fvan
9 May 2018

FULL REVIEW: Pi-Top - A Raspberry Pi Laptop - Review

My pi-top arrived last week! To not keep you in the dark until the very last moment, I've decided to split up this review in multiple blog posts, each with a specific topic to cover. The actual review will then link to these blog posts along with a description and conclusion.

As the title suggests, this first blog post will cover the unboxing and setup of the pi-top, with some initial impressions of the product.

 

  • Unboxing
  • Physical Installation
  • Build Quality
  • pi-topOS

 

Unboxing

 

A big box from element14 was delivered last week Thursday. Inside were two things:

  • pi-top
  • Raspberry Pi 3B+

 

image

 

I didn't expect a Raspberry Pi 3B+ to be included, especially because the RoadTest description specified "Raspberry Pi not included". So thank you for adding one of those, it is much appreciated!

 

Upon closer inspection of the box, I did notice all the seals (main box and inventor's kit) had already been cut, the box was slightly damaged, and that the laptop was even put back in the box incorrectly. I'm not sure if this was done pre shipping or by customs, as the package was marked as hazardous most likely due to the laptop's battery. Perhaps rscasny can shed some light on this. Anyway, no bits were missing or damaged, which is most important.

 

imageimage

 

Inside the box, everything you can expect:

  • pi-top laptop
  • Power supply 18V/2.5A
  • Getting started guide which also contains a 8GB microSD card preloaded with pi-topOS
  • Inventor guide
  • Inventor kit containing a special breadboard and some components such as LED, LDR, ultrasonic sensor, buzzer, etc ...
  • Project cutouts to be used with the inventor kit

 

There is a slot foreseen inside the packaging to fit a Raspberry Pi, so it appears to be an option.

 

{gallery} Pi-Top Unboxing

image

01: The pi-top (inserted incorrectly). Power supply in the top-right corner, slot for Raspberry Pi in top-left corner.

image

02: The pi-top!

image

03: The keyboard slides down to reveal access to the electronics.

image

04: Under the pi-top is the inventor's kit.

image

05: The kit contains a special breadboard with various connectors and various components.

image

06: The power supply comes with different connectors.

image

07: Two booklets are included. The getting started guide and the inventor guide.

image

08: The Pi's microSD card is attached to the getting started guide.

image

09: Some cutouts are included to give the example projects an extra touch and more appealing appearance.

 

Physical Installation

 

The instructions to install the Raspberry Pi in the pi-top are clearly detailed in the getting started guide. There is even a miniature multi-tool present to screw/unscrew and to remove or insert the microSD card once the Pi is installed.

 

The Pi slides into two flexible USB connectors at the rear of the laptop. This gave me some trouble as one of the two connectors would bend and not connect. After some fiddling, both connectors were inserted correctly and I could fasten the Pi in place. The two USB ports seem to be used for the keyboard/trackpad combo and a USB port inside the laptop. The remaining two USB ports and the ethernet port are exposed at the back of the laptop.

 

imageimage

 

The pi-top hub connects to the Pi's HDMI and audio jack. The hub's audio jack is exposed at the back of the laptop along with the charger input. The Pi's GPIO are connected to the hub as well, but via the cooling bridge that is mounted on top.

 

That's all the physical installation there is for the base device. Additional modules such as a speaker or the inventor kit's breadboard can be added via the magnetic rails.

 

Build Quality

 

The pi-top is a good looking device. It feels solid, isn't too heavy or too big. The keyboard keys have a nice click to them and the screen has a 180° swivel, so the screen can sit flat.

 

There are however some imperfections to the entire assembly of the device.

 

The first one I discovered is that the keyboard slider isn't flush with the main body of the laptop:

imageimage

When sliding the keyboard back into place, I can also feel it slightly bump into the cooling bridge, even though it is screwed on tight. There should be a little bit more clearance on the inside of the device.

 

Finally, one of the magnetic rails wasn't glued into place properly. Using the magnetic multi-tool, one rail came loose easily, while the other remained in place. Easily fixed by adding some glue myself, though.

image

 

pi-topOS

 

The pi-top's native OS is ... pi-topOS. A customised Raspbian with some pi-top specific applications and interface.

 

The pi-topOS which is pre-flashed on the microSD card is not the latest version (released on 25/04), and as a consequence, does not support the Raspberry Pi 3B+ yet. That is quickly solved by downloading the latest image and flashing it onto the microSD card.

 

The image can be downloaded from the pi-top website, and flashed onto a microSD card using Etcher.

image

 

Upon first boot, some configuration is required with regards to language, keyboard layout, etc ...

 

{gallery} pitopOS

image

01: Start screen

image

02: Language selection. It's quite limited.

image

03: Country and time zone.

image

04: The keyboard layout selection is also very limited.

image

05: Networking setup.

image

06: Network connectivity working, and detecting available updates.

image

07: Network no longer connected when trying to install the updates.

image

08: The desktop!

 

The last step of the wizard checks for available updates after configuring network connectivity. When the wizard switches to the desktop to install the updates, it seems to disconnect the network and the update fails. There is no command to try again.

It's not a one off, as I was able to reproduce the same issue when installing the latest image on my pi-topCEED. The script should either wait for the device to reconnect to the network, or offer the possibility to retry the update.

 

What I do find a pity, is the supported languages. We are not native English speakers, and with my daughter being 8 years old, she doesn't master it yet. With the pi-top being marketed as an educational tool, I think supporting more languages is important.

The same applies to the documentation. Things are explained very well, in simple terms, but in English only.

 

That being said, the variety of applications and the structure of the desktop are excellent. Everything is neatly organised and easily accessible.

On one occasion, I did have an issue with the display. Rebooting the pi-top appears to have solved it for now, but it remains strange.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The pi-top also emits a very annoying, constant beep, when powered on. Even with the keyboard closed, it is clearly audible. I tried to record the sound using my phone, to give you an idea. You'll have to turn up the volume.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

That's it for part 1. See you next time!

  • Sign in to reply

Top Comments

  • three-phase
    three-phase over 8 years ago +1
    Nice start to your review, look forward to the updates. Kind regards
  • vlaine
    vlaine over 8 years ago +1
    Nice first part. Can’t wait to see the rest. I noticed the high pitch sound too. I think it comes from the cooling bridge. I got used to it.
Parents
  • vlaine
    vlaine over 8 years ago

    Nice first part.  Can’t wait to see the rest.

    I noticed the high pitch sound too.  I think it comes from the cooling bridge.  I got used to it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vlaine
    vlaine over 8 years ago

    Nice first part.  Can’t wait to see the rest.

    I noticed the high pitch sound too.  I think it comes from the cooling bridge.  I got used to it.