RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs SimpleLink™︎ Sub-1 GHz Wireless Microcontroller - Check  Received Signal Strength
  • Blogs
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: Jan Cumps
  • Date Created: 21 Jun 2016 11:47 AM Date Created
  • Views 4749 views
  • Likes 6 likes
  • Comments 18 comments
Related
Recommended
  • RoadTest
  • cc1310
  • rssi
  • texas_instruments
  • sub1ghz
  • simplelink
  • launchpad
  • feature_tutorial
  • ti_rt

SimpleLink™︎ Sub-1 GHz Wireless Microcontroller - Check  Received Signal Strength

Jan Cumps
Jan Cumps
21 Jun 2016

Complexity: easy

What do you need:

  • two CC1310 LaunchPads Out of Box
  • A serial communication program (PuTTY or your personal favourite)

 

You can test the reception strength of the CC1310 radio straight away after you pulled the devices out of the box.

This exercise works with the pre-loaded firmware.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

You'll learn the range and the possibilities of the radios by trying this out from different locations in and out your lab.

 

 

Setting things up

 

If you have a Code Composer Studio installation, you will have the right USB drivers.

Plug in both LaunchPads, and check the serial port that's assigned to them.

 

You'll know how to do that for your operating system. Here' how it looks like on my localised Windows 10.

 

image

 

(you don't have to do this from one pc. This also works when each LaunchPad is attached to a different computer)

 

Fire up your serial communication program. If you don't have one installed, PuTTY is a possible option.

There is also a Terminal view available in CCS.

Set up communication as 115200 baud, 8 data bits, 1 stop, no parity, no flow control.

Select the first COM port.

image

 

Press the Reset button on top of one of the LaunchPads.

If nothing happens in the Terminal, press the Reset on the other one.

 

The one that reacts will be your TX device for today.

 

Click either button 1 or 2 to get a menu

Push button 2 until you are on the Mode line.

Press the left button to go select TX

image

 

Now start a second terminal program, and connect to the second serial port.

Push the Reset of the other launchpad. This one will become the receiver.

Press any button to go to the menu. This one is already in receive mode, so we don't have to change that.

Use the button 2 to navigate to Start, and press Button 1 to activate the receiving device.

 

image

It's now waiting for traffic.

image

 

Start the Communication

 

We're ready now to test the traffic.

Return to your first Terminal session. The one where you set the device to TX.

Use button 2 to navigate to Start

image

 

Each time you press Button 1, the device will transmit 10 packets.

In the receiver's terminal, you can see the count of received packages increase.

image

 

You'll also get an indication of the signal's strength. Keep pushing that button 1 of the transmitter, and the count will keep going up.

Try this exercise from different locations in your house, garden, neighbourhood, to appreciate the range of sub-1 GHz.

 

image

 

What if you have overwritten the Out-of-Box firmware

 

If you want to re-load the Out-of-Box firmware (the project will be included in the next TI-RTOS release, but currently unavailable), you can do that by:

 

  • Connecting  the LaunchPad.
  • Navigate to here: Welcome to CC1310 Launchpad
  • Locate the button that says ~ CC1310F128 and Click it

Done.

 

image

 

 

SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Check  Received Signal Strength
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Use SmartRF to Try Radio Configs
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Debug 2 LaunchPads at the Same Time
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Side Note: Recognise your PuTTY Sessions
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Side Note: Recognise your Code Composer Studio Sessions
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Debug a Sender to Receiver Conversation
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Side Note: Start a Fresh Project
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Create a Transmitter with SmartRF Studio Part 1
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Create a Transmitter with SmartRF Studio Part 2
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Sensor Controller Engine Part 1: Dry Run
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Sensor Controller Engine Part 2: RTOS Integration
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Sensor Controller Engine Part 3: Wake Up Options
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Side Note : Measure Power Use of Sensor Controller Engine
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - ToolKit for Range Testing

on TI E2E community: How to connect a CC1310 LaunchPad to the SIGFOX network

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 9 years ago +2
    Competition time: At the moment Robert Peter Oakes (rural area) and shabaz (metropolitan area) are the owners of the Sub-1GHz range record. Peter claims "the back of his garden". In Canada, where the gardens…
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Jan Cumps +2
    Cool he:
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Jan Cumps +2
    I don't think we got any closer to the Soviet Building Ideal than this:
Parents
  • Jan Cumps
    Jan Cumps over 9 years ago

    Competition time:

     

    At the moment Robert Peter Oakes (rural area) and  shabaz (metropolitan area) are the owners of the Sub-1GHz range record.

    Peter claims "the back of his garden". In Canada, where the gardens are long (and high) that's impressive. Shabaz says "at least a housing block, 290 metres".

    (TI claims 10s of kilometers with their CC112X device - but that requires mountain ranges, few other signals )

     

    I also live in a metropolitan setting, so I'm trying to do better than shabaz.

    And I'm going to do the attempt with two very nice antennas that he has kindly given me.

     

    image

     

    They are two Pulse Electronics "Outdoor 868 & 915 MHz Antennas". 18 cm decent quality flexible antennas with an SMA connector.

    Outdoor means that they can widstand the elements - in particular UV.

    image

     

    Electrical Specifications

    • Frequency [MHz] 868 - 928
    • Nominal Impedance [Ω] 50
    • Return Loss (dB) -8
    • Gain (dBi) 2
    • Polarization Omnidirectional

     

    I now need to order conversion material to connect the LaunchPad's male Murata JSC connector to the antenna's male SMA connector, and a few 0R resistors to convert the CC1310 LaunchPads from PCB antenna to external.

    The on-board connector (Murata MM5829-2700) is very tiny, but good quality. But the miniaturisation has its impact: the female connector that fits on that has a guaranteed life cycle of no more than 30 connections.

    ,image

    I'm going to purchase 2 female JSCs and 2 female SMAs. I'll then mount the transmitter LaunchPad on my balcony in Schaarbeek, Brussels.

    I'll carry the receiver with me trough the area. It's a hilly area here and my house is on the top of one of the hills.

    It's possible that I loose contact and gain it back when moving up the next hill.

    A big disadvantage is that the national Radio and TV tower is very close by (as in: I can see it from my street)

    image

     

    If I don't post here again in the next few days, it may be because one of the following entities doesn't like my endeavours.

    image

     

    Tell 'm I did it for science image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Jan Cumps

    jancumps wrote:

     

    ...

     

    I now need to order conversion material to connect the LaunchPad's male Murata JSC connector to the antenna's male SMA connector, and a few 0R resistors to convert the CC1310 LaunchPads from PCB antenna to external.

    The on-board connector (Murata MM5829-2700) is very tiny, but good quality. But the miniaturisation has its impact: the female connector that fits on that has a guaranteed life cycle of no more than 30 connections.

    ...,

    I'm going to purchase 2 female JSCs and 2 female SMAs. ..

     

     

    I decided to do this different. I've ordered two antenna evaluation kits that contain the adapters I need, but also an additional set of PCB antenna designs for several frequency ranges.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to DAB

    I really don't know what to expect. I'm new to the subject.

    The antenni are collateral goods. I needed the conversion cables that are in this kit.

    but what a great learning opportunity lies ahead.

    There are designs for sub-1 Ghz and for the WiFi bandwidth.

    I'm going to try as many as I can.

    Non-scientific, because I don't have the neccessary test gear.

    I'll have to rely on the dB levels reported by the radio firmware.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to Jan Cumps

    That looks like a tiny connector! Smaller than UF.L..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 9 years ago in reply to Jan Cumps

    What frequency range(s) does this antenna support?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to clem57

    It's a kit, Clem, with a range of antennas and frequencies.

    The ones that I'm planning to use are in the Sub-1GHz and WiFi range, 868 MHz -> 2.44 GHz.

    The others I'll keep aside - maybe one day I'll find a purpose...

     

    Here's the list (from the start guide)

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to shabaz

    shabaz wrote:

     

    That looks like a tiny connector! Smaller than UF.L..

    Yes, and very touchy. If properly handled, they have a re-use rate of 30 times. After that, they aren't guaranteed to give a reliable contact.

    These things are so tiny that it's almost impossible to make them strong.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to shabaz

    shabaz wrote:

     

    That looks like a tiny connector! Smaller than UF.L..

    Yes, and very touchy. If properly handled, they have a re-use rate of 30 times. After that, they aren't guaranteed to give a reliable contact.

    These things are so tiny that it's almost impossible to make them strong.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data