RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs SimpleLink™︎ Sub-1 GHz Wireless Microcontroller - Side Note: Recognise your PuTTY Sessions
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: Jan Cumps
  • Date Created: 25 Jun 2016 7:02 PM Date Created
  • Views 1758 views
  • Likes 1 like
  • Comments 5 comments
Related
Recommended
  • putty
  • cc1310
  • simplelink
  • launchpad
  • feature_tutorial
  • ti_rt

SimpleLink™︎ Sub-1 GHz Wireless Microcontroller - Side Note: Recognise your PuTTY Sessions

Jan Cumps
Jan Cumps
25 Jun 2016

I have been blogging on how to make the two seemingly identical LaunchPads distinct, and how to configure Code Composer Studio to recognise them.

 

image

 

 

We still have one weak point: PuTTY.

In its standard setup, both the TX and RX terminal session look very similar. The only visual clue we have is the port number in the title.

 

image

 

Visual Clues to show if PuTTY Connects to TX or RX

 

I've configured my PuTTY sessions in a way that its more obvious. The TX one has a red background, the RX one  is purple.

I've also marked the label on my launchpads with the same colour.

 

image

 

The window title is also adapted. It shows TX and RX.

 

Configuring PuTTY

 

Open your TX puTTY configuration.

image

 

Set the Window Title CC1310 TX

 

image

 

Select a distinct colour. My advice is to use one where you have a matching colour crayon for, so you can also colour the LaunchPad's label image.

 

image

 

Navigate back to Session and Save.

 

Now load the RX configuration. Choose a different colour and make the title 1310 RX

Save the session. All Done.

Never ever will you have to guess what terminal talks to RX or TX.

 

 

SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Check  Received Signal Strength
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Use SmartRF to Try Radio Configs
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Debug 2 LaunchPads at the Same Time
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Side Note: Recognise your PuTTY Sessions
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Side Note: Recognise your Code Composer Studio Sessions
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Debug a Sender to Receiver Conversation
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Side Note: Start a Fresh Project
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Create a Transmitter with SmartRF Studio Part 1
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Create a Transmitter with SmartRF Studio Part 2
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Sensor Controller Engine Part 1: Dry Run
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Sensor Controller Engine Part 2: RTOS Integration
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Sensor Controller Engine Part 3: Wake Up Options
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - Side Note : Measure Power Use of Sensor Controller Engine
SimpleLinkTm Sub-1 GHz Wireless Microcontroller - ToolKit for Range Testing

on TI E2E community: How to connect a CC1310 LaunchPad to the SIGFOX network

  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +1
    Great post Jan. I really like what you are doing with this series. Both with the communication testing between the launch pads, but also experimenting with data transfer rates. Very useful information…
  • clem57
    clem57 over 10 years ago in reply to Jan Cumps +1
    May need to change cloths too to be color coordinated. Just kidding! Great work Jan Cumps
Parents
  • clem57
    clem57 over 10 years ago

    A very overlooked feature that turns useful here. Thanks Jan Cumps

    PS. I noticed the coloring on the labels as well.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to clem57

    I'm going to check if I can colour-code Code Composer Studio as well...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to clem57

    I'm going to check if I can colour-code Code Composer Studio as well...