element14 Community
element14 Community
    Register Log In
  • Site
  • Search
  • Log In Register
  • Community Hub
    Community Hub
    • What's New on element14
    • Feedback and Support
    • Benefits of Membership
    • Personal Blogs
    • Members Area
    • Achievement Levels
  • Learn
    Learn
    • Ask an Expert
    • eBooks
    • element14 presents
    • Learning Center
    • Tech Spotlight
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
    • element14 presents Projects
    • Project14
    • Arduino Projects
    • Raspberry Pi Projects
    • Project Groups
  • Products
    Products
    • Arduino
    • Avnet Boards Community
    • Dev Tools
    • Manufacturers
    • Multicomp Pro
    • Product Groups
    • Raspberry Pi
    • RoadTests & Reviews
  • Store
    Store
    • Visit Your Store
    • Choose another store...
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
  • Settings
RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Blog TI and Würth Elektronik LED RoadTest+ - Circuit Crafting - 8/10
  • Blog
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: tonyboubady
  • Date Created: 10 Jan 2016 2:15 PM Date Created
  • Views 680 views
  • Likes 2 likes
  • Comments 11 comments
Related
Recommended
  • RoadTest
  • ledroadtestplus
  • würth
  • we
  • elektronik
  • texas_instruments
  • ti

TI and Würth Elektronik LED RoadTest+ - Circuit Crafting - 8/10

tonyboubady
tonyboubady
10 Jan 2016

Update: I am working on the soldering WE's SMD LEDs with my tricks and ideas. You know what? it really looks cool and works great...but... I don't think I can do the thermal protection with the board I have etched, it seems super hard and as well the amount of LEDs with thermal holes seems almost snap off point of the board, too close and board is getting weak...My design could work with professional PCB with 3 layers. I am going to finish this project up for demonstration purpose only...will update on next post...

 

Hello, here I am again with some update image

 

I have managed to finish the etching process today, successfully... and I am happy about it. I started with printing my circuit design with laser print and I am not using any glossy paper, it was a quite a story that I can't take laser print with glossy paper here, so I have figured out a way to do it with regular A4 paper and some tricks image

 

This is my successful toner transfer to copper clad board...

 

image

 

I had to do some adjustment with permanent marker pen (Sharpie), yeah! that's how we call it here in India.

 

image

 

Now it's time to etch the board with Ferric Chloride - FeCl3 ... and this is the result.

 

image

 

It's not the perfect one but it does the job...

 

image

 

I am happy about the result... even less than half a millimetre space has been etched, really cool... the next process is soldering the SMD LEDs, WOW!!! but I have some IDEA to do it without using hot air gun, soldier paste with oven etc etc... image. I will post my process in next coming days.

  • Sign in to reply

Top Comments

  • tomaja
    tomaja over 9 years ago in reply to shabaz +3
    Hi shabaz , Do you think he could use solder just to reach the bottom side of the board and then thermal paste to connect to heatsink? (I originally planned to do that, but later I found suitable Aluminium…
  • shabaz
    shabaz over 9 years ago +2
    Hi Antony, I'd hate for you to solder on all those LEDs, and then find out, but have you checked what heatsinking requirements are needed? If these are LEDs with 350mA or higher current consumption, then…
  • shabaz
    shabaz over 9 years ago in reply to tomaja +2
    Hi tomaja Interesting idea, it may be possible, if it is filled with solder from the underside somehow and then flipped over and sanded/polished flat. There is a product which would have been suitable…
Parents
  • shabaz
    shabaz over 9 years ago

    Hi Antony,

     

    I'd hate for you to solder on all those LEDs, and then find out, but have you checked what heatsinking requirements are needed?

    If these are LEDs with 350mA or higher current consumption, then there will be a _lot_ of heat produced, normally needs a large aluminium heatsink for all those LEDs. This type of PCB is not a good conductor for heat, so it will be difficult to mount it in this manner. So, worth thinking about the heat considerations first (I don't have an answer, because it depends on what you have available. You can see dougw implementation, using a MCPCB (metal core PCB). Personally I would try to get those if you can, or something similar,

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tonyboubady
    tonyboubady over 9 years ago in reply to shabaz

    Yeah! you are correct...The thermal pad traces are bigger than the actual size of the LED size, so I can make hole out of it and connect the heatsink on the backside of the PCB, the connection will be solder from hole through the backside which will be again soldered with heatsink... one medium sized heatsink can be used for more than 10 LEDs... hope it will workout.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to tonyboubady

    I see.. Great, was just checking you'd considered the heatsink.

    It will be a big gap (1.6mm is the normal thickness of a PCB) down to the heatsink, so I'm guessing you have a plan for that. Aluminium is very hard to solder (see this solderability page) and super hard when it is a heatsink, because it will be sinking away all the soldering iron heat from where you want the soldering to occur.

    Basically it will be a significant challenge (and the heatsink needs to be large at a guess, due to the very large amount of LEDs if these are going to be operated at 350mA or more.


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 9 years ago in reply to tonyboubady

    I see.. Great, was just checking you'd considered the heatsink.

    It will be a big gap (1.6mm is the normal thickness of a PCB) down to the heatsink, so I'm guessing you have a plan for that. Aluminium is very hard to solder (see this solderability page) and super hard when it is a heatsink, because it will be sinking away all the soldering iron heat from where you want the soldering to occur.

    Basically it will be a significant challenge (and the heatsink needs to be large at a guess, due to the very large amount of LEDs if these are going to be operated at 350mA or more.


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • tonyboubady
    tonyboubady over 9 years ago in reply to shabaz

    I have tried something called oxidation with aluminium to solder...and I have did the solder successfully before. It's not my idea though, I have read some article about it from web and tried that...and yes it's all about how fast I drill the PCB image...of course it's a challenge to handle this much of LED that which is drawing 350mA, well that's all challenge contest is for...Let's see how it goes...:)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tomaja
    tomaja over 9 years ago in reply to shabaz

    Hi shabaz,

    Do you think he could use solder just to reach the bottom side of the board and then thermal paste to connect to heatsink?

    (I originally planned to do that, but later I found suitable Aluminium PCB's on eBay)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to tomaja

    Hi tomaja

    Interesting idea, it may be possible, if it is filled with solder from the underside somehow and then flipped over and sanded/polished flat. There is a product which would have been suitable too, called the PowerPeg, which is like a copper plug that can be soldered and the attached using a screw to a heatsink. But that needs some practise too, so basically Antony may need to experiment.

    Once it is flat, there are also other interesting products, like very thin sheet material (e.g. SIL-PAD) which can take up small imperfections, but it would be pricey on a large area maybe, so perhaps usual heatsink compound is the way to go.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tonyboubady
    tonyboubady over 9 years ago in reply to shabaz

    Cool, that PowerPeg and SIL-PAD things are something new I have learned from you today... but it's all about what I can buy and access to... so I will try my best with what I have...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to tonyboubady

    Hi Antony,

     

    Exactly, you can try to replicate things with what you have access to, such as fill with solder as tomaja suggests instead of using copper pegs, and using heatsink compound instead of SIL-PAD, and you will be ok to run at a lower current even if 350mA is not possible. Just usual physics applies, so try to make as much contact as possible using metal (solder or otherwise) or other thermal conductors between the LED and the heatsink, avoid even the tiniest of air gaps, and keep the heatsink large and screwed to the PCB.

    • Cancel
    • Vote Up +1 Vote Down
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.