RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Microchip AVR-IoT question: How to correctly format a POST request
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 2569 subscribers
  • Views 4589 views
  • Users 0 members are here
  • REST Post
Related

Microchip AVR-IoT question: How to correctly format a POST request

ischonfeld
ischonfeld over 3 years ago

I've been working with the Microchip mini dev board in the Arduino environment [Side note, very nice board so far]. I am converting a program that currently runs using Wifi to this board. It does a POST to a service called Scriptr. The original stripped down code that does the POST is:

  // Working code for Wifi (stripped of error checking and other extraneous stuff)
  const char* ssid     = "myssid";
  const char* password = "mypw";
  String mymsg = "TestMSG";
  const char* bearer    = "xxxxx...xxxxx";  // API Key

  WiFiSSLClient client;

  WiFi.begin(ssid, password);
  client.connect("api.scriptrapps.io", 443)) 

  client.print(String("POST ") + "/SNDSMS/?sms=" + mymsg + " HTTP/1.1\r\n" +  
               "Host: api.scriptrapps.io\r\n" + 
               "Authorization:bearer " + bearer + "\r\n" + // 23 + 68
               "Content-type: application/x-www-form-urlencoded\r\n" +
               "Connection: close\r\n\r\n");
  

The corresponding code for the Microchip mini dev board that I've tried is:

  Lte.begin();
  HttpClient.configure(host, 443, true);   // Have tried true and false for TLS

  HttpResponse response;

  // Following doesn't work
  response = HttpClient.post("/SNDSMS/","?sms=TestMSG HTTP/1.1\r\nHost: api.scriptrapps.io\r\nAuthorization:bearer xxxxx...xxxxx\r\nContent-type: application/x-www-form-urlencoded\r\nConnection: close\r\n\r\n" ); 

  // Following doesn't work either
  response = HttpClient.post("/SNDSMS","/?sms=TestMSG HTTP/1.1\r\nHost: api.scriptrapps.io\r\nAuthorization:bearer xxxxx...xxxxx\r\nContent-type: application/x-www-form-urlencoded\r\nConnection: close\r\n\r\n" ); 

  // Following doesn't work either
  response = HttpClient.post("api.scriptrapps.io","/SNDSMS/?sms=TestMSG HTTP/1.1\r\nHost: api.scriptrapps.io\r\nAuthorization:bearer xxxxx...xxxxx\r\nContent-type: application/x-www-form-urlencoded\r\nConnection: close\r\n\r\n" ); 

I ran https_configure_ca so HTTPS should be enabled. 

I"ve tried numerous guesses at how to format the Post request for the board, all either result in a response of 400 or 0. 

The board is connecting just fine to AT&T and obviously sending the request to Scriptr or I wouldn't be getting 400 errors (at least some of the time). 

Can anyone point me to how I should be formatting the POST request so that it does what the Wifi version does?

Thank you, Ira. 

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago +2
    It appears the HttpClient library they provide is too simple to allow for this - you are configuring the headers on a POST request and not the post body. The code itself is pretty clear - if you examine…
  • Gough Lui
    Gough Lui over 3 years ago +2 suggested
    I have modified the version of the library to allow for the extra parameters and it seems to work. First of all, the sample test code: #include <Arduino.h> #include <http_client.h> #include <led_ctrl…
  • Gough Lui
    Gough Lui over 3 years ago +1
    Further to my previous comment - Actually, I may have spoken too soon - it is early morning where I am, but it seems that AT+SQNFPUT for POST or PUT does support an extra header line, see Page 70, as…
Parents
  • shabaz
    0 shabaz over 3 years ago

    Hi,

    There are two tools that are very useful for such work, they are Postman, and Wireshark. Using those, you can test out the message using your PC (i.e. no microchip), so that you know the exact format you need. Then you can use a print statement in your microcontroller code, and compare with what you got with Postman. Use Wireshark if you need to go deeper into the message or message exchange, but probably Postman may be sufficient. There's no point trying this on the microcontroller until you're entirely happy with the response using the PC, otherwise you'll be repeatedly compiling and testing things, and the code-test cycle is slower in that way. Postman will format things correctly (depends on its usage).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ischonfeld
    0 ischonfeld over 3 years ago in reply to shabaz

    Hi, I know the format I need - it's already working on various other boards via Wifi. What I need to know is how to format the httpclient.post function call for this particular microcontroller library to get my request string sent correctly. Thanks. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to ischonfeld

    I see. In that case, it could be worthwhile setting up a local server just to capture POSTs and display them. In other words, send your POST from your Microchip board, to your server instead of the proper scriptr server. 

    A quick way would be to find an example Python or Node.js server, that will just dump output to the screen or log file, i.e. no need to install a more full-blown server. Then you can inspect the dump/log to see what got sent, and then you know what needs to change in your code to correct it.

    EDIT: I guess it needs to be an Internet facing server (you're testing a mobile wireless board?) then you could do it using AWS or whatever, i.e. spin up an EC2 server and put your simple server there, and close it down afterwards, i.e. there's no security issue then.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 3 years ago in reply to ischonfeld

    I see. In that case, it could be worthwhile setting up a local server just to capture POSTs and display them. In other words, send your POST from your Microchip board, to your server instead of the proper scriptr server. 

    A quick way would be to find an example Python or Node.js server, that will just dump output to the screen or log file, i.e. no need to install a more full-blown server. Then you can inspect the dump/log to see what got sent, and then you know what needs to change in your code to correct it.

    EDIT: I guess it needs to be an Internet facing server (you're testing a mobile wireless board?) then you could do it using AWS or whatever, i.e. spin up an EC2 server and put your simple server there, and close it down afterwards, i.e. there's no security issue then.
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.