RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Microchip AVR-IoT question: How to correctly format a POST request
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 2570 subscribers
  • Views 4595 views
  • Users 0 members are here
  • REST Post
Related

Microchip AVR-IoT question: How to correctly format a POST request

ischonfeld
ischonfeld over 3 years ago

I've been working with the Microchip mini dev board in the Arduino environment [Side note, very nice board so far]. I am converting a program that currently runs using Wifi to this board. It does a POST to a service called Scriptr. The original stripped down code that does the POST is:

  // Working code for Wifi (stripped of error checking and other extraneous stuff)
  const char* ssid     = "myssid";
  const char* password = "mypw";
  String mymsg = "TestMSG";
  const char* bearer    = "xxxxx...xxxxx";  // API Key

  WiFiSSLClient client;

  WiFi.begin(ssid, password);
  client.connect("api.scriptrapps.io", 443)) 

  client.print(String("POST ") + "/SNDSMS/?sms=" + mymsg + " HTTP/1.1\r\n" +  
               "Host: api.scriptrapps.io\r\n" + 
               "Authorization:bearer " + bearer + "\r\n" + // 23 + 68
               "Content-type: application/x-www-form-urlencoded\r\n" +
               "Connection: close\r\n\r\n");
  

The corresponding code for the Microchip mini dev board that I've tried is:

  Lte.begin();
  HttpClient.configure(host, 443, true);   // Have tried true and false for TLS

  HttpResponse response;

  // Following doesn't work
  response = HttpClient.post("/SNDSMS/","?sms=TestMSG HTTP/1.1\r\nHost: api.scriptrapps.io\r\nAuthorization:bearer xxxxx...xxxxx\r\nContent-type: application/x-www-form-urlencoded\r\nConnection: close\r\n\r\n" ); 

  // Following doesn't work either
  response = HttpClient.post("/SNDSMS","/?sms=TestMSG HTTP/1.1\r\nHost: api.scriptrapps.io\r\nAuthorization:bearer xxxxx...xxxxx\r\nContent-type: application/x-www-form-urlencoded\r\nConnection: close\r\n\r\n" ); 

  // Following doesn't work either
  response = HttpClient.post("api.scriptrapps.io","/SNDSMS/?sms=TestMSG HTTP/1.1\r\nHost: api.scriptrapps.io\r\nAuthorization:bearer xxxxx...xxxxx\r\nContent-type: application/x-www-form-urlencoded\r\nConnection: close\r\n\r\n" ); 

I ran https_configure_ca so HTTPS should be enabled. 

I"ve tried numerous guesses at how to format the Post request for the board, all either result in a response of 400 or 0. 

The board is connecting just fine to AT&T and obviously sending the request to Scriptr or I wouldn't be getting 400 errors (at least some of the time). 

Can anyone point me to how I should be formatting the POST request so that it does what the Wifi version does?

Thank you, Ira. 

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago +2
    It appears the HttpClient library they provide is too simple to allow for this - you are configuring the headers on a POST request and not the post body. The code itself is pretty clear - if you examine…
  • Gough Lui
    Gough Lui over 3 years ago +2 suggested
    I have modified the version of the library to allow for the extra parameters and it seems to work. First of all, the sample test code: #include <Arduino.h> #include <http_client.h> #include <led_ctrl…
  • Gough Lui
    Gough Lui over 3 years ago +1
    Further to my previous comment - Actually, I may have spoken too soon - it is early morning where I am, but it seems that AT+SQNFPUT for POST or PUT does support an extra header line, see Page 70, as…
Parents
  • Gough Lui
    0 Gough Lui over 3 years ago

    Further to my previous comment -

    Actually, I may have spoken too soon - it is early morning where I am, but it seems that AT+SQNFPUT for POST or PUT does support an extra header line, see Page 70, as does AT+SQNHTTPSND, see Page 80.

    You will need to edit the library to add an extra few arguments to the function by changing the function prototype in http_client.h and then modifying the #define and functions in http_client.c, specifically Http:ClientClass::post.

    The first is post_param, of which 0 gives you 'application/x-www-form-urlencoded already, which is what you need. The next is extra_header_line (up to 1500 bytes) which I would suggest you put "Authorization:bearer xxxx" only. The HTTP version, hostname and connection disposition should be handled by the HTTP/S stack within the modem itself and should not be included.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ischonfeld
    0 ischonfeld over 3 years ago in reply to Gough Lui

    I'm not sure where your original comment wound up, but these modifications may be beyond my capability. I can certainly drop the extra header items you mention. As far as changing the function prototype, that's not something I understand how to do. 

    Also, which document are you referencing for "page 70". 

    Is the upshot of what you're saying that I can't send header information (authorization in particular) with the existing library? 

    Thanks. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 3 years ago in reply to ischonfeld

    The AT command reference is referred to in my previous reply - you will find it in the thread but also copied here - https://iot.microchip.com/docs/assets/files/ATCommandsLR8.0-NoCopyright-f9315d856c8b84593a1cf8391b904c36.pdf

    The modem is capable, the library not at this time as it is rather rudimentary and seemingly only exposes the most common options (i.e. post destination and payload only).

    I might be able to do some modifications and send you something directly, but I am not using whatever service you are, so I don't have a convenient way to know if the modifications would work or not.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 3 years ago in reply to ischonfeld

    The AT command reference is referred to in my previous reply - you will find it in the thread but also copied here - https://iot.microchip.com/docs/assets/files/ATCommandsLR8.0-NoCopyright-f9315d856c8b84593a1cf8391b904c36.pdf

    The modem is capable, the library not at this time as it is rather rudimentary and seemingly only exposes the most common options (i.e. post destination and payload only).

    I might be able to do some modifications and send you something directly, but I am not using whatever service you are, so I don't have a convenient way to know if the modifications would work or not.

    - Gough
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.