RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Do You Have a Need for High Speed Multi-Function Recorder?
  • Blogs
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 2720 subscribers
  • Views 5047 views
  • Users 0 members are here
  • roadtest survey
  • bk precision
  • DAS60
Related

Do You Have a Need for High Speed Multi-Function Recorder?

rscasny
rscasny over 2 years ago

imageI have been speaking with a manufacturer who has a High Speed Multi-Function Recorder that it would like to roadtest. We are looking to see if there are some people on the community who have an immediate need of a recorder such as its DAS60 model .

Here's a description of the product:

It's a high-speed multi-function recorder with versatile channel configurability, high-speed sampling (1 MSa/s), a wide input range (±5 mV to ±500 V), large internal solid-state memory of up to 64 GB, and 9.5 hours of battery life. Each channel can record a different signal such as voltage, temperature, current or frequency simultaneously, using a common time base.

Here are some features:

  • Fast 1 MSa/s sample rate (memory mode) and 100 kHz bandwidth for capturing intermittent events
  • Accurately view and record signals from ±5 mV to ±500 and 424 VRMS
  • CAT III 600 V rated isolated channels
  • Wide 10-inch touchscreen TFT display
  • Capture mixed signals with one instrument, such as high voltage, current waveforms, temperature, and logic data
  • Battery life up to 9.5 hours
  • 64 GB (DAS60) and 32 GB (DAS30/50) internal solid-state memory
  • 6 analog input channels
  • 14-bit resolution
  • 16 logic input channels
  • Temperature measurements supporting thermocouples and Pt100/Pt1000 sensors (factory option on DAS30/50)
  • WiFi monitoring and control (standard USB WiFi dongle required)
  • 2 USB host ports and one LAN interface
  • 110 mm thermal printer (factory option)

Here are some of the common uses:

  • Measure signals ranging from small sensors to large electrical systems
  • Maintenance and failure analysis
  • Power analysis of single and three-phase systems

Here is some documentation:

Datasheet 

Prog. Manual 

User Manual 

Roadtester Polls



  • Sign in to reply
  • Cancel
  • dang74
    dang74 over 2 years ago in reply to robogary

    True.  I should have alluded to this caveat.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 2 years ago in reply to hlipka

    Perhaps it was a poor choice of words on my part.  I wasn't referring the need to buy one.  At this point, I was thinking along the lines of do you have something where you could use a 6 channel recorder? I was just trying to gauge how many members really had an application or situation where they could use this recorder to its fullest extent. This would influence how many units I would recommend to the sponsor for the roadtest.

    Randall

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 2 years ago

    I don't have a need for a multi-function recorder, but it looks interesting and I will certainly be reading any road test to find out more about it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 2 years ago

    Nice looking instrument.

    I wish I had a need, but I just do not.

    Does have some interesting capabilities.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelwylie
    michaelwylie over 2 years ago in reply to robogary

    ahhh, ty for the clarification.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 2 years ago in reply to michaelwylie

    Service unit is one that had an early life failure and was repaired, at deep discount  , not MSRP. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelwylie
    michaelwylie over 2 years ago in reply to robogary

    So, RoadTest the unit, write a detailed review, and don't get to keep the unit? Rolling eyes

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 2 years ago in reply to michaelwylie

    Maybe Sefram can send a service unit :-) 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelwylie
    michaelwylie over 2 years ago

    Yes, in fact, I do have a need for a recorder like this. We record very high sample rates on acoustic emission sensors and I have been actively seeking a recorder. However, I likely won't apply for the RoadTest because of the tax liability.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to Jan Cumps

    The precision of the cheap plastic ruler probably wasn't that great either. Slight smile

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>