OpenScope MZ Development Kit

Table of contents

image

 

 

 

{tabbedtable} Tab LabelTab Content
About

The OpenScope MZ is an open source, multi-function, electronic instrumentation device that can be controlled using a computer or mobile device to acquire, analyze, visualize, and generate signals from circuits, sensors, and other electronic devices. OpenScope MZ makes it easy to generate analog and digital signals using the power supply, function generator and GPIO and measure and visualize analog and digital signals using the oscilloscope and logic analyzer. Develop and debug circuits faster by generating stimuli and visualizing the response using OpenScope MZ.

image

Features

  • Two scope channels with 12 bits at 2MHz bandwidth and 6.25 MS/s max sampling rate
  • One function generator output with 1MHz bandwidth at 10MS/s update rate
  • Ten user programmable pins configurable as GPIO or 10-channel logic analyzer
  • User programmable power supplies supplying up to 50mA and ±4V of power
  • Can powered through USB bus or external PSU
  • On-board WiFi
  • Can be used with the browser based WaveFroms Live software
  • Reprogrammable through Arduino or Microchip MPLAB IDE

 

Additional Information

OpenScope MZ Reference Manual

Important Dates

Enrollment Begins: Oct 11 2017

Enrollment Ends: Nov 14 2017

RoadTesters Selected: Dec 8 2017

Product Shipped: Dec 12 2017

RoadTesting Begins: Dec 19 2019

Reminder/Update Email: Jan 19 2018*

Submit Reviews By: Feb 12 2018*

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

The following applicants were selected as official RoadTesters:

 

Terms and Conditions

OpenScope MZ Dev Kit– RoadTest

Terms and Conditions

These are the terms and conditions which govern the OpenScope MZ Dev Kit RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

Analog System Lab Kit

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Nov 14 2017

Announcement of Winner (estimated): Nov 21 2017

 

Prize: OpenScope MZ Dev Kit
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
  • Noob question: Is this basically a budget friendly compact oscilloscope? Just a compact version that is interfaced with PC.

    How well would this compare to standard low-end scopes found in student labs? Good enough for average electronics projects?

    Is there a standard way to connect signals to GPIO? I assume a solderless breadboard is a bad method if I'm worried about noise?

     

    Thanks!

    Jordan

  • With the relatively limited bandwidth etc, I would say that it will be ok with anything coming out of a PI / Arduino / or other microcontroller system, it won't even get close to low frequency RF like sub GHz radios, For audio and ultrasonic type frequencies it will be great, it should also be able to resolve small signals on larger ones too as this has a 12bit A-D convertor

     

    be aware though, it has only a 1MOhm input impedance so could load some circuits to the point of failure, but as with all scopes, thats what a 10X probe if for, it would not take much to fabricate a 9MOhm resistor etc to make your own if needed.

  • It has a scope and waveform generator and power supply. Also theres a Bode plot and FFT tool.

     

    If you need to use traditional probes for attenuation the BNC Adapter that's designed for the Analog Discovery works with the OpenScope: https://blog.digilentinc.com/can-the-analog-discovery-adapters-work-with-openscope-mz/

     

    Also if the specifications on the OpenScope MZ aren't enough for your needs the Analog Discovery(https://analogdiscovery.com/ ) provides higher bandwidth, but at a higher price point.

Comment Children