TI Robotic Systems Learning Kit (TI-RSLK)

Table of contents

Sign Up for the Companion Webinar: Learn, Build, and Compete with TI Robotics System Learning Kit (Basic and Advanced)

 

 

{tabbedtable} Tab LabelTab Content
About

TI-RSLK is a low-cost robotics kit and classroom curriculum, which provide students with a deeper understanding of how electronic system designs work. Designed to supplement university faculty curriculum, the TI-RSLK Maze Edition comes with 20 learning modules covering basic to advanced topics.

 

Each module is complete with lecture videos and slides, lab documentation and demonstration videos, quizzes and classroom activities and resources from TI to support the learning experience. The kit and curriculum is fully customizable, allowing faculty to choose how they integrate the TI-RSLK into their class. The TI-RSLK is targeted to teach embedded systems and applications, and can be expanded and used in a variety of engineering classes at any level along a college student’s learning journey.

 

Basic Kit

Buy NowBuy Now

image

Advanced Kit

Buy NowBuy Now

image

Additional Information

TI-RSLK

Important Dates

Enrollment Begins: May 1 2018

Enrollment Ends: June 1 2018

RoadTesters Selected: June 20 2018 (estimated)

Product Shipped: June 21 2018

RoadTesting Begins: June 28 2018

Reminder/Update Email: July 28 2018

Submit Reviews By: August 29 2018**

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

The following applicants have been selected as official roadtesters:

 

 

Terms and Conditions

TI Robotic Systems Learning Kit (TI-RSLK) RoadTest

Terms and Conditions

These are the terms and conditions which govern the TI Robotic Systems Learning Kit (TI-RSLK) RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

TI Robotic Systems Learning Kit (TI-RSLK)

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on May 1 2018

Announcement of Winner (estimated): Jun 1 2018

 

PrizeTI Robotic Systems Learning Kit (TI-RSLK)
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
  • Hello @ Randall Scasny
    Seems somehow while i was out this morning my application went in for this project but the body of my prioject did not i have updated the body and it would not accept it after., not sure what happened there.
    Hoping you will have a look at the saved draft.
    Sincerely Christopher Montgomery.

Comment
  • Hello @ Randall Scasny
    Seems somehow while i was out this morning my application went in for this project but the body of my prioject did not i have updated the body and it would not accept it after., not sure what happened there.
    Hoping you will have a look at the saved draft.
    Sincerely Christopher Montgomery.

Children
  • Hello good people of Element 14 and @ Randall Scasny

    I have a project idea for a little assistant that would operate off wearable electronics clothing for children with slight disabilities as a protective assistant of sorts.

    Myself having a daughter that has cerebral palsy and she liked to have the ability to get away from the parents now and then,

    but she had occasionally flipped her wheelchair and not knowing that something happened right away until one of the other kids in the neighborhood

     

    came to ask for help or tell us she had tipped her chair again there was a few times she was in a uncomfortable position for 10-15 minutes.

     

    So i have thought this could be a good little starter project with enough features to give it a go and field test it.

    That is just one of the parts to the needs some children with the disability have also communication and sign language is the other thought is if it could speak for her,

    Times when she cant get words out for a variety of reasons and if she was wearing gloves that transmit her hand gestures to the bot,

    and it would speak for her to the other children she is playing with and or people when she is in an emotional state or nervous and cant speak but she can always seem to sign.

    I have other ideas to put all together with it, but that is the jest of the project that I have in mind.

     

    Thank you for this opportunity to do something for children who need just a little bit of help at times and have their independence still and can get away from over bearing parents, haha.

    Sincerely Christopher Montgomery,

  • Christopher,

     

    Whilst this sounds like a good idea for a project, this robotics kit is probably not the platform for it. The first thing I think of would be TI's CC1350 sensor tag. It is small, battery powered and has an accelerometer built in. It also a sub 1GHz radio which should allow it to communicate with another similar device over a range of at least a few hundred metres.

    CC1350STK Simplelink CC1350 SensorTag Bluetooth and Sub-1GHz Long Range Wireless Development Kit | TI.com

  • This was to be a follow-along part of the puzzle I have an Uno R3 and other sensors etc as pieces to tie all the project together, The bot was to be one part of the full project.
    Thanks for your input.
    Christopher Montgomery

  • Very interesting idea! Sounds like a good challenge for the design challenge "Design for å Cause". I sure would love to give it a go, but i do not know if i have the abilities or resources. No doubt in my mind that there are LOTS of people here who have both, though image!

  • Actually, I like the idea.  The bot could be a companion to someone like your daughter and be used to indicate events such as when the wheel chair is no longer righted and seek help.  Now, on the wheel chair or the person in it you could have a wearable such as the CC1350 communicates to the bot via Bluetooth or Sub 1GHz which then can either go look for help or forward the condition to a cloud resource where a SMS message could be sent out. Adding a tilt sensor on the wheel chair would be one way to know if the chair is righted or not.

     

    However, going a step further, using the same IR and bump sensor concept as the TI-RSLK bot and placing these on the wheel chair I could see where this could help the person in such a chair navigate around an area with obstacles.  A light or sound sensor could be used to indicate when an obstacle is encountered.  If the chair is motorized then with some electrical skill, the obstacle sensors could be used to provide some autonomy to the chair.

     

    As Raymond mentioned, your project would be a good fit for the Design for a Cause challenge, and given that the kit for that challenge has a MKR1000 in it, you could use something like MQTT to communicate between the chair and the bot and set up different topics for a variety of events from the chair including if it has turned over.

     

    I see many possibilities. 

  • Christopher,

    I believe that a BBC Micro:Bit could be a much better platform than the Arduino to design this specific solution on. It has many built in sensors that could be used by your application:

    It also has more built in memory and Bluetooth. I believe that it costs about the same as an Arduino, and it also has a free online programming environment for developing and installing applications on it. If i find time to do so, i will look into writing an application for you on it that you can use to solve your stated requirements.

     

    - raymond

  • I was looking at the micro:bit but didn't think it had quite enough features for the whole projects ideas and versatility expansion options have envisioned.  I had figured i would need a few boards working together to cover all bases.
    Christopher

  • Spare funds vs time to apply just don't look like it's going to fit together right now. But there is always other days other challenges.
    Th bot side is the price ding in my budget.
    Christopher