Sensirion Environmental Sensor Shield - Industrial Sensing

Table of contents

image

 

 

{tabbedtable} Tab Label Tab Content
About

The Sensirion Environmental Sensor Shield (ESS) is a sensor shield that features our SHTC1 humidity and temperature sensor along with a SGP30 total VOC and CO2eq sensor. It has been designed to be used with any reference design that supports I2C, and follows the Arduino footprint, which has been adapted by a lot of reference designs and development kits.

image

Connecting the ESS

For boards using the Arduino footprint, the board can simply be plugged in by aligning the pin headers and pushing down. For boards that don’t follow the Arduino footprint, there’s two possibilities: the first it to use an adapter board (those are available for example for Raspberry Pi, or 96boards), or simply to use four cables and connect the four pins on the back of the ESS to the corresponding ports on the reference design. The pins are labelled on the back of the ESS, and represent the I2C signal, i.e. VCC, SCL, SDA and GND. The ESS can work with both 3.3V and 5V designs.

 

Additional Information

GitHub

Tutorial

Important Dates

Enrollment Begin: May 25 1018

Enrollment Ends: Jun 30 2018

RoadTesters Selected: July 3 2018 (estimated)

Product Shipped: July 5 2018

RoadTesting Begins: July 12 2018

Reminder/Update Email: August 12 2018*

Submit Reviews By: Sept 12 2018*

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

The following applicants have been selected as official roadtesters:

 

Terms & Conditions

RoadTest

Terms and Conditions

These are the terms and conditions which govern the Sensirion Environmental Sensor Shield RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

Sensirion Environmental Sensor Shield

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on June 30 2018

Announcement of Winner (estimated): July 6 2018

 

Prize: Sensirion Environmental Sensor Shield
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
How To Locate the Official Review Form Click Here for Directions
Comment List
Anonymous
Parents
  • Interesting product.  I was interested in seeing a schematic, to better understand the interconnect of the sensors (using this with something other than the Arduino).  Has anyone run across a schematic or documentation for this board?

    Thanks,

    Gene

  • Hi Gene,

     

    I was interested in that too.  They refer to a "reference design" here and as quoted below but I couldn't find it.  It appears to be just I2C with level shifting for 3V3 or 5V and some LEDs though.

     

    From link above:  "For boards that don’t follow the Arduino footprint, there’s two possibilities: the first it to use an adapter board (those are available for example for Raspberry Pi, or 96boards), or simply to use four cables and connect the four pins on the back of the ESS to the corresponding ports on the reference design. The pins are labelled on the back of the ESS, and represent the I2C signal, i.e. VCC, SCL, SDA and GND. The ESS can work with both 3.3V and 5V designs."

     

    The LEDs are on pins 9, 10, 11 of the Arduino pinout per the code in github

     

    I2C addresses are in the code and they apparently have support for the Raspberry Pi.

     

    Datasheets are here and here.

     

Comment
  • Hi Gene,

     

    I was interested in that too.  They refer to a "reference design" here and as quoted below but I couldn't find it.  It appears to be just I2C with level shifting for 3V3 or 5V and some LEDs though.

     

    From link above:  "For boards that don’t follow the Arduino footprint, there’s two possibilities: the first it to use an adapter board (those are available for example for Raspberry Pi, or 96boards), or simply to use four cables and connect the four pins on the back of the ESS to the corresponding ports on the reference design. The pins are labelled on the back of the ESS, and represent the I2C signal, i.e. VCC, SCL, SDA and GND. The ESS can work with both 3.3V and 5V designs."

     

    The LEDs are on pins 9, 10, 11 of the Arduino pinout per the code in github

     

    I2C addresses are in the code and they apparently have support for the Raspberry Pi.

     

    Datasheets are here and here.

     

Children
No Data