Cool Tools: Weatherproof Equipment Case

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

$35.70 USD ONLY!  Durable equipment case provides maximum shock protection for contents making it useful for instruments, audio/video equipment, tactical gear, photographic equipment and test equipment. Cubed foam insert for custom use. Internal size - 17" x 11" x 6.5"

image

  • Built-in O-ring with secure latches prevent water and moisture damage to contents
  • Padlock compatible for additional security
  • Built in pressure relief valve
  • High-density polymer provides outstanding strength and corrosion resistance
RoadTester

Terms and Conditions

Weatherproof Equipment Case RoadTest

Terms and Conditions

These are the terms and conditions which govern the Weatherproof Equipment Case RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

Weatherproof Equipment Case

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on June 6 2018

Announcement of Winner (estimated): June 11 2018

Due date: Aug11 2018

 

Prize: Weatherproof Equipment Case
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
  • Interesting roadtest, not sure how I would test this, but I'm sure there are ways, just need to think about it.

     

    Kas

  • You'd also need to include a pressure difference test. ....

     

    I'd suggest that the case be heated and then left outside in cold damp environment to see if moisture gets sucked in.

     

    We had major issues with antennas that were very well sealed, after service in the field with the heat/cool cycling, they sucked in moisture.

    In the end we added a drain so they were ventilated to overcome it.

     

     

     

    The other issue I see is cold damp foam is not going to behave well when you heat it up.

    It's likely to give up the moisture and spread it into the equipment you have fitted in it.

     

    Be an interesting set of tests.

    Mark

Comment
  • You'd also need to include a pressure difference test. ....

     

    I'd suggest that the case be heated and then left outside in cold damp environment to see if moisture gets sucked in.

     

    We had major issues with antennas that were very well sealed, after service in the field with the heat/cool cycling, they sucked in moisture.

    In the end we added a drain so they were ventilated to overcome it.

     

     

     

    The other issue I see is cold damp foam is not going to behave well when you heat it up.

    It's likely to give up the moisture and spread it into the equipment you have fitted in it.

     

    Be an interesting set of tests.

    Mark

Children
  • It's annoying how moisture laden air gets sucked into the minutest of gaps as the air inside cools but the moisture never gets expelled again. You are right that an engineered drain is the way rather than go hermetically sealed. Alternatively if you have the equipment and budget, a source of positive pressure dried air into enclosures/antennas is good.

     

    Re: for the Duratool equipment case - a bag of silica gel could be dried, weighed and placed inside for a good few days of thermal cycling outside. Weighing the silica gel bag afterwards would reveal how good the seal was; the bag could be weighed using something like this perhaps Product LinkProduct Link

     

    Rod

  • a bag of silica gel could be dried, weighed and placed inside for a good few days of thermal cycling outside

    That's a good method, that could work.

     

     

    We used positive pressure in our waveguides.

    When I was at Telecom, they had a controlled leak at the top so that any moisture was blown out, since it was the highest point.

    Where I am now, our Satellite dishes have a waveguide and a positive air system, but they don't have a controlled leak, and surprise, surprise they have corrosion at the top.

     

    I tried leading that horse to water, but failing the "brick and the camel joke" I wasn't able to convince them about controlled leaks.

     

    Cheers

    Mark