LPCXpresso 51U68 Dev Board

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The LPCXpresso51U68 board has been developed by NXP to enable evaluation of and prototyping with the LPC51U68 MCUs, and is based on the LPC51U68JBD64 version of the MCU.

image

About LPC51U68 MCUs

Based on the highly energy-efficient Arm® Cortex®-M0+ core and operating at CPU frequencies of up to 100 MHz, NXP’s 32-bit LPC51U68 microcontrollers for embedded applications feature larger memory resources including 96 KB of on-chip SRAM and 256 KB of on-chip flash programming memory with flash accelerator.

 

NXP’s LPC51U68 MCU features added performance, expanded memory resources and flexible serial port configuration, including USB connectivity, bringing unparalleled design flexibility, computing performance and integration into today’s demanding IoT and industrial applications. In addition, this MCU is pin compatible with the LPC5411x and LPC5410x MCU families providing scalability options to Arm Cortex-M4 cores.

 

Features

  • On-board, high-speed USB based, Link2 debug probe with ARM’s CMSIS-DAP and SEGGER J-Link protocol options.
  • Link2 probe can be used with on-board LPC51U68 or external target.
  • Support for external debug probes.
  • Tri-color LED.
  • Target Reset, ISP, and WAKE buttons.
  • Expansion options based on Arduino UNO and PMod™, plus additional expansion port pins.
  • On-board 1.8/3.3V or external power supply options.
  • Built-in power consumption measurement.
  • UART, I2C and SPI port bridging from LPC51U68 target to USB via the on-board debug probe.
  • FTDI UART connector

 

How To Apply

 

You must answer the following questions in your application:

  • Tell us about yourself.  The element14 Community consists of over 500,000 members. So, we may not know you personally. That’s why it is a good idea to introduce yourself. We don’t need your life story (unless it’s relevant) but do tell us about your previous or current job, credentials, and your previous experience using products like the one you want to test.

 

  • Why are you applying? Winners don’t get any additional compensation over the cost of the product – so, why are you applying?  What’s your motivation? If you are excited about this product, tell us why. Being honest, authentic and personal helps us determine who is committed enough to complete the RoadTest and have some fun in the process.

 

  • How will you RoadTest the product? Now we are getting into the details of your review of the product. Give us a description of your testing procedure. This helps us understand your knowledge of product as well as its applications. If you don’t have an exact procedure written down, then provide us with an outline of the steps you will take. Be detailed. Using graphics, block diagrams, images, even a video can really help you stand out from the other applicants.

 

  • Describe your participation in the element14 community: Since RoadTests are an element14 "participation" program, we look for applicants who are participating in the community. So, list a few ways you have participated in the community, such as blogs written, discussions started, comments made, or any involvements in other community programs.

 

  • Can you commit to completing the testing and review writing in 60 days ?  We want to select RoadTest applicants who not only have the skills to conduct a thorough review of the product, but also have the commitment and time to complete it. So, give us an idea of your schedule and indicate whether you can complete the RoadTest within 60 days from receipt of the product.
Important Dates

Enrollment Begin: Aug 1 2018

Enrollment Ends: Sept 3 2018

RoadTesters Selected: Sept 24 2018

Product Shipped: Sept 25 2018

RoadTesting Begins: Oct 2 2018

Reminder/Update Email: Nov 2 2018*

Submit Reviews By: Dec 2 2018*

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

Roadtesters

The following applicants have been selected:

 

Terms and Conditions

LPCXpresso 51U68 Dev Board

RoadTest

Terms and Conditions

These are the terms and conditions which govern the LPCXpresso 51U68 Dev Board RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

LPCXpresso 51U68 Dev Board

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Sept 3 2018

Announcement of Winner (estimated): Sept 10 2018

Prize:LPCXpresso 51U68 Dev Board

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

How to Write a Winning ApplicationClick here to view the short webinar
Comment List
Anonymous
  • Like David, I’ve just logged on to post an application to find it closed.

     

    Sad to hear you didn’t get enough good applicants Randall, but probably better to go with quality rather than quantity. Hopefully you’ll find a use for them on an upcoming project - I was going to partner it with an LCD shield and make some test instrumentation, not sure the timescales would fit your next design challenge though.

     

    A lesson for us all to get our applications in sooner I guess,

     

    Good luck Randall

  • No. But I had to go with what I had. The big issue was that the supplier wanted to get me 5 more boards and I didn't have enough detailed applications for that. So, I have proposed to use the 5 extra boards for projects. So, keep posted.

     

    Randall

  • I was just about to put in an application, but I see it's closed. I hope that means you've now got enough good quality entries.

  • Thanks for pointing this out. I thought it was live.

     

    But this is the copy within the document:

     

    If you are interested in applying to this roadtest, I re-opened the enrollment for a few days.  This is what I need in an application:

     

    • Tell us about yourself.  The element14 Community consists of over 500,000 members. So, we may not know you personally. That’s why it is a good idea to introduce yourself. We don’t need your life story (unless it’s relevant) but do tell us about your previous or current job, credentials, and your previous experience using products like the one you want to test.

     

    • Why are you applying? Winners don’t get any additional compensation over the cost of the product – so, why are you applying?  What’s your motivation? If you are excited about this product, tell us why. Being honest, authentic and personal helps us determine who is committed enough to complete the RoadTest and have some fun in the process.

     

    • How will you RoadTest the product? Now we are getting into the details of your review of the product. Give us a description of your testing procedure. This helps us understand your knowledge of product as well as its applications. If you don’t have an exact procedure written down, then provide us with an outline of the steps you will take. Be detailed. Using graphics, block diagrams, images, even a video can really help you stand out from the other applicants.

     

    • Describe your participation in the element14 community: Since RoadTests are an element14 "participation" program, we look for applicants who are participating in the community. So, list a few ways you have participated in the community, such as blogs written, discussions started, comments made, or any involvements in other community programs.

     

    • Can you commit to completing the testing and review writing in 60 days ?  We want to select RoadTest applicants who not only have the skills to conduct a thorough review of the product, but also have the commitment and time to complete it. So, give us an idea of your schedule and indicate whether you can complete the RoadTest within 60 days from receipt of the product.
  • That's unfortunate to hear that it keeps happening - but a heads up , it seems like the User Guide is not accessible:

    image

  • To All,

     

    I looked at the applications---90% of them are single sentence applications.

     

    If you are interested in applying to this roadtest, I re-opened the enrollment for a few days.  This is what I need in an application:

     

    • Tell us about yourself.  The element14 Community consists of over 500,000 members. So, we may not know you personally. That’s why it is a good idea to introduce yourself. We don’t need your life story (unless it’s relevant) but do tell us about your previous or current job, credentials, and your previous experience using products like the one you want to test.

     

    • Why are you applying? Winners don’t get any additional compensation over the cost of the product – so, why are you applying?  What’s your motivation? If you are excited about this product, tell us why. Being honest, authentic and personal helps us determine who is committed enough to complete the RoadTest and have some fun in the process.

     

    • How will you RoadTest the product? Now we are getting into the details of your review of the product. Give us a description of your testing procedure. This helps us understand your knowledge of product as well as its applications. If you don’t have an exact procedure written down, then provide us with an outline of the steps you will take. Be detailed. Using graphics, block diagrams, images, even a video can really help you stand out from the other applicants.

     

    • Describe your participation in the element14 community: Since RoadTests are an element14 "participation" program, we look for applicants who are participating in the community. So, list a few ways you have participated in the community, such as blogs written, discussions started, comments made, or any involvements in other community programs.

     

    • Can you commit to completing the testing and review writing in 60 days ?  We want to select RoadTest applicants who not only have the skills to conduct a thorough review of the product, but also have the commitment and time to complete it. So, give us an idea of your schedule and indicate whether you can complete the RoadTest within 60 days from receipt of the product.

     

     

    Single Sentence Applications Will Never Win

     

    Randall Scasny

    RoadTest Program Manager

  • To all applicants.

     

    I peeked at the applications for this roadtest. Half are single-sentence applications. Most of you know how I feel about 1-liners. If don't, imagine yourself in a job interview and you answered the following question in a single sentence: Why are you the best candidate for this job? If you are competing against 10, 20 or 30 other people, a single sentence will not win you the job. Same goes for roadtests.

     

    I would suggest that if you wrote a very brief application to re-visit it. Here are three questions to answer in your application:

     

    1. What is your knowledge and/or background for this roadtest?

    2. How are you going to test this product?

    3. What is your typical schedule and do you have the availability to completing the testing and review writing on element14 within 60 days of receipt of the product?

     

    Randall Scasny

    RoadTest Program Manager

  • I used the baby brother of this board LPC11U37H LPCXPRESSO BOARD with Cortex M0

    The ULINKPLUS-Universal Debug Trace Adapter road-test can be read here although my focus was on KEIL and the debugger and not really on the board itself.

     

    ARM’s CMSIS-DAP is an interesting feature to check out.

     

    Cheers image

  • This chip has a nice boost in features and performance over a typical Cortex M0 MCU.