Microchip AVR-IoT WG Dev Board

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The AVR-IOT WG board implements a wireless (WiFi) IoT sensor node using a small and inexpensive AVR microcontroller of the latest generation.

 

  • The ATmega4808 provides an easy migration path for existing AVR microcontroller applications by providing 48KB of Flash and 6K of RAM with a rich complement of analog and digital peripherals including Core Independent (Event System) functionality.
  • The ATECC608A Secure Elements provides secure key generation/storage and offloads all cryptography tasks enabling the highest level of security available to modern IoT applications. The secure element is pre-provisioned for immediate (out of the box) authentication with the Google IoT Core Cloud services.
  • The WINC1510 Network Controller provides wireless connectivity and offloads all networking tasks from the main processor providing a secure socket connection and server authentication.
  • The MCP9808 Temperature sensor, a third party lighting sensor, Battery Charger MCP73871, Power Regulator MIC33350, nEDBG Debugger.

 

image

Note: this product does not come with pin headers. You will need to obtain the headers and solder them on.

Important Dates

Enrollment Begin: Nov 19 1018

Enrollment Ends: Dec 21 2018

RoadTesters Selected: Dec 26 2018

Product Shipped: Jan 4 2019

RoadTesting Begins: Jan 11 2019

Reminder/Update Email:  Feb 11 2019*

Submit Reviews By: Mar 11 2019*

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

Terms and Conditions

RoadTest

Terms and Conditions

These are the terms and conditions which govern theMicrochip AVR-IoT WG Dev Board RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Dec 21 2018

Announcement of Winner (estimated): Dec 26 2018

Prize:Microchip AVR-IoT WG Dev Board
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
  • Before I decide to publish my thoughts in the review, I’d like to share few doubts concerning issues I faced up, which still remains unsolved.

    First most annoying matter is instability of connection with “own” program prepared according to Leverege instructions .

    I tested two ways - using ready to use Atmel-Start example (+ compilation in Atmel Studio) and building “from the beginning” using MPLAB-X and MCC.

    After upload, the “firmware” it disconnects often - sometimes restores to work for the while or get lost at all!

     

    To avoid advices how to correct the WiFi connection reliability I must ensure, my WLAN’s are sufficient enough,  the board works fine with original firmware/ software.

    I checked it with two WLAN's - everything went fine with "base"  [AVR-IoT_WG_Sensor_Node_v1.0.3.hex] and also “fresh” [v1.1.0] firmware.

    After clicking "CLICK-ME.HTM" dashboard on  https://avr-iot.com/device/---- is alive and online full time.

    image

     

    Unfortunately after putting my ".hex" (nothing beyond the example from manual) into the board, after move to my dashboard at https://avr-iot-mc1.firebaseapp.com/device/0123...

    it catches the connection for a moment to lose it soon.

     

    I checked - this is not a problem with my WLAN, in many places and with different routers the issue repeats!

    image

    Above - very rare screen in my case

     

    I was told about the UI feature, which expects a constant flow of data,and would show the “connection page” if it doesn't receive data for 15s or longer.

    But I didn’t change data flow parameters. I suppose “my” firmware broadcasts data as frequently as “original”,

    I was suggested to  adjust the maxDataAge variable in the UI source code but, honestly, I’m afraid that parameter is unavailable in our standard project.

    Did somebody encountered similar issue? Or just could suggest solution?

     

    And one other minor one:

    As told before, I succeed to compile the project preparing it from the beginning in MPLAB-X. Also I did produce one using Atmel Start.

    Attempt to import the Atmel START example to MPLAB went good

    imageimage

    But at the end, imported project couldn't be compiled in MPLAB-X.

    image

    Nevermind, the compilation at Atmel Studio went fluently.

     

    Marek

Comment
  • Before I decide to publish my thoughts in the review, I’d like to share few doubts concerning issues I faced up, which still remains unsolved.

    First most annoying matter is instability of connection with “own” program prepared according to Leverege instructions .

    I tested two ways - using ready to use Atmel-Start example (+ compilation in Atmel Studio) and building “from the beginning” using MPLAB-X and MCC.

    After upload, the “firmware” it disconnects often - sometimes restores to work for the while or get lost at all!

     

    To avoid advices how to correct the WiFi connection reliability I must ensure, my WLAN’s are sufficient enough,  the board works fine with original firmware/ software.

    I checked it with two WLAN's - everything went fine with "base"  [AVR-IoT_WG_Sensor_Node_v1.0.3.hex] and also “fresh” [v1.1.0] firmware.

    After clicking "CLICK-ME.HTM" dashboard on  https://avr-iot.com/device/---- is alive and online full time.

    image

     

    Unfortunately after putting my ".hex" (nothing beyond the example from manual) into the board, after move to my dashboard at https://avr-iot-mc1.firebaseapp.com/device/0123...

    it catches the connection for a moment to lose it soon.

     

    I checked - this is not a problem with my WLAN, in many places and with different routers the issue repeats!

    image

    Above - very rare screen in my case

     

    I was told about the UI feature, which expects a constant flow of data,and would show the “connection page” if it doesn't receive data for 15s or longer.

    But I didn’t change data flow parameters. I suppose “my” firmware broadcasts data as frequently as “original”,

    I was suggested to  adjust the maxDataAge variable in the UI source code but, honestly, I’m afraid that parameter is unavailable in our standard project.

    Did somebody encountered similar issue? Or just could suggest solution?

     

    And one other minor one:

    As told before, I succeed to compile the project preparing it from the beginning in MPLAB-X. Also I did produce one using Atmel Start.

    Attempt to import the Atmel START example to MPLAB went good

    imageimage

    But at the end, imported project couldn't be compiled in MPLAB-X.

    image

    Nevermind, the compilation at Atmel Studio went fluently.

     

    Marek

Children
No Data