Digilent Zybo Z7 + Pcam 5C

Table of contents

image

To view the webinar recording, go here: Embedded Vision on Xilinx FPGA

 

{tabbedtable} Tab LabelTab Content
About

The Zybo Z7 is a feature-rich, ready-to-use embedded software and digital circuit development board built around the Xilinx Zynq-7000 family. This is the second generation update to the popular Zybo that was released in 2012. The Zynq family is based on the Xilinx All Programmable System-on-Chip (AP SoC) architecture, which tightly integrates a dual-core ARM Cortex-A9 processor with Xilinx 7-series Field Programmable Gate Array (FPGA) logic. The Zybo Z7 surrounds the Zynq with a rich set of multimedia and connectivity peripherals to create a formidable single-board computer, even before considering the flexibility and power added by the FPGA. The Zybo Z7's video-capable feature set, including a MIPI CSI-2 compatible Pcam connector, HDMI input, HDMI output, and high DDR3L bandwidth, was chosen to make it an affordable solution for the high end embedded vision applications that Xilinx FPGAs are popular for. Attaching additional hardware is made easy by the Zybo Z7's Pmod connectors, allowing access to Digilent's catalog of over 70 Pmod peripheral boards, including motor controllers, sensors, displays, and more.

 

image

The Pcam 5C is an imaging module meant for use with FPGA development boards. The module is designed around the Omnivision OV5640 5 megapixel (MP) color image sensor. This sensor includes various internal processing functions that can improve image quality, including automatic white balance, automatic black level calibration, and controls for adjusting saturation, hue, gamma and sharpness. Data is transferred over a dual-lane MIPI CSI-2 interface, which provides enough data bandwidth to support common video streaming formats such as 1080p (at 30 frames per second) and 720p (at 60 frames per second). The module is connected to the FPGA development board via a 15-pin flat-flexible cable (FFC) that is pin compatible with the connector found on the popular Raspberry Pi development board. The Pcam 5C comes with a 10 cm flat-flexible cable and a factory-installed fixed focus lens with M12 lens mount, so it is ready to use out of the box.

Important Dates

Enrollment Begin: Apr 10 2019

Enrollment Ends: May 13 2019

RoadTesters Selected:May 292019

Product Shipped: May 30 2019

RoadTesting Begins: June 5 2019

Reminder/Update Email: July 5 2019*

Submit Reviews By: August 5 2019*

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

Terms and Conditions

RoadTest

Digilent Zybo Z7 + Pcam 5C

Terms and Conditions

These are the terms and conditions which govern the Digilent Zybo Z7 + Pcam 5C contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Apr 10 2019

Announcement of Winner (estimated): May 13 2019

Prize: Digilent Zybo Z7 + Pcam 5C
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
  • I'm going through the ZYBO Z7 & Pcam 5C HLS Video Workshop and just couldn't get some of the examples working in 2019.1. I just downloaded 2018.2  image

  • I have managed to get the Video Workshop example working on Vivado 2019.1. As thought, the problem is due to the example being created for a different  Vivado version (2018.1). To make it work on 2019.1, I have modified the example. While many changes are just "cosmetic"  (use current version tag 2019.1 rather than the old versions), the one change that I think is more substantial is the one made to Digilent's IP MIPI_CSI_2_RX v1:0, used in the "camera_in" block.

     

    While trying to synthesise the project, the synthesis of the above IP kept failing, complaining a signal (axi_data_count) couldn't be found. Earlier, when Vivado performed the IP Upgrade, I noticed something suspicious in the log: a warning about one of Xilinx's IP being updated:

    WARNING: [IP_Flow 19-3501] Upgraded line_buffer from AXI4-Stream Data FIFO 1.1 to AXI4-Stream Data FIFO 2.0

    Looking at the IP implementation (found in the zyboz7_workshop/vivado_project/repo/vivado-library/ip/MIPI_CSI_2_RX/hdl folder), the error seems to be due to the signal being declared in the interface for a line buffer, which is not actually present in the IP implementation of such interface. As mentioned, this could possibly be due to the version change for the AXI4-Stream IP. Although not 100% sure about this, I decided to comment out the signal, and this seems to have done the trick: the synthesis finally completed successfully, and I was able to generate the bitstream, and export to the SDK to be used to execute the demo on the Zybo Z7.

     

    Using Vivado 2019.1, the implementation reports some timing failiures (negative slack) on 3 endpoint. I need to investigate those further, to see if there is an easy way to fix them. Anyway, they don't seem to affect the functionality, the video work exactly as for the 2018.1 version.

     

    I have uploaded the modified version of the workshop files for Vivado 2019 on Github.

     

    Fabio

  • That's very helpful, thanks. I've made some progress on getting stuff working. I that's the error I got a couple of days ago when I had to put the Zybo down for a bit. (Huge project at work going live.)  Vivado versioning does appear to be quite a tricky issue.

Comment
  • That's very helpful, thanks. I've made some progress on getting stuff working. I that's the error I got a couple of days ago when I had to put the Zybo down for a bit. (Huge project at work going live.)  Vivado versioning does appear to be quite a tricky issue.

Children