RoadTest the Raspberry Pi 4 Model B (2GB)

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The Raspberry Pi 4 Model B is the latest product in the popular Raspberry Pi range of computers. It offers ground-breaking increases in processor speed, multimedia performance, memory, and connectivity compared to the prior-generation Raspberry Pi 3 Model B+, while retaining backwards compatibility and similar power consumption.

image

For the end user, Raspberry Pi 4 Model B provides desktop performance comparable to entry-level x86 PC systems. This product’s key features include a high-performance 64-bit quad-core processor, dual-display support at resolutions up to 4K via a pair of micro-HDMI ports, hardware video decode at up to 4Kp60, up to 4GB of RAM, dual-band 2.4/5.0 GHz wireless LAN, Bluetooth 5.0, Gigabit Ethernet, USB 3.0, and PoE capability (via a separate PoE HAT add-on). The dual-band wireless LAN and Bluetooth have modular compliance certification, allowing the board to be designed into end products with significantly reduced compliance testing, improving both cost and time to market.

 

The product featured in this RoadTest is the Raspberry Pi 4 Model B (2GB Variant)

 

{gallery} Raspberry Pi 4 Model B

image

image

image

image

 

Specifications

 

Processor

  • Broadcom BCM2711, quad-core Cortex-A72 (ARM v8) 64-bit SoC @ 1.5GHz

 

Memory

  • 1GB, 2GB or 4GB LPDDR4-2400 SDRAM (depending on model)

 

Connectivity

  • 2.4 GHz and 5.0 GHz IEEE 802.11b/g/n/ac wireless LAN, Bluetooth 5.0, BLE
  • Gigabit Ethernet
  • 2 × USB 3.0 ports
  • 2 × USB 2.0 ports

 

GPIO

  • Standard 40-pin GPIO header (fully backwards-compatible with previous boards)

 

Video & sound

  • 2 × micro HDMI ports (up to 4Kp60 supported)
  • 2-lane MIPI DSI display port
  • 2-lane MIPI CSI camera port
  • 4-pole stereo audio and composite video port

 

Multimedia

  • H.265 (4Kp60 decode);
  • H.264 (1080p60 decode, 1080p30 encode);
  • OpenGL ES, 3.0 graphics

 

SD card support

  • Micro SD card slot for loading operating system and data storage

 

Input power

  • 5V DC via USB-C connector (minimum 3A1)
  • 5V DC via GPIO header (minimum 3A1)
  • Power over Ethernet (PoE)–enabled (requires separate PoE HAT)

 

Environment

  • Operating temperature 0–50ºC

 

Compliance

  • For a full list of local and regional product approvals, please visit

https://www.raspberrypi.org/documentation/hardware/raspberrypi/conformity.md

 

Production lifetime

  • The Raspberry Pi 4 Model B will remain in production until at least January 2026.
Important Dates

Enrollment Begin: June 24 2019

Enrollment Ends: July 15 2019

RoadTesters Selected: Aug 4 2019

Product Shipped: Aug 6 2019

RoadTesting Begins: Aug 13 2019

Reminder/Update Email: Sept 13 2019

Submit Reviews By: Oct 13 2019

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

(deadline Nov 5 2019)

(deadline Nov 6 2019)

  (deadline Nov 11 2109)

Terms and Conditions

RoadTest

RoadTest the Raspberry Pi 4 Model B

Terms and Conditions

These are the terms and conditions which govern the RoadTest the Raspberry Pi 4 Model B contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on July 15 2019

Announcement of Winner (estimated): July 22 2019

Prize: RoadTest the Raspberry Pi 4 Model B

 

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

Comment List
Anonymous
  • Oh, I'm sorry!

    Given that here we talk about the roadtest, I thought you won the Raspberry!!! Sorry again!



  • I bought it. image

    At the first, Farnell told me in June, the PI4 with 4GB will come at the end of September. Then Farnell corrected the delivery-time later to November.

    But "voilà", I received the PI4 at the end of July.

     

    The point, I wanted it with the bigger memory. ""The chance to win a PI4 for the roadtest was very small for me.....""image

    No, this was a joke.

    But I think, the PI4 with the 4GB memory was not yet ready for the market. Raspberry wrote on its websites also about an 8GB version. But this is a future product, I think so.

  • Excuse me, but why did you receive a PI4 with 4GB and instead me and all other people received a 2GB version (official roadTest)???

  • Fine. I received my PI4 with 4GB at the end of July,2019. Faster than I thought.

    Please check the PCB board with a magnifying glass. I found tin balls on it.

    They can roll under the IC devices.

    image

    image

     

    Best Regards

    Gerald

    ---

  • Finally I got the Pi4.Excited to do the project and review.imageimage

  • For desktop operation with the RPi 4 sitting in the open, it seems to do a good job of keeping itself cool.

     

    However, if it is desired to mount the RPi4 in a very small enclosure with limited ventilation, the enclosure may need a fan.

     

    If the RPi is mounted in an enclosure with open sides and vent slots on top ( or a screen or louvers over the top) it should be OK as is.

  • Good approach, Gary!

     

    My question is: how much it is really necessary to cool the PI ?

  • Wow - Using the Raspberry Pi 3B as an example for deciding whether to put heatsinks and a fan on the Raspberry Pi 4 seemed a rational decision and backed by published articles by others on the RPi4.

     

    When the RPi 4 heatsinks and fan arrived, before applying them, the Raspberry Pi 4 went thru the same experiments as I had previously done with the RPi3B.

    VCN from a W10 PC to RPI 4 , RPi4 in free air.

    RPi4 goes online to You Tube videos. “Why me?” by Big Bad Voodoo Daddy, “Dream On” by Aerosmith, and Metallica “No Leaf Clover”.

    **** VNC cant keep up with the stream of a stream, But is keeping up much better than the RPi3B did. I'll put the actual frame rate numbers in the Road Test report.

     

    pi@raspberrypi:~ $ vcgencmd measure_temp

    RPI4 CPU temp is 73C, running 5C cooler than RPi3B did ( and RPi3B had heatsinks already installed!)

    Fan cooling the RPI4 (no heatsinks applied yet) the CPU temp dropped to 46 C while still running VNC and You Tube videos.

    After adding heatsinks, ( actually 2 on the CPU - one copper slab and aluminum fins) , running RPi4 with same conditions again, the CPU temp stabilized at 67C , and took several minutes to get there.

    Fan cooling the heatsinks under the same test conditions, took several minutes to stabilize to 42C. Again, much cooler than the RPi3B.

    image

    Summarizing: Without heatsinks or fans, RPi 4 ran 5C cooler than the RPi3B (which did have heatsinks). Adding heatsinks to RPi4 in free air, cooled another 5C.

    RPi 4  did a great job, was faster updating VNC screens, and is running cooler to boot compared to the RPi3B.

    As long as the RPI 4 is left in free air, it can do alot of crunching without heatsinks or fans.

    .......and watch out for this guy

    image

  • So much for coincidence! I received mine about 10 minutes back I live in India. Can't wait to test it out!

  • image

    Received the raspberry Pi 4B a few minutes ago. On Monday the test projects starts!

     

    Enrico